DMM Wsn Node + BLE Simple Peripheral
Table of Contents
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Dynamic Multi-protocol Manager
- Usage
- DMM Limitations
Introduction
The dmm_wsnnode_ble_sp project showcases a dynamic multi-protocol example which enables concurrent proprietary Sub-1G and BLE5. This example uses the tasks from the Wireless Sensor Network Node example and the BLE simple_peripheral example along with TI's DMM (Dynamic Multi-protocol Manager) to demonstrate the multi-protocol and dual band features of the CC1352R.
This baseline example is provided so customers can familiarize themselves with existing single mode examples that where released for previous TI connectivity devices and see how the DMM is used to enable these example to be run concurrently on a CC13x2.
Hardware Prerequisites
The default Simple Peripheral configuration uses the LAUNCHXL-CC1352R. This hardware configuration is shown in the below image:
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the dependencies section of the Release Notes located in root folder of the SDK.
For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack Quick Start Guide.
Note: If you are running an OAD example, be sure to first build and flash a BIM project located in
/examples/nortos/<BOARD>/bim
. For more instructions on how to do this, please refer to the BLE5-Stack Quick Start Guide.
Dynamic Multi-protocol Manager
The DMM uses 2 main components to dynamically arbitrate the RF resource.
- A Policy Manager
- A Scheduler
TI CC1352 devices are capable of dual band operation, the CC1352 LaunchPad (TI development platform) has a dual band antenna which performs well in the 868/916MHz band as well as the 2.4GHz band. Using the DMM on a CC1352 device enables not only multi-protocol, but also dual band. The below diagram shows how the DMM allows 2 stacks to run on the same device, which was previously only possible on 2 devices. For illustration purposes we will assume the stacks are a proprietary Sub-1G stack (called Wireless Sensor Network) and a BLE Stack. However this is defined by the developer for the stacks being used.
Single mode setup:
DMM Setup:
The DMM makes scheduling decisions based on Application Level information, Stack Level information, and the Global Priority Table (GPT).
The Stack Level information is embedded in each RF command and it includes: Start Type, Start Time, AllowDelay, Priority, Activity, etc.
The Global Priority Table (GPT) defines relative priorities of the two stacks
based on the activity and priority of RF commands. For details of the GPT,
refer to <SDK_DIR>\source\ti\common\dmm\dmm_priority_ble_wsn.c/h
.
The Application Level information is the user defined information via the policy
table and inludes: Application State Name, Weight, AppliedActivity, Pause, etc;
the policy table can have multiple policies. A policy defines a specific state
of the DMM application where the user wants to apply different priority based on
an action. A simplified policy table is shown below, it defines the behavior
when Stack 1 is performing an OAD and does not take into account the specific
state of the stack 2 (i.e. any state). It specifies that when Stack 1 is in an
OAD state, the priority of the BLE_CONNECTION
, in this case, is increased by
25. If any RF scheduling conflicts happen during the OAD, they will be resolved
by taking into account the modified priority defined in the policy.
Stack 1 State Name | Stack 2 State Name | Weight | Applied Activity | Description |
---|---|---|---|---|
OAD | Any | 25 | CONNECTION | Increase the priority of CONNECTION activity of Stack 1 by 25 during OAD operation |
The policy used in this example is more complex than the illustration above. For
details of the actual policy used refer to
<SDK_DIR>\source\ti\common\dmm\policy.h
and ti_dmm_application_policy.c/h
as
generated by the SysConfig tool.
The DMM also supports pausing/resuming stacks based on a policy change. This is achieved by an application callback, which is called from the DMM policy manager when a policy change requiring a stack to pause operation is entire. An example of pausing the Zigbee stack during a BLE_OAD is provided in the DMM Zigbee Coordinator Switch + BLE OAD example.
See the DMM chapter in your protocol stack user's guide for more information about DMM.
Usage
The idea behind this base line DMM example is that both Sub-1G application and BLE application behave the same as their single mode version while running concurrently on the same device.
For more information on the WSN Node usage and behavior refer to the User Guide for the single mode example here.
For more information on the BLE Simple Peripheral usage and behavior refer to the User Guide for the Single mode example here.
Note: If you are using a smartphone as the BLE central device and the same CC1352 LaunchPad was used previously with a different DMM or BLE example then you may need to forget the device in the smartphone BLE settings, then disable and enable BLE. Not doing this could result in the smartphone application displaying incorrect services and characteristics
BLE Multi-Connections
This project is configured by default to make use of Multiple (4) BLE Connections. This means that the DMM project will be able to support 4 BLE connections on top of the secondary stack network.
Updating Multi-Connection Settings
The Multi-Connection Settings can easily be changed via the Sysconfig tool. No application changes are required by the user to go from 1 connection to 4 connections.
As always, with network configuration changes, it's important to recognize that the update will change the maximum bandwidth required by the BLE Stack. When moving from the default settings to something new, you as the developer should take time to consider how this will effect your network requirements.
DMM Limitations
The initial implementation of DMM has only been tested with this policy. It is important that the BLE policy is not changed as this could result in issue within the BLE stack. The following limitations exist in the initial DMM implementation:
- Sub-1G SLR Phy not supported.
- Connection intervals lower than 60ms will result in high Sub-1G packet loss when BLE is connected.
- When connecting to a central device Sub-1G packet loss may be experienced until the update parameters are sent 1s after connection. This will be dependent on the initial connection interval of the BLE central devices.