RTLS System
Table of Contents
General Information
- Detailed guide can be found on SimpleLink Academy
- To get usage information for the RTLS Node Manager scripts and GUI please refer to:
tools\ble5stack\rtls_agent\README.md
- In order to edit and view how the RTLS subsystem handles uNPI commands, please refer to the following file:
tools\ble5stack\rtls_agent\rtls\rtls\ss_rtls.py
- In order to see a usage example, please refer to
tools\ble5stack\rtls_agent\examples\rtls_example.py
which shows how to use a RTLS Master + RTLS Slave + RTLS Passive combination - To access GUI, please refer to the readme file found in
tools\ble5stack\rtls_agent
.
Introduction
This readme contains the following information: 1. How to setup AoA demo 2. Description of commands accepted by RTLS Control and their meaning Both Connected AoA and Connectionless AoA are activated by OOB example
General Configuration
The following is a list of all possible build defines and corresponding options that can be set for each define in the build_config.opt file:
Add the following define to build_config.opt (using "-D") to activate the following option:
GATT_DB_OFF_CHIP
Indicates that the GATT database is maintained off the chip on the Application Processor (AP).
GAP_BOND_MGR
Used to include the Bond Manager
HOST_CONFIG
(BLE Host Build Configurations) Possible Options:
- PERIPHERAL_CFG - Used to include the GAP Peripheral Role support
- CENTRAL_CFG - Used to include the GAP Central Role support
- BROADCASTER_CFG - Used to include the GAP Broadcaster Role support
- OBSERVER_CFG - Used to include the GAP Observer Role support
BLE_V41_FEATURES
Configure the stack to use features from the BLE 4.1 Specification
- L2CAP_COC_CFG - Enable L2CAP Connection Oriented Channels
BLE_V50_FEATURES
Configure the stack to use features from the BLE 5.0 Specification The following BLE 5.0 features are enabled by default and cannotbe disabled.
- PHY_2MBPS_CFG - Enable 2 Mbps data rate in the Controller
- HDC_NC_ADV_CFG - Enable High Duty Cycle Non-Connectable Advertising
- CHAN_ALGO2_CFG - Enable Channel Selection Algorithm 2
HCI_TL_FULL
All supported HCI commands are available via the Tranport Layer's NPI. Intended for NP solution.
HCI_TL_NONE
No supported HCI commands are available via the Transport Layer's NPI. Intended for SOC solutions.
Periodic Advertising and Connectionless AoA
Receiver - RTLS Master
- MAX_NUM_CTE_BUFS=xx
- USE_PERIODIC_SCAN
- USE_PERIODIC_RTLS
Transmitter - RTLS Slave
- USE_PERIODIC_ADV
Combo Roles:
Combo roles can be set by defining multiple roles for HOST_CONFIG. The possible combo roles and HOST_CONFIG defines are: * Peripheral + Observer : PERIPHERAL_CFG+OBSERVER_CFG * Central + Broadcaster : CENTRAL_CFG+BROADCASTER_CFG * Peripheral + Central : PERIPHERAL_CFG+CENTRAL_CFG
Angle of Arrival - Setup
Software Setup
AoA is currently supported on all roles with the following caveats:
RTLS Master
- Master role will collect I/Q samples
- Master role supports the official BT5.1 Connected AoA implementation
- AoA API's can be accessed by using RTLS Services host module
RTLS Slave
- Slave will send out a constant tone at the end of connection packet and it will not collect I/Q samples
- Slave supports the official BT5.1 Connected AoA implementation
- AoA API's can be accessed by using RTLS Services host module
- The tone length is configured by the user using the CTE Time parameter (refer to
tools\ble5stack\rtls_agent\rtls\rtls\ss_rtls.py
). Note that RTLS Passive only supports reception of a tone of length 20
RTLS Passive
- Passive will collect I/Q samples with the following limitation: CTE Time is always configured to 20, Sample Rate is always 4Mhz and Sample Size is always 16 bit
- When using AoA raw output mode (AOA_MODE_RAW), consider the following:
- Connection interval of BLE must be at least 300ms to accomodate outputing all of the samples (a large 2k bytes chunk)
- Large amounts of heap will be used to support this mode
Hardware Setup
Note: Pin 29 will be held high on application initialization in order to enable a TX/RX antenna in cases where BOOSTXL-AOA is attached
AoA requires 2 devices at minimum: RTLS Master/Slave. The devices should be flashed with the rtls_master/rtls_slave applications as described above (with AoA flags). Compile and flash your applications.
- RTLS Master - CC2642R1 LaunchPad with BOOSTXL-AOA
Optional For Extra Accuracy
Add an RTLS Passive to the setup - also equipped with BOOSTXL-AOA
For the RTLS Master/Passive hardware setup, please take a look at Angle of Arrival BoosterPack
Running The Example
The steps to run the out of box example is described in tools\ble5stack\rtls_agent\README.html
- Mind the timing when using both features, if the connection interval is insufficient, it may be that the SW stack won't have enough resources to both keep the BLE connection alive and continuously output results
- The best way to check your timings is by using a Logic Analyzer and debugging the RF RX and TX signals. Refer BLE5-Stack Debugging Guide.
Raw Mode
Note that this mode puts extra strain on the UART and the timing of the system since RAW mode involves outputing large chunks of data.
When using RAW mode for AoA * Minimum recommended latency (Connection Interval) is 300ms * Maximal recommended latency is 800ms