UTIL Extension Vendor Specific API¶
UTIL Extension Commands¶
UTIL_NV_Read¶
- Opcode
0xFE81
- Command Description
Send this command to read an NV parameter.
Command Parameters
- nvID
- Size
2 byte(s)
- Default
0
- Range
Any 2-byte value
- nvLen
- Size
1 byte(s)
- Default
0
- Range
Any 1-byte value
Events Generated
When this command is received, the host will send the CommandStatus Event.
UTIL_NV_Write¶
- Opcode
0xFE82
- Command Description
Send this command to write an NV parameter.
Command Parameters
- nvID
- Size
2 byte(s)
- Default
0
- Range
Any 2-byte value
- nvDataLen
Size of NV data
- Size
1 byte(s)
- Value
size(nvData)
- nvData
NV Data Field. Structure can be different for each NV item
- Size
input byte(s)
- Default
“00”
- Range
Any 1-byte value
Events Generated
When this command is received, the host will send the CommandStatus Event.
UTIL_ForceBoot¶
- Opcode
0xFE83
- Command Description
Force the boot loader to run.
Events Generated
When this command is received, the device resets if the boot loader is present. Otherwise, the host will send the CommandStatus Event.
UTIL_BuildRevision¶
- Opcode
0xFE84
- Command Description
This command is used to read the build revision information of the BLE stack software.
Events Generated
When this command is received, the host will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen
- Size
1 byte(s)
- Range
- stk ver (mj/mn/ph)
- Condition
( StatStatus==0x00)
- Size
3 byte(s)
- Range
- bld ver
- Condition
( StatStatus==0x00)
- Size
2 byte(s)
- Range
- stk info
- Condition
( StatStatus==0x00)
- Size
1 byte(s)
- Range
Value
Description
0x01
IARProject
0x02
CCSProject
0x10
IARLibrary
0x80
ROMBuild
- ctrl info
- Condition
( StatStatus==0x00)
- Size
2 byte(s)
- Range
Value
Description
0x01
ADV_NCONN
0x02
ADV_CONN
0x04
SCAN
0x08
INIT
0x10
PING
0x20
SLV_FEAT_EXCHG
0x40
CONN_PARAM_REQ
- host info
- Condition
( StatStatus==0x00)
- Size
2 byte(s)
- Range
Value
Description
0x01
BROADCASTER
0x02
OBSERVER
0x04
PERIPHERAL
0x08
CENTRAL
UTIL_GetMemStats¶
- Opcode
0xFE87
- Command Description
Get memory statistics
Command Parameters
- command ID
- Size
1 byte(s)
- Default
2
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
Events Generated
When this command is received, the host will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen
- Size
1 byte(s)
- Range
:all cmdID receive :
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- cmdID
- Condition
( (cmdID & 0x01) == 0x01)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Size
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- Heap Size Free
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- Biggest free buffer Available
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- cmdID
- Condition
( (cmdID & 0x02) == 0x02)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Fail number
- Condition
( (cmdID & 0x02) == 0x02)
- Size
2 byte(s)
- Range
- Heap Allocated
- Condition
( (cmdID & 0x02) == 0x02)
- Size
4 byte(s)
- Range
- Heap Max Allocated
- Condition
( (cmdID & 0x02) == 0x02)
- Size
4 byte(s)
- Range
- cmdID
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Number of Thread
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
An array of size “Count” will be returned containing the parameters starting here:
- Priority
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
- Handle
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
- max Stack used
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
- stack size
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
The array of parameters ends here.
UTIL Extension Events¶
UTIL_GetMemStats¶
- Opcode
0x0681
- Event Description
This event displays memory statistics for debugging.
Event Parameters
- Status
- Size
1 byte(s)
- Range
See Status Table
- Module
- Size
1 byte(s)
- Range
Value
Description
0x00
HCI TL
0x01
Host TL
- cmdID
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- cmdID
- Condition
( (cmdID & 0x01) == 0x01)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Size
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- Heap Size Free
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- Biggest free buffer Available
- Condition
( (cmdID & 0x01) == 0x01)
- Size
4 byte(s)
- Range
- cmdID
- Condition
( (cmdID & 0x02) == 0x02)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Heap Fail number
- Condition
( (cmdID & 0x02) == 0x02)
- Size
2 byte(s)
- Range
- Heap Allocated
- Condition
( (cmdID & 0x02) == 0x02)
- Size
4 byte(s)
- Range
- Heap Max Allocated
- Condition
( (cmdID & 0x02) == 0x02)
- Size
4 byte(s)
- Range
- cmdID
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
Value
Description
0x01
Light Heap Statistic
0x02
Full Heap Statistic (requieres HEAPMGR_METRICS)
0x04
Thread usage Statistic (requieres HEAPMGR_METRICS)
- Number of Thread
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
An array of size “Count” will be returned containing the parameters starting here:
- Priority
- Condition
( (cmdID & 0x04) ==0x04)
- Size
1 byte(s)
- Range
- Handle
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
- max Stack used
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
- stack size
- Condition
( (cmdID & 0x04) ==0x04)
- Size
2 byte(s)
- Range
The array of parameters ends here.