CryptoKey.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
84 #ifndef ti_drivers_cryptoutils_cyptokey_CryptoKey__include
85 #define ti_drivers_cryptoutils_cyptokey_CryptoKey__include
86 
87 #include <stdint.h>
88 #include <stdbool.h>
89 
90 #ifdef __cplusplus
91 extern "C" {
92 #endif
93 
117 #define CryptoKey_STATUS_RESERVED (-32)
118 
132 #define CryptoKey_STATUS_SUCCESS (0)
133 
140 #define CryptoKey_STATUS_ERROR (-1)
141 
148 #define CryptoKey_STATUS_UNDEFINED_ENCODING (-2)
149 
150 
159 typedef uint8_t CryptoKey_Encoding;
160 static const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U;
161 static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U;
162 static const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U;
163 static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U;
164 static const CryptoKey_Encoding CryptoKey_KEYBLOB = 0x20U;
165 static const CryptoKey_Encoding CryptoKey_BLANK_KEYBLOB = 0x40U;
166 
173 typedef struct {
174  uint8_t *keyMaterial;
175  uint32_t keyLength;
177 
184 typedef struct {
185  void* keyStore;
186  uint32_t keyLength;
187  uint32_t keyIndex;
189 
196 typedef struct {
197  uint8_t *keyBlob;
198  uint32_t keyBlobLength;
200 
209 typedef struct {
210  CryptoKey_Encoding encoding;
211  union {
215  } u;
216 } CryptoKey;
217 
218 
229 typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy;
230 
239 int_fast16_t CryptoKey_getCryptoKeyType(CryptoKey *keyHandle, CryptoKey_Encoding *keyType);
240 
249 int_fast16_t CryptoKey_isBlank(CryptoKey *keyHandle, bool *isBlank);
250 
260 int_fast16_t CryptoKey_markAsBlank(CryptoKey *keyHandle);
261 
272 
273 #ifdef __cplusplus
274 }
275 #endif
276 
277 #endif /* ti_drivers_cryptoutils_cyptokey_CryptoKey__include */
Keyblob CryptoKey datastructure.
Definition: CryptoKey.h:196
uint32_t keyBlobLength
Definition: CryptoKey.h:198
CryptoKey_Plaintext plaintext
Definition: CryptoKey.h:212
static const CryptoKey_Encoding CryptoKey_KEYSTORE
Definition: CryptoKey.h:162
uint32_t keyIndex
Definition: CryptoKey.h:187
uint8_t CryptoKey_Encoding
List of the different types of CryptoKey.
Definition: CryptoKey.h:159
static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT
Definition: CryptoKey.h:161
static const CryptoKey_Encoding CryptoKey_KEYBLOB
Definition: CryptoKey.h:164
CryptoKey datastructure.
Definition: CryptoKey.h:209
Key store CryptoKey datastructure.
Definition: CryptoKey.h:184
static const CryptoKey_Encoding CryptoKey_BLANK_KEYBLOB
Definition: CryptoKey.h:165
int_fast16_t CryptoKey_getCryptoKeyType(CryptoKey *keyHandle, CryptoKey_Encoding *keyType)
Gets the key type of the CryptoKey.
void * keyStore
Definition: CryptoKey.h:185
static const CryptoKey_Encoding CryptoKey_PLAINTEXT
Definition: CryptoKey.h:160
uint32_t keyLength
Definition: CryptoKey.h:186
int_fast16_t CryptoKey_markAsBlank(CryptoKey *keyHandle)
Marks a CryptoKey as &#39;blank&#39;.
uint8_t * keyBlob
Definition: CryptoKey.h:197
CryptoKey_KeyBlob keyBlob
Definition: CryptoKey.h:214
CryptoKey_Encoding encoding
Definition: CryptoKey.h:210
Plaintext CryptoKey datastructure.
Definition: CryptoKey.h:173
int_fast16_t CryptoKey_initSecurityPolicy(CryptoKey_SecurityPolicy *policy)
Function to initialize the CryptoKey_SecurityPolicy struct to its defaults.
int_fast16_t CryptoKey_isBlank(CryptoKey *keyHandle, bool *isBlank)
Wheather the CryptoKey is &#39;blank&#39; or represents valid keying material.
CryptoKey_KeyStore keyStore
Definition: CryptoKey.h:213
struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy
Structure that specifies the restrictions on a CryptoKey.
Definition: CryptoKey.h:229
static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE
Definition: CryptoKey.h:163
uint8_t * keyMaterial
Definition: CryptoKey.h:174
uint32_t keyLength
Definition: CryptoKey.h:175
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale