Go to the documentation of this file. 44 #define HS_DONE_OK 0x3440 45 #define HS_DONE_RXTIMEOUT 0x3441 46 #define HS_DONE_RXERR 0x3442 47 #define HS_DONE_TXBUF 0x3443 48 #define HS_DONE_ENDED 0x3444 49 #define HS_DONE_STOPPED 0x3445 50 #define HS_DONE_ABORT 0x3446 51 #define HS_ERROR_PAR 0x3840 55 #define HS_ERROR_RXBUF 0x3841 56 #define HS_ERROR_NO_SETUP 0x3842 57 #define HS_ERROR_NO_FS 0x3843 58 #define HS_ERROR_RXOVF 0x3844 59 #define HS_ERROR_TXUNF 0x3845
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale