Running the Example Applications¶
This section provides an overview of the Z-Stack out-of-box example applications and instructions on how to run them. The examples are out-of-box compliant with the ZCL v7 Specification but will further Product Certification will be required.
Note
Most examples have a coordinator, end device and router application. Green Power Device examples complement the Sink coordinator/router examples. The Network Processor is standalone. Generic App provides the template code for application development with minimal overhead (i.e. no ZCL support included). Sample App incorporates the Zigbee Application Builder in SysConfig to help configure the required Zigbee application device type, clusters/attributes, commands, and command callback APIs.
Note
All sample applications are supported for 2.4 GHz capable devices. The READMEs listed below point to the CC26X2R1 example but if a different platform is intended to be used, replace the board name in the path to find the corresponding document(e.g. “examples/rtos/CC1352R1_LAUNCHXL/zstack/zc_doorlock/README.html” if CC1352R1 platform is intended).
Control and Indicating Equipment (CIE)
- Control and Indicating Equipment Coordinator Readme
- Control and Indicating Equipment End Device Readme
- Control and Indicating Equipment Router Readme
Door Lock
Door Lock Controller
- Door Lock Controller Coordinator Readme
- Door Lock Controller End Device Readme
- Door Lock Controller Router Readme
Generic App
Green Power Switch
Green Power Temperature Sensor
Light
Light Sink
Network Processor
OTA Server
Sample App
Switch
Switch OTA
Temperature Sensor
- Temperature Sensor Coordinator Readme
- Temperature Sensor End Device Readme
- Temperature Sensor Router Readme
Thermostat
Thermostat Sink
Warning Device
Zone Device