Example Application Guide¶
This section provides an overview of the TI Wi-SUN FAN Stack out-of-box example applications and instructions on how to run them.
The Wi-SUN FAN mesh network consists of two types of logical devices:
- The border router device
- Router node devices.
This separation of the device types derives from the Wi-SUN FAN Specification. The TI Wi-SUN FAN Stack can be configured in either of the two roles by choosing the corresponding application.
The example applications provided in the TI Wi-SUN FAN Stack are developed for the CC13xx platform. The examples can be run in two modes:
- Embedded mode, where the full Wi-SUN Stack and application run on the CC13xx device.
- NWP mode, where the CC13xx device acts as a network processor. In this case, you will need a host device, e.g. a laptop.
You can read more about these two modes in the chapter Architecture Choices.
Router Node Embedded Mode Example Application (ns_coap_node)¶
A router node (RN) is a device capable of connecting to other devices in the mesh
network. It can provide upward and downward packet forwarding. A new device is
able to join the network through any router. The connections between different
router nodes form the mesh topology. The ns_coap_node example implements the
router node with embedded mode architecture. This is the recommended example
to use as a starting point for router node development.
The ns_coap_node example is a fully embedded application demonstrating a
CoAP server on Wi-SUN FAN stack. The example is intended to work with the border
router example, which acts as the CoAP client that interacts via the CoAP
protocol with the CoAP node server. CoAP is an abbreviation of COnstrained
Application Protocol.
Running the Application¶
For information on how to run the router node example application please see the
README.md included with the application source code.
Device support¶
ns_coap_node is supported on the following development boards:
- CC1312R7 LaunchPad
- CC1352P7-1 LaunchPad
Router Node NWP Mode Example Application (ns_node)¶
A router node (RN) is a device capable of connecting to other devices in the mesh
network. It can provide upward and downward packet forwarding. A new device is
able to join the network through any router. The connections between different
router nodes form the mesh topology. The ns_node example implements the
router node with NWP mode architecture. Please note, in most situations it makes
sense to run the router node in embedded mode. For an example of this, please
refer to the Router Node Embedded Mode Example Application (ns_coap_node).
Running the Application¶
For information on how to run the router node example application please see the
README.md included with the application source code.
Device support¶
ns_node is supported on the following development boards:
- CC1312R1 LaunchPad
- CC1352P-1 LaunchPad
- CC1352R1 LaunchPad
- CC1312R7 LaunchPad
- CC1352P7-1 LaunchPad
Border Router Example Application (ns_br)¶
A border router (BR) device is a router that can also act as gateway between the
Wi-SUN FAN and a different network. In addition, the border router acts as the
root device and establishes the network. For this reason, a Wi-SUN FAN
needs at least one BR. The ns_br example implements the border router with
NWP mode architecture.
Running the Application¶
For information on how to run the border router example application please see the
README.md included with the application source code.
Device support¶
ns_br is supported on the following development boards:
- CC1312R7 LaunchPad
- CC1352P7-1 LaunchPad
Configuration Parameters¶
Example configuration is done mainly through SysConfig. You can read about SysConfig configuration in System Configuration (SysConfig).
For NWP mode, many values can be set at run time through the NWP interface. Please see the NWP interface guide or ti-wisunfan py-spinel readme for details.