Memory Map¶
The devices supported by the SimpleLink CC13xx/CC26xx SDK each contains several memory regions including RAM, ROM, and Flash. This section aims to show how these memory regions are utilized by the stack and user application. The stack library configuration memory map can be seen below.
CC2672x3 or CC13x2x1 or CC26x2x1 Memory Map¶
The following table contains the memory map for the CC2672x3, CC13x2x1 or CC26x2x1.
Memory Section | Starting Address | Size (bytes) | Description |
---|---|---|---|
Flash | 0x00000000 | 60 | Cortex Interrupt Vecs |
0x00001000 | 816 | TI RTOS ROM Jump Table | |
Application / Stack Code | |||
NV | 2-5 pages | Non-Volatile Storage | |
Last Flash Page* | 88 | CCFG | |
ROM | 0x10000000 | ROM_SIZE | TI-RTOS, IEEE 802.15.4 MAC, Crypto, Driverlib, Boot |
RAM | 0x20000000 | RAMVEC_SIZE | Interrupt Vector Table in RAM for dynamic Hwi creation |
0x20000100 | RTOSRAM_SIZE | Reserved for pointers for TI-RTOS in ROM | |
.bss and .data | |||
TI-RTOS kernel system stack (CSTACK) | |||
AUX RAM | 0x400E0000 | AUXRAM_SIZE | Memory area belonging to the Sensor Controller |
CC13x2x7 or CC26x2x7 Memory Map¶
The following table contains the memory map for the CC13x2x7 or CC26x2x7.
Memory Section | Starting Address | Size (bytes) | Description |
---|---|---|---|
Flash | 0x00000000 | 60 | Cortex Interrupt Vecs |
0x00001000 | 816 | TI RTOS ROM Jump Table | |
Application / Stack Code | |||
NV | 2-5 pages | Non-Volatile Storage | |
Last Flash Page* | 88 | CCFG | |
ROM | 0x10000000 | ROM_SIZE | TI-RTOS, IEEE 802.15.4 MAC, Crypto, Driverlib, Boot |
RAM | 0x20000000 | RAMVEC_SIZE | Interrupt Vector Table in RAM for dynamic Hwi creation |
0x20000100 | RTOSRAM_SIZE | Reserved for pointers for TI-RTOS in ROM | |
.bss and .data | |||
TI-RTOS kernel system stack (CSTACK) | |||
AUX RAM | 0x400E0000 | AUXRAM_SIZE | Memory area belonging to the Sensor Controller |
CC13x1x3 or CC26x1x3 Memory Map¶
The following table contains the Memory Map for the CC13x1x3 or CC26x1x3.
Memory Section | Starting Address | Size (bytes) | Description |
---|---|---|---|
Flash | 0x00000000 | 60 | Cortex Interrupt Vecs |
Application / Stack Code | |||
NV | 2-5 pages | Non-Volatile Storage | |
Last Flash Page* | 88 | CCFG | |
RAM | 0x20000000 | RAMVEC_SIZE | Interrupt Vector Table in RAM for dynamic Hwi creation |
.bss and .data | |||
TI-RTOS kernel system stack (CSTACK) |
Memory Map Variables¶
At the tables above, the following variables are platform dependent.
- Last Flash Page: top of the Flash subtracted by its page size
- CC2672x3, CC13x2x1 or CC26x2x1 : 344 kB or 0x56000 (0x58000 - 0x2000)
- CC13x2x7 or CC26x2x7 : 696 kB or 0xAE000 (0xB0000 - 0x2000)
- CC13x1x3 or CC26x1x3 : 344 kB or 0x56000 (0x58000 - 0x2000)
- ROM_SIZE :
- CC2672x3, CC13x2x1 or CC26x2x1 : 256 kB
- CC13x2x7 or CC26x2x7 : 256 kB
- CC13x1x3 or CC26x1x3 : N/A. ROM not used on device for TI-RTOS
- RAMVEC_SIZE :
- CC2672x3, CC13x2x1 or CC26x2x1 : 216 B
- CC13x2x7 or CC26x2x7 : 216 B
- CC13x1x3 or CC26x1x3 : 216 B
- RTOSRAM_SIZE :
- CC2672x3, CC13x2x1 or CC26x2x1 : 24 B
- CC13x2x7 or CC26x2x7 : 24 B
- CC13x1x3 or CC26x1x3 : N/A. No reserved for pointers for TI-RTOS in ROM, due to no ROM used for TI-RTOS
- AUXRAM_SIZE :
- CC2672x3, CC13x2x1 or CC26x2x1 : 4 kB
- CC13x2x7 or CC26x2x7 : 4 kB
- CC13x1x3 or CC26x1x3 : N/A. No AUX RAM present on device
TI-RTOS ROM Jump Table¶
The TI-RTOS ROM Jump Table can be relocated to any address. To do that, open the .cfg file of your project and add the following lines after the ROM declaration:
Note
There is no TI-RTOS ROM Jump Table on CC13x1x3 or CC26x1x3
var ROM = xdc.useModule('ti.sysbios.rom.ROM');
if (Program.cpu.deviceName.match(/CC26/)) {
ROM.romName = ROM.CC26X2V2;
}
else if (Program.cpu.deviceName.match(/CC13/)) {
ROM.romName = ROM.CC13X2V2;
}
ROM.constStructAddr = 0x4000; // replace 0x4000 with any address in FLASH
ROM.externFuncStructAddr = 0x43C0; // replace 0x43C0 with any address in FLASH
ROM.dataStructAddr = 0x20001080; // replace 0x20001080 with any address in RAM
The .map file for a given project can be consulted to see exactly what sections of the stack reside in ROM.
Note
The NV region can be configured to be two to five pages long using the
NVOCMP_NVPAGES
define. Refer to Flash for more information.
Determining Project Build Size¶
Project options such as device type (ZC, ZR, ZED, ZNP), features (OTA, UART, etc), and the network configurations provided above will affect the flash and RAM space required to build the application. In order to understand this dependency, it is possible to refer to the MAP file generated after building a Z-Stack project. For CCS this is the MEMORY CONFIGURATION section at the top of the MAP file located inside the default folder, where total Flash is equivalent to the total of the FLASH, FLASH_NV, and FLASH_LAST used rows. With IAR it is the Grand Total at the bottom of the MAP file found within the Output folder by adding the code, ro data, and rw data columns.