TI Z-Stack 5.30.00 Release Notes

Table of Contents

Introduction

Z-Stack 3.x is a component of the SimpleLink™ CC13xx/CC26xx Software Development Kit. This component enables development of Zigbee® 3.0 specification based products. Z-Stack is TI’s complete solution for developing certified Zigbee 3.0 solution on CC13xx and CC26xx platforms. Z-Stack contained in this release is based on Zigbee 3.0 specification with the added benefit of running on top of TI-RTOS.

Key features of Z-Stack 5.30.00 :

Additional information about TI’s Zigbee solution can be found at www.ti.com/zigbee

Z-Stack Documentation

The SimpleLink CC13xx and CC26xx Software Development Kit(SDK) allows easier product development by combining TI-RTOS and the Zigbee protocol stack in one unified SDK. All Z-Stack sample applications are based off the TI-RTOS Kernel. Key documents needed for Zigbee application development include:

Installation and Usage

What’s New

ID Summary
ZIGBEE-1572 Add CC2652PSIP platform

Fixed Issues

ID Summary
ZIGBEE-1656 ZED rejoin fails if BDB Network Steering initiated during active Network Discovery
ZIGBEE-1636 End Device should only discard Leave Request when macSrcAddr field does not match
ZIGBEE-1635 Update Device not sent to TC on receipt of a neighboring router NLME-LEAVE.indication
ZIGBEE-1606 Power Mode capabilities should not be configurable for Routers in Sysconfig
ZIGBEE-1592 SysConfig txPower is not used for power configuration on GPD applications
ZIGBEE-1556 Zigbee Application Builder does not generate all Client Cluster Attributes
ZIGBEE-1531 Routing devices do not discard APS Remove Device packets without APS encryption
ZIGBEE-1527 IEEE_addr_rsp responds with corrupt IEEE address
ZIGBEE-1517 ZR sends Update Device using Well-Known Link Key instead of pre-configured key for legacy TCs
ZIGBEE-1516 Parent only removes child from AssocTable on Mgmt_Leave_req when NLME-LEAVE.req is delivered
ZIGBEE-1406 Trust Center discards link key A before joiner acknowledges Confirm Key packet reception of link key B
ZIGBEE-1299 End Devices performing TC Rejoin broadcast Device Annce without first receiving Transport Key

Known Issues

ID Summary
ZIGBEE-1617 Z-Stack sleepy ZED unexpectedly active when using large poll period values

Upgrade and Compatibility Information

The Z-Stack 5.30.00 only supports Revision E SimpleLink CC13xx and CC26xx devices. No support for previous silicon revisions or LaunchPad™ development kits using earlier silicon revisions. If you’re unsure of the revision number of your device, please see the Package Symbolization and Revision Identification section of the Errata Note.

Operating System Support

Dependencies

The Z-Stack sample applications were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.

Note: Earlier IDE/toolchain versions are not supported and compatibility with newer versions of supported IDEs is not assured.

Device Support

Development Board Support

Validation

The Z-Stack sample applications were built & tested with versions of the following Integrated Development Environments (IDEs) and tool chains listed in the top-level SDK release notes:

This release is for evaluation and development purposes only. End products being developed with this protocol stack version will require a future update prior to obtaining Zigbee and/or regulatory certification.

Versioning

This product follows a version format, M.mm.pp.bb, where:

Technical Support and Product Updates