TI Bluetooth Mesh and the Zephyr Project¶
Here we will go over a high level overview of how Bluetooth Mesh builds on top of TI BLE5-Stack, including a stack architecture diagram to show how the Zephyr Project’s Bluetooth Mesh stack is used in parallel with our current TI BLE5-Stack.
As shown above in Figure 139., TI’s Bluetooth Mesh implementation ports over the Zephyr Mesh Stack while still leveraging our existing TI BLE5-Stack for use on embedded devices. For this reason, we only use Zephyr’s mesh stack functionality and not the BLE stack layers (i.e. Host/Controller). The porting layer serves as a translator that allows us to use both the Zephyr mesh stack along with the TI BLE5-Stack. Put simply, this layer converts Zephyr mesh specific API calls to the relevant TI BLE5-Stack API call.
Figure 140. shows an example of how the porting layer translates Zephyr mesh API’s to the appropriate TI BLE5-Stack APIs.
For more information on the Zephyr Mesh solution, see the Zephyr Project web page. The Zephyr Mesh implementation is documented here: Zephyr Mesh Documentation.