BLE5-Stack 2.00.01 (SDK 2.40) to BLE5-Stack 2.00.02 (SDK 3.10)¶
This section will describe a way to migrate a project from BLE5-Stack 2.00.01 to a BLE5-Stack 2.00.02 project.
Note
There now exists a GUI to assist in creating and configuring applications. Eventually all example applications that don’t use SysConfig will be deprecated. If you have an existing project and you want to start using SysConfig, see the SysConfig Migration guide.
For BLE5-Stack 2.00.02, example projects are split into two categories:
Example Project | Project structure |
---|---|
Host test | Same folder structure as before |
Multi role | New folder structure |
Project zero | Same folder structure as before |
Simple broadcaster | New folder structure |
Simple central | New folder structure |
Simple peripheral | New folder structure |
Simple peripheral oad off-chip | Same folder structure as before |
Simple peripheral oad on-chip | Same folder structure as before |
If you are porting a project that has been given a new folder structure, please skip to the Porting a Project With New Structure.
Porting a Project With the Same Folder Structure as Before¶
For this migration guide, Project Zero from BLE5-Stack 2.00.01 will be ported over to BLE5-Stack 2.00.02. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE5-Stack 2.00.02 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.00.02 example project that contains your target project’s base functionality.
In this example, we’re going to use Project Zero as the starting BLE5-Stack 2.00.02 sample project.
Transfer all modified application files from BLE5-Stack 2.00.01 into the BLE5-Stack 2.00.02 example project.
In this example, the following files from BLE5-Stack 2.00.01 were moved into Project Zero BLE5-Stack 2.00.02 example:
project_zero.c
project_zero.h
Modify
main.c
in the BLE5-Stack 2.00.02 example if additional tasks were added in the BLE5-Stack 2.00.01 project.Move any profiles and services that the application is using to the BLE5-Stack 2.00.02 project.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.00.02 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
OAD Modifications¶
If you have modified bim_main.c
in your BLE5-Stack 2.00.01 implementation,
you should be aware of the following change and implement it in your
BLE5-Stack 2.00.02 implementation. If you have not modified bim_main.c
, you
can just use the default file from the BLE5-Stack 2.00.02.
The only change is that the SHA2 driver has been replaced by the SHA2 driverlib implementation. This can be accomplished by the following steps:
In
bim_main.c
, include the SHA2 driverlib file (instead of SHA2CC26XX.h):#include "sha2_driverlib.h"
Add the following files to the bim project:
- ti/ble5stack/common/cc26xx/sha2/sha2_driverlib.c
- ti/ble5stack/common/cc26xx/sha2/sha2_driverlib.h
In
bim_main.c
in Bim_payloadVerify() replace/*total memory for operation: workzone and 5 key buffers*/ SHA2CC26XX_initialize((SHA256_memory_t *)(ecdsaSigVerifyBuf->SHAWorkzone)); SHA2CC26XX_execute((SHA256_memory_t *)ecdsaSigVerifyBuf->SHAWorkzone,dataPayload,payloadlen); SHA2CC26XX_output((SHA256_memory_t *)ecdsaSigVerifyBuf->SHAWorkzone, finalHash);
with
SHA2_open(); SHA2_addData(dataPayload, payloadlen); SHA2_finalize(finalHash); SHA2_close();
Porting a Project With New Structure¶
In BLE5-Stack 2.00.02 projects have been given a structure. The biggest differences are:
- Only one project per example (stack library is pre-built and included in the app project as library files).
- Many project configurations moved from the
.projectspec
/.ewp
files to the projectmakefile
. - IAR: New required step to set up the workspace.
For this migration guide, Simple Peripheral from BLE5-Stack 2.00.01 will be ported over to BLE5-Stack 2.00.02. Because of this restructuring, the recommended approach is to start with a BLE5-Stack 2.00.02 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.00.02 example project that contains your target project’s base functionality. For reference, see available sample projects that start with simple_
In this example, Simple Peripheral is used as the starting BLE5-Stack 2.00.02 sample project.
Transfer all modified application files from BLE5-Stack 2.00.01 into the BLE5-Stack 2.00.02 example project.
In this example, the following files from BLE5-Stack 2.00.01 were moved into Simple Peripheral BLE5-Stack 2.00.02 example:
simple_peripheral.c
simple_peripheral.h
The RCOSC build configuration no longer exists. To use RCOSC, add the following define in the project predefined symbols:
USE_RCOSC
.The PTM build configuration no longer exists. To use PTM mode, add the following define in the project predefined symbols:
PTM_MODE
. In addition, you will have to increase the number of ICall enabled tasks. To do this, increment theICALL_MAX_NUM_TASKS
by one. (In Simple Peripheral, set-DICALL_MAX_NUM_TASKS=4
insimple_peripheral_app.opt
.)Configure
build_config.opt
. This file has been moved to the application main folder (e.g.simple_peripheral_app_CC26X2R1_LAUNCHXL_tirtos_ccs/build_config.opt
).Modify
main.c
in the BLE5-Stack 2.00.02 example if additional tasks were added in the BLE5-Stack 2.00.01 project.Move any profiles and services that the application is using to the BLE5-Stack 2.00.02 project.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.00.02 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
The following predefined symbols used to be stored in the stack library project. In order to use these features, the linked stack libraries must be replaced with custom libraries for that feature.
For CCS, open the Project → Properties → Build → ARM Linker → File Search Path and make the substitutions.
For IAR, open Options → Runtime Checking → Linker → Extra Options and make the substitutions.
Define Default File Replace with file More information ATT_DELAYED_REQ OneLib.a
OneLib_del.a
Delaying an ATT Read Request StackWrapper.a
StackWrapper_del.a
ble_r2.symbols
ble_r2_del.symbols
GATT_NO_CLIENT OneLib.a
N/A Exchanging Supported Privacy Feature Information StackWrapper.a
StackWrapper_no_clnt.a
ble_r2.symbols
ble_r2_no_clnt.symbols
L2CAP_COC_CFG OneLib.a
OneLib_coc.a
Using the GATT Service StackWrapper.a
StackWrapper_coc.a
ble_r2.symbols
ble_r2_coc.symbols
- The
SC_HOST_DEBUG
symbols has been moved from the stack project to the app project list of predefined symbols. For information on how to use this define, please see LE Secure Connections.