OAD Application

The application layer is responsible for plugging the OAD service. The OAD profile and communication with the BLE-Stack is encapsulated inside the OAD module. An application developer wishing to implement use the TI OAD solution will not need to worry about implementing the OAD state machine, but instead can just include the module and make the proper calls as detailed in Adding BLE OAD to an Existing Project. However, the details of the OAD application layer are documented here for completeness and to aide in debugging.

OAD Software Architecture

The building blocks of the OAD software architecture are detailed below. In the figure below the following terms have been abbreviated for compactness in the image.

  • CB : Callback
  • SVC: BLE Service
  • Func: Function
../_images/ditaa-7382bbf87f7b2caa69a8ed798a00a953afaa88ba.png

Internally the OAD service is responsible for the following:

  • Implementing the OAD profile
  • Plugging the GATT read and write callback from the BLE5-Stack
  • Serializing and de-serializing structures from over the messages
  • Sending OAD related requests and responses to the BLE5-Stack to be sent over the air
  • Queuing up messages from stack callbacks to be processed later by the application
  • Implementing the OAD state machine, and ensuring proper state transitions
  • Implementing the OAD inactivity timers
  • Implementing getter/setter functions for the application to use and configure the OAD service

External to the OAD service the application task is responsible for the following. See Adding BLE OAD to an Existing Project more more information.

  • Plugging an OAD event handler
  • Calling the OAD event processing function in a task context when events are posted.
  • Resetting the device when the OAD_DL_COMPLETE event is received.

A message sequence chart is included below to show a sample of an application’s interaction with the OAD service.

@startuml
hide footbox

participant app_task.c as app
participant oad.c as oad
participant "BLE Stack" as BLE
participant "OAD Queue" as OADQ

box "BLE-Stack Context"
    participant "GATT R/W Callback" as GATT
end box

activate app

group Initialize OAD service
    app -> oad : OAD_open()

    activate oad
    oad -> BLE : GATTServApp_InitCharCfg() (repeat for each char CCCD)
    oad -> BLE : GATTServApp_RegisterService()

    oad -> OADQ : Queue_construct()
    deactivate oad

    app -> oad : OAD_register()
end

BLE -> app : ATT_MTU_UPDATED_EVENT
app -> oad : OAD_setBlockSize()


group Processing OAD Service Messages
    note over oad, BLE
        Peer device sends OTA command/write
    end note

    activate GATT
    GATT -> oad : oadWriteAttrCB()

    activate oad
    oad -> OADQ : oadEnqueueMsg()
    oad -> app : Execute (*oadWriteCB_t)
    deactivate OAD
    deactivate GATT

    app -> oad : OAD_processQueue()
    oad -> OADQ : Queue_get()

    note over oad
        Process event
    end note
end

group
@enduml

Figure 213. OAD service/ Application interaction

OAD State Machine

The OAD service implements an ‘OAD State Machine’ for performing the OAD. The following state machine depicts the OAD service state transitions and its interactions with the OAD communication profile messages for both on-chip and off-chip OAD.

../_images/oad_state_machine.png

Figure 214. OAD Types Overview

The states and state transitions are encapsulated inside the OAD service, but some of the critical states are described below to aide in understanding.

Note these sections refer to internal state handling and transitions local to the target device. For a summary of the over the air sequence see Sequence diagram for OAD process and for a breakdown of the different types of profile messages and how to interpret them over the air please see BLE-Stack OAD Profile.

Image Validation

After establishing a new connection, updating the connection interval for a faster OAD and enabling notifications of OAD Image Identify and OAD Image Block characteristics on the OAD target, the OAD distributor shall write to the Image Identify characteristic of the OAD target. The message data will be the header retrieved from the OAD Image available for OAD.

On receiving the Image Identify message, the OAD target will verify that the contents of the image can be supported. This is done by checking the Image Header fields, BIM & header versions, and length of the image.

The OAD target will then perform boundary checks in the case of an Application Only or Stack Only OAD. This is done to ensure no boundary violations will occur between the upgraded image and the images that remain on the device.

Image Block Transfers

After the Image Validation has completed, the OAD target will switch to the configuration state. There it will get the block size and set image count. When the OAD distributor sends the Start OAD Command to the Control Characteristic (for more details see OAD Control Characteristic Supported Commands.), the OAD target will respond with a Control characteristic notification requesting the first block. The OAD distributor will then send the first block to the OAD target.

This process continues with the OAD target notifying the OAD distributor of the next block it needs and the OAD distributor sending the requested image block until all blocks have been transferred.

Completion of the OAD Process

After receiving the complete image, the CRC32 of the entire image will be calculated and the ‘CRC32 status’ bytes will be set accordingly. If the computed CRC matches with the ‘CRC’ field of received image, it switches to ‘End’ state.

After the OAD process is complete the system will wait for the newly downloaded image to be enabled. Once the image is successfully enabled the OAD module will signal to the app that it should reset. After reset the BIM will process the new image accordingly.

With security enabled, BIM will validate the new image as part of the BIM procedure. If the image signature is valid, the BIM procedure continues as normal. However, an invalid image signature will reject the image, and BIM will continue searching for another image.

Warning

Since secure OAD images are validated in BIM, it is impossible for an application to know if a new image has a valid signature or not. Only during the BIM procedure is the image signature validated, and subsequently accepted or rejected. From the application’s stand point of view, the only indication of “success” that the OAD operation occurred successfully is the presence of a new image.

Read more about OAD image signature validation step in Section Secure BIM. For tips on how to verify that an OAD completed successfully please see Performing a BLE OAD, specifically Modifying the Image Version.