ECDHCC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
104 #ifndef ti_drivers_ecdh_ECDHCC26X2__include
105 #define ti_drivers_ecdh_ECDHCC26X2__include
106 
107 #include <stdint.h>
108 #include <stdbool.h>
109 
110 #include <ti/drivers/Power.h>
111 #include <ti/drivers/ECDH.h>
114 
115 #include <ti/devices/DeviceFamily.h>
116 #include DeviceFamily_constructPath(driverlib/pka.h)
117 
118 #include <ti/drivers/dpl/HwiP.h>
119 #include <ti/drivers/dpl/SwiP.h>
120 #include <ti/drivers/dpl/SemaphoreP.h>
121 
122 #ifdef __cplusplus
123 extern "C" {
124 #endif
125 
126 /* Exit the SWI and wait until an HWI call posts the SWI again */
127 #define ECDHCC26X2_STATUS_FSM_RUN_PKA_OP ECDH_STATUS_RESERVED - 0
128 /* Execute the next FSM state immediately without waiting for the next HWI */
129 #define ECDHCC26X2_STATUS_FSM_RUN_FSM ECDH_STATUS_RESERVED - 1
130 
140 typedef enum {
142 
146 
150 
154 
159 
166 typedef struct {
179  uint8_t intPriority;
181 
187 typedef struct {
188  bool isOpen;
191  int_fast16_t operationStatus;
196  ECDHCC26X2_FsmState fsmState;
198  uint32_t resultAddress;
200 
201 #ifdef __cplusplus
202 }
203 #endif
204 
205 #endif /* ti_drivers_ecdh_ECDHCC26X2__include */
ECDHCC26X2_FsmState
ECDHCC26X2 states.
Definition: ECDHCC26X2.h:140
ECDH_OperationType
Enum for the operation types supported by the driver.
Definition: ECDH.h:626
bool isOpen
Definition: ECDHCC26X2.h:188
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: ECDHCC26X2.h:179
The CryptoKey type is an opaque representation of a cryptographic key.
uint32_t semaphoreTimeout
Definition: ECDHCC26X2.h:197
ECDHCC26X2 Object.
Definition: ECDHCC26X2.h:187
Power Manager.
int_fast16_t operationStatus
Definition: ECDHCC26X2.h:191
Definition: ECDHCC26X2.h:141
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:649
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
ECDH_OperationType operationType
Definition: ECDHCC26X2.h:195
bool operationInProgress
Definition: ECDHCC26X2.h:189
uint32_t resultAddress
Definition: ECDHCC26X2.h:198
bool operationCanceled
Definition: ECDHCC26X2.h:190
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X2.h:193
ECDH_Operation operation
Definition: ECDHCC26X2.h:194
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X2.h:192
ECDH_ReturnBehavior
The way in which ECC function calls return after performing an encryption + authentication or decrypt...
Definition: ECDH.h:549
ECDHCC26X2_FsmState fsmState
Definition: ECDHCC26X2.h:196
ECDHCC26X2 Hardware Attributes.
Definition: ECDHCC26X2.h:166
Definition: ECDHCC26X2.h:145
Union containing pointers to all supported operation structs.
Definition: ECDH.h:618
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale