Time synchronization over the air¶
In a network of multiple devices, it is often required that all participants operate on a common time base. This document describes how to synchronize multiple CC13xx devices using the proprietary PHY.
In our example we have a central and a node and we want to synchronize the
node clock to the central’s clock. Both clocks run at the same tick rate, but
the node clock has an initial offset relative to the central.
Assuming that
and
specify absolute timestamps with
index
on the central and the node, respectively, we get the
relationship:
(1)¶
Initially, the node doesn’t know and hence,
is always
different from the central’s time
.
As the timer domain, we choose the radio timer RAT on the RF core which provides 32 bit timestamps at 4 MHz (4 ticks per µs). RAT timestamps can be used as absolute start and end triggers for radio operation commands.
One-way synchronization example¶
In order to get , it would be enough to send one message at a
timestamp
from the central to the node as shown in the sequence
chart below:
Figure 29. Sequence chart of the one-way time synchronization process.
The node would receive the message after a certain delay
at
and could deduce
by the
following formula:
(2)¶
is the time of the receiver signal Syncword found. The
transmission offset
contains the time to bring up the RF
front-end, to calibrate the synthesizer and to send the packet preamble and
the syncword. The time of flight (TOF) is very small compared to that value
and can be ignored.
is a fixed value and depends on the
chosen RF settings. It must be measured/only once during development and is
then compiled into the application.
A two-way synchronization algorithm¶
This section describes an indirect approach that doesn’t require to measure
. But it can also be used to deduce
indirectly. We use an algorithm similar to the Network Time
Protocol.
The following sequence diagram shows the synchronization process.
Figure 30. Sequence chart of the two-way time synchronization process.
The node sends a synchronization request to the central at and
sets
as an absolute start trigger for the TX command.
The central receives the message after at
.
This is the timestamp that is appended as meta data to the packet and
specifies the time when the sync word was found:
(3)¶
After a short time , the central responds to the
request with a reply message at
. It sets the TX command start
trigger to
and includes
into the packet payload as
well:
(4)¶
When the client receives the reply at , it has the following timing
information and can calculate the initial clock offset
:
: Request sent by the client
: Request received by the central
: Reply received by the client
: A fixed delay for message processing on the central
From (1), we know that:
(5)¶
We do not know , but we know its offset to
which is
:
(6)¶
(7)¶
We still do not know , but we know that it is included
into the round-trip time
as follows:
(8)¶
With the help of (8) we can rewrite (7) to:
(9)¶
and finally obtain . This value must now be added to any further RF
operation on the client.
Sending and receiving timestamp messages¶
This section provides code snippets for implementing the above algorithms.
When sending a timestamp message at a certain time, we use txTimestamp as
an absolute start trigger, but include it also into the packet payload:
// Convenience macro
#define RF_convertMsToRatTicks(milliseconds) \
(((uint32_t)(milliseconds)) * 1000 * 4)
// Exported from SmartRF Studio
rfc_CMD_PROP_TX_t txCommand;
// Set a time in the near future (5ms)
uint32_t txTimestamp = RF_getCurrentTime() + RF_convertMsToRatTicks(5);
// Set txTimestamp as an absolute start trigger
txCommand.startTrigger.triggerType = TRIG_ABSTIME;
txCommand.startTime = txTimestamp;
// Include it also into the payload
uint32_t payload[1] = { txTimestamp };
txCommand.pPkt = (uint8_t*)&payload[0];
txCommand.pktLen = sizeof(payload);
When receiving this packet, the receiver must read the timestamp from the
packet payload, but must also configure the RF core to append a timestamp to
each received packet. This is the time when the RF core raises the signal
“Synchronization found” and we choose the name rxTimestamp:
// Exported from SmartRF Studio
rfc_CMD_PROP_RX_t rxCommand;
// Append RX timestamp to the payload
RF_cmdPropRx.rxConf.bAppendTimestamp = 1;
// The code to execute the RX command and to setup
// the RX data queue is not shown here.
// When reading the packet content from the
// RX data queue, rxTimestamp is behind the payload:
rfc_dataEntryGeneral_t* currentDataEntry = RFQueue_getDataEntry();
// Assuming variable length
uint8_t packetLength = *(uint8_t*)(¤tDataEntry->data);
uint8_t* packetDataPointer = (uint8_t*)(¤tDataEntry->data + 1);
uint32_t rxTimestamp;
memcpy(&rxTimestamp, &packetDataPointer + packetLength, 4);
// The TX timestamp is found in the payload
uint32_t txTimestamp;
memcpy(&rxTimestamp, packetDataPointer + packetLength, 4);