TI BLE5-Stack API Documentation
2.02.05.00
|
This file contains OAD Profile header file.
Go to the source code of this file.
Data Structures | |
struct | blockReqPld_t |
struct | blockSizeRspPld_t |
struct | deviceTypeRspPld_t |
struct | extImgEnableReq_t |
struct | genericExtCtrlRsp_t |
struct | imageInfo_t |
struct | imageInfoRspPld_t |
struct | imgIdentifyPld_t |
struct | oadTargetCBs_t |
struct | oadTargetWrite_t |
struct | profileVerRsp_t |
struct | swVersionPld_t |
Macros | |
#define | EXT_CTRL_OP_CODE(pData) (pData[0]) |
#define | OAD_ALREADY_STARTED 4 |
OAD is already is progress. | |
#define | OAD_ATT_OVERHEAD 3 |
#define | OAD_AUTH_FAIL 12 |
Authorization failed. | |
#define | OAD_BLK_NUM_HDR_SZ 4 |
#define | OAD_BUFFER_OFL 3 |
Block Number doesn't match requested. | |
#define | OAD_CCCD_CNT OAD_CHAR_CNT |
#define | OAD_CCCD_NOT_ENABLED 15 |
CCCD is not enabled, notif can't be sent. | |
#define | OAD_CHAR_CNT 3 |
#define | OAD_CRC_ERR 1 |
Downloaded image CRC doesn't match. | |
#define | OAD_DEFAULT_BLOCK_SIZE 20 |
#define | OAD_DEFAULT_INACTIVITY_TIME 10000 |
#define | OAD_DL_COMPLETE 14 |
OAD image payload download complete. | |
#define | OAD_DL_COMPLETE_EVT Event_Id_02 |
#define | OAD_DL_NOT_COMPLETE 6 |
An OAD is ongoing. | |
#define | OAD_EFL_MAX_META 4 |
#define | OAD_EXT_CTRL_BLK_RSP_NOTIF 0x12 |
#define | OAD_EXT_CTRL_CANCEL_OAD 0x05 |
#define | OAD_EXT_CTRL_CMD_NOT_SUPPORTED 0xFF |
#define | OAD_EXT_CTRL_DISABLE_BLK_NOTIF 0x06 |
#define | OAD_EXT_CTRL_ENABLE_IMG 0x04 |
#define | OAD_EXT_CTRL_ERASE_BONDS 0x13 |
#define | OAD_EXT_CTRL_GET_BLK_SZ 0x01 |
#define | OAD_EXT_CTRL_GET_DEV_TYPE 0x10 |
#define | OAD_EXT_CTRL_GET_IMG_INFO 0x11 |
#define | OAD_EXT_CTRL_GET_IMG_STAT 0x08 |
#define | OAD_EXT_CTRL_GET_PROF_VER 0x09 |
#define | OAD_EXT_CTRL_GET_SW_VER 0x07 |
#define | OAD_EXT_CTRL_IMG_CNT 0x02 |
#define | OAD_EXT_CTRL_START_OAD 0x03 |
#define | OAD_EXT_CTRL_UUID 0xFFC5 |
#define | OAD_EXT_NOT_SUPPORTED 13 |
Ctrl point command not supported. | |
#define | OAD_FLASH_ERR 2 |
Flash function failure (int, ext) | |
#define | OAD_IDX_EXT_CTRL 2 |
#define | OAD_IDX_IMG_BLOCK 1 |
#define | OAD_IDX_IMG_IDENTIFY 0 |
#define | OAD_IMAGE_ID_RSP_LEN 0x01 |
#define | OAD_IMAGE_TOO_BIG 8 |
Candidate image is too big. | |
#define | OAD_IMG_BLOCK_UUID 0xFFC2 |
#define | OAD_IMG_COUNT_UUID 0xFFC3 |
#define | OAD_IMG_ID_RETRIES 3 |
#define | OAD_IMG_ID_TIMEOUT 16 |
Image identify timed out, too many failures. | |
#define | OAD_IMG_IDENTIFY_UUID 0xFFC1 |
#define | OAD_IMG_INFO_ONCHIP 0x01 |
#define | OAD_IMG_PG_INVALID 0xFF |
OAD Security Types. More... | |
#define | OAD_IMG_STATUS_UUID 0xFFC4 |
#define | OAD_INCOMPATIBLE_FILE 11 |
BIM or FW mismatch. | |
#define | OAD_INCOMPATIBLE_IMAGE 9 |
Image signing failure, boundary mismatch. | |
#define | OAD_INVALID_FILE 10 |
If Invalid image ID received. | |
#define | OAD_MAX_BLOCK_SIZE 244 |
#define | OAD_MIN_INACTIVITY_TIME 4000 |
#define | OAD_NO_RESOURCES 7 |
If memory allocation fails. | |
#define | OAD_NOT_STARTED 5 |
OAD has not yet started. | |
#define | OAD_OUT_OF_MEM_EVT Event_Id_03 |
#define | OAD_QUEUE_EVT Event_Id_01 |
#define | OAD_SEC_AES_128_CBC 0x02 |
OAD Security Type for AES 128. | |
#define | OAD_SEC_ECDSA_P256 0x01 |
OAD Security Type for ECDSA P256. | |
#define | OAD_SERVICE_UUID 0xFFC0 |
#define | OAD_SUCCESS 0 |
OAD succeeded. | |
#define | OAD_WRITE_PERMIT GATT_PERMIT_WRITE |
Typedefs | |
typedef void(* | oadWriteCB_t) (uint8_t event, uint16_t arg) |
Enumerations | |
enum | oadEvent_e { OAD_WRITE_IDENTIFY_REQ, OAD_WRITE_BLOCK_REQ, OAD_IMAGE_COMPLETE, OAD_EXT_CTRL_WRITE_CMD, OAD_TIMEOUT } |
enum | oadState_e { OAD_IDLE, OAD_VALIDATE_IMG, OAD_CONFIG, OAD_DOWNLOAD, OAD_CHECK_DL, OAD_COMPLETE } |
Functions | |
void | OAD_cancel (void) |
void | OAD_close (void) |
bool | OAD_evenBitCount (uint32_t value) |
uint16_t | OAD_getactiveCxnHandle () |
uint16_t | OAD_getBlockSize (void) |
bool | OAD_getSWVersion (uint8_t *swVer, uint8_t len) |
bool | OAD_isUsrAppValid (void) |
uint8_t | OAD_open (uint32_t oadTimeout) |
uint8_t | OAD_processQueue (void) |
void | OAD_register (oadTargetCBs_t *pfnOadCBs) |
uint8_t | OAD_setBlockSize (uint16_t mtuSize) |
uint8_t | oadCreateFactoryImageBackup (void) |