BLE5-Stack 2.02.03 (SDK 5.30) to BLE5-Stack 2.02.04 (SDK 5.40)¶
This section will describe a way to migrate a project from BLE5-Stack 2.02.03 to a BLE5-Stack 2.02.04 project.
The best way to migrate is to open a new project from the new SDK and transfer your changes and application code over to the new example.
Porting Simple Peripheral¶
For this migration guide, Simple Peripheral from BLE5-Stack 2.02.03 will be ported over to BLE5-Stack 2.02.04. The recommended approach is to start with a BLE5-Stack 2.02.04 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.04 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.02.03 into the BLE5-Stack 2.02.04 example project.
In this example, the following files from BLE5-Stack 2.02.03 were moved into Simple Peripheral BLE5-Stack 2.02.04 example:
simple_peripheral.csimple_peripheral.h
Move any profiles and services that the application is using to the BLE5-Stack 2.02.04 project.
Transfer the SysConfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
Update the radio configuration as described in Radio configuration update for migration from BLE5-Stack 2.02.03 to BLE5-Stack 2.02.04.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.02.04 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
Porting Simple Central¶
This section of the migration guide will focus on porting Simple Central from BLE5-Stack 2.02.03 to the BLE5-Stack 2.02.04. The recommended approach is to start with a BLE5-Stack 2.02.04 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.04 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.02.03 into the BLE5-Stack 2.02.04 example project.
In this example, the following files from BLE5-Stack 2.02.03 were moved into Simple Central BLE5-Stack 2.02.04 example:
simple_central.csimple_central.h
Modify
main.cin the BLE5-Stack 2.02.04 example if additional tasks were added in the BLE5-Stack 2.02.03 project.Move any profiles and services that the application is using to the BLE5-Stack 2.02.04.
Transfer the Sysconfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
Update the radio configuration as described in Radio configuration update for migration from BLE5-Stack 2.02.03 to BLE5-Stack 2.02.04.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.02.04 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
A Few Noteworthy Changes from BLE5-Stack 2.02.03 to BLE5-Stack 2.02.04¶
You can follow the guide above without addressing these updates, they are listed for your information only. All fine grained details might not be mentioned, please refer to the specific example you need to port and do a compare between the old and new project files. Please refer to the BLE5-Stack Release Notes for all the details.
Attention
Please note that the location of the precompiled RF libraries has moved to match the same pattern as other components in the SDK. The old path is now deprecated. Migration to the new library path may be required. Customers that disable SysCfg may be affected. See all the details in the RFLib release notes.
Stability and latency improvements in BLE Mesh
Added multi-role example for the CC2651P3 device
Bug fixes
Radio configuration update for migration from BLE5-Stack 2.02.03 to BLE5-Stack 2.02.04¶
The radio configuration has been updated in SDK 5.40 (BLE5-Stack 2.02.04) in relation with Radio_03 errata. Please refer to the silicon errata document of the device used for details.
The suggestions below are only applicable to devices using Bluetooth LE. Please make sure to refer to the guide corresponding to the device you are using.
For CC2642R, CC2652R and CC2652P devices¶
If you are using SysConfig - If configured to do so, SysConfig automatically generates the proper radio configuration. Refer to Radio for more details and verify if the option is properly enabled.
If you are NOT using SysConfig - Some changes should be implemented manually in the file
ti_radio_config.c.Add the following include
#include DeviceFamily_constructPath(rf_patches/rf_patch_mce_bt5.h)Modify the structure
RF_modeBleas below// TI-RTOS RF Mode Object RF_Mode RF_modeBle = { .rfMode = RF_MODE_AUTO, .cpePatchFxn = &rf_patch_cpe_bt5, .mcePatchFxn = &rf_patch_mce_bt5, .rfePatchFxn = 0 };
Modify the table
pOverrides_ble1Mbpsas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_ble1Mbps[] = { // override_ble5_setup_override_1mbps.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeadjust (uint32_t)0x015302A3, // override_ble5_residual_per.json // Symbol tracking: timing correction HW_REG_OVERRIDE(0x50D4,0x00F9), // Symbol tracking: reduce sample delay HW_REG_OVERRIDE(0x50E0,0x0087), // Symbol tracking: demodulation order HW_REG_OVERRIDE(0x50F8,0x0014), (uint32_t)0xFFFFFFFF };
Modify the table
pOverrides_ble2Mbpsas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_ble2Mbps[] = { // override_ble5_setup_override_2mbps_mce.json // PHY: Use MCE RAM (patch), RFE ROM MCE_RFE_OVERRIDE(1,0,2,0,3,2), // override_ble5_setup_override_2mbps.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeAdjust (uint32_t)0x00F102A3, // Bluetooth 5: increase low gain AGC delay for 2 Mbps HW_REG_OVERRIDE(0x60A4,0x7D00), // Rx: increase AGC hysteresis (HIGH_GAIN=15, LOW_GAIN=11) HW_REG_OVERRIDE(0x6098,0x75FB), // override_ble5_residual_per.json // Symbol tracking: timing correction HW_REG_OVERRIDE(0x50D4,0x00F9), // Symbol tracking: reduce sample delay HW_REG_OVERRIDE(0x50E0,0x0087), // Symbol tracking: demodulation order HW_REG_OVERRIDE(0x50F8,0x0014), (uint32_t)0xFFFFFFFF };
Modify the table
pOverrides_bleCodedas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_bleCoded[] = { // override_ble5_setup_override_coded.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeadjust (uint32_t)0x07A902A3, // Rx: Set AGC reference level to 0x21 (default: 0x2E) HW_REG_OVERRIDE(0x609C,0x0021), (uint32_t)0xFFFFFFFF };
For CC2642R-Q1 devices¶
If you are using SysConfig - Leveraging, SysConfig and Radio assess if you want to set
RF DesignationtoSelectivityorSensitivity. After that, SysConfig will automatically generate the proper radio configuration.If you are NOT using SysConfig - First assess if the radio should be optimized for selectivity or sensitivity while in receive mode on the LE 2M PHY.
If the radio should be optimized for selectivity, the radio configuration used in SDK 5.30 can be kept as it. No additional change is required.
If the radio should be optimized for sensitivity, some changes should be implemented manually in the file
ti_radio_config.c.Add the following include
#include DeviceFamily_constructPath(rf_patches/rf_patch_mce_bt5.h)Modify the structure
RF_modeBleas below// TI-RTOS RF Mode Object RF_Mode RF_modeBle = { .rfMode = RF_MODE_AUTO, .cpePatchFxn = &rf_patch_cpe_bt5, .mcePatchFxn = &rf_patch_mce_bt5, .rfePatchFxn = 0 };
Modify the table
pOverrides_ble1Mbpsas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_ble1Mbps[] = { // override_ble5_setup_override_1mbps.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeadjust (uint32_t)0x015302A3, // override_ble5_residual_per.json // Symbol tracking: timing correction HW_REG_OVERRIDE(0x50D4,0x00F9), // Symbol tracking: reduce sample delay HW_REG_OVERRIDE(0x50E0,0x0087), // Symbol tracking: demodulation order HW_REG_OVERRIDE(0x50F8,0x0014), (uint32_t)0xFFFFFFFF };
Modify the table
pOverrides_ble2Mbpsas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_ble2Mbps[] = { // override_ble5_setup_override_2mbps_mce.json // PHY: Use MCE RAM (patch), RFE ROM MCE_RFE_OVERRIDE(1,0,2,0,3,2), // override_ble5_setup_override_2mbps.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeAdjust (uint32_t)0x00F102A3, // Bluetooth 5: increase low gain AGC delay for 2 Mbps HW_REG_OVERRIDE(0x60A4,0x7D00), // Rx: increase AGC hysteresis (HIGH_GAIN=15, LOW_GAIN=11) HW_REG_OVERRIDE(0x6098,0x75FB), // override_ble5_residual_per.json // Symbol tracking: timing correction HW_REG_OVERRIDE(0x50D4,0x00F9), // Symbol tracking: reduce sample delay HW_REG_OVERRIDE(0x50E0,0x0087), // Symbol tracking: demodulation order HW_REG_OVERRIDE(0x50F8,0x0014), (uint32_t)0xFFFFFFFF };
Modify the table
pOverrides_bleCodedas below// Overrides for CMD_BLE5_RADIO_SETUP uint32_t pOverrides_bleCoded[] = { // override_ble5_setup_override_coded.json // Bluetooth 5: Set pilot tone length to 20 us HW_REG_OVERRIDE(0x5320,0x03C0), // Bluetooth 5: Compensate syncTimeadjust (uint32_t)0x07A902A3, // Rx: Set AGC reference level to 0x21 (default: 0x2E) HW_REG_OVERRIDE(0x609C,0x0021), (uint32_t)0xFFFFFFFF };
For CC2652RB devices¶
The radio configuration used in SDK 5.30 can be kept as it. No additional change is required.
For CC1352R and CC1352P devices¶
The radio configuration used in SDK 5.30 can be kept as it. No additional change is required.