Generic Access Profile (GAP)¶
The GAP layer of the Bluetooth Low Energy protocol stack is responsible for connection functionality. This layer handles the access modes and procedures of the device including device discovery, link establishment, link termination, initiation of security features, and device configuration. See GAP State Diagram. for more details.
Based on the role for which the device is configured, GAP State Diagram. shows the states of the device. The following describes these states.
Standby: The device is in the initial idle state upon reset.
Advertiser: The device is advertising with specific data letting any initiating devices know that it is a connectable device (this advertisement contains the device address and can contain some additional data such as the device name).
Scanner: When receiving the advertisement, the scanning device sends a scan request to the advertiser. The advertiser responds with a scan response. This process is called device discovery. The scanning device is aware of the advertising device and can initiate a connection with it.
Initiator: When initiating, the initiator must specify a peer device address to which to connect. If an advertisement is received matching that address of the peer device, the initiating device then sends out a request to establish a connection (link) with the advertising device with the connection parameters described in GAP Connection State.
Peripheral/Central: When a connection is formed, the device functions as a Peripheral if it is the advertiser and a Central if it is the initiator.
Bluetooth devices operate in one or more GAP roles based on the application use case. The GAP roles utilize one or more of the GAP states. Based on this configuration, many Bluetooth Low Energy protocol stack events are handled directly by the main application task and sometimes routed from the GAP Bond Manager. The application can register with the stack to be notified of certain events.
GAP Roles¶
Based on the configuration of the device, the GAP layer always operates in one of four (4) roles as defined by the specification:
Broadcaster - The device is an advertiser that is non connectable.
Observer - The device scans for advertisements but cannot initiate connections.
Peripheral - The device is an advertiser that is connectable and operates as Peripheral in a single link-layer connection.
Central - The device scans for advertisements and initiates connections and operates as a Central in a single or multiple link-layer connections.
The Bluetooth Core Specifications Version 5.2 allows for certain combinations of multiple roles, which are supported by the Bluetooth Low Energy protocol stack. For configuration of the Bluetooth Low Energy stack features, see Developing a Custom Application
Note
Bluetooth 5 also introduces new features including Extended Advertising. Bluetooth 5 supports legacy advertising maintaining backwards compatibility with previous versions. The following sections will describe how to operate the device for various GAP roles along with how to use the new Extended Advertising features with the new APIs.
The following sections will describe how to use the LE Advertising Extension feature. As its name suggests, the amount of advertising data that can be sent over the air has been extended from 31 bytes to 1650 bytes. Also multiple advertising sets can be created using a mix of legacy and extended advertisements. Extended advertisements introduces use the secondary advertising channels which uses the data channels to send extensive data in addition to the primary advertising channels (Ch. 37, 38, and 39) used in legacy advertisement.
GAP Constraints¶
GAP Scanner can only scan one PHY per scanning cycle.
The data length of the advertising data and the scan response data for Extended Advertising is limited to 1650 bytes. The connectable undirected advertising data is limited to 212 bytes. The connectable directed advertising data is limited to 206 bytes. For more information, refer to the Host Advertising Data section ([Vol 6], Part B, Section 2.3.4.9) of the Bluetooth Core Specifications Version 5.2. Following is the overview of maximum payload with different Advertising Extension events.
Advertisement Extensions Event Type and its Maximum Payload Size
Type |
Max AdvData |
Max ScanRsp |
PDUs Used |
PDUs Listened for |
---|---|---|---|---|
Connectable (Non-Scannable) |
212 bytes |
0 |
ADV_EXT_IND AUX_ADV_IND |
AUX_CONNECT_REQ |
Scannable |
0 |
1650 bytes w/chain |
ADV_EXT_IND AUX_ADV_IND AUX_CHAIN_IND |
AUX_SCAN_REQ |
Broadcast |
1650 bytes |
0 |
ADV_EXT_IND AUX_ADV_IND AUX_CHAIN_IND |
N/A |
Periodic Advertising |
1650 bytes |
0 |
ADV_EXT_IND AUX_ADV_IND AUX_SYNC_IND |
N/A |
GAP Advertiser¶
The application and profiles can directly call GAP API functions to perform Bluetooth Low Energy-related functions such as advertising or connecting. The GAP layer functionality is mostly defined in library code. The function headers can be found in gap.h. The advertising specific implementation is found in gap_advertiser.h. Most of these functions can be called directly.
The GAP Advertiser module lets you create advertisement sets. The application can then enable and disable the sets. This way, the application can quickly change the advertisement parameters and advertisement data. For example, an application can create an advertisement set for legacy advertising and one for long range advertising. If both sets are enabled, the application advertises both on the primary advertising channels with legacy advertising, and on a LE Coded PHY with the long range set. With long range advertising, more advertising data can be sent and connections can be formed from larger distances compared to legacy advertising.
Note
The advertisement data is de-coupled from the advertisement sets, so multiple sets can use the same advertisement data.
Multiple active advertising sets can set different advertising intervals. The
figure below illustrate how two advertising sets with different interval are
scheduled. The intervals does not need to be multiples of each other. In the
examples the advertising interval can be set in the .primIntMin
and
primIntMax
Advertisement Params (GapAdv_params_t
) member before the
advertisement set is enabled or during advertising as described in
Changing advertising parameters.
1 advParams1.primIntMin = 160; // 100 ms 2 advParams1.primIntMax = 160; // 100 ms 3 advParams2.primIntMin = 800; // 500 ms 4 advParams2.primIntMax = 800; // 500 ms
The following list describes how to configure the GAP layer for advertising. The simple peripheral example project will be used as an example.
Note
The advertisement set creation can be done using SysConfig.
Create Advertisement set with GapAdv_create(). The return value of GapAdv_create() is a handle for the advertisement set. The create function takes a GapAdv_params_t variable, so the first thing to do is to create this variable. The Tx Power of legacy advertisements cannot be individually set.
Some GapAdv_params_t variables are defined in gap_advertiser.h. In this example we will use one of them,
GAPADV_PARAMS_LEGACY_SCANN_CONN
. You can of course define your own GapAdv_params_t variable or modify an existing GapAdv_params_t variable.1 // Temporary memory for advertising parameters. These will be copied by the GapAdv module 2 GapAdv_params_t advParamLegacy = GAPADV_PARAMS_LEGACY_SCANN_CONN;
1 // Advertising handle 2 static uint8 advHandleLegacy;
1 // Create Advertisement set and assign handle 2 status = GapAdv_create(&SimplePeripheral_advCallback, &advParamLegacy, &advHandleLegacy);
Set Advertiser’s virtual address set with GapAdv_setVirtualAdvAddr(). The handle for the advertisement set, returned from GapAdv_create(), can also be used to create a custom private address for that advertisement set. This allows different advertising sets to have different addresses. This is only applicable for legacy non-connectable and non-scannable advertising sets.
1 // Set virtual address 2 status = GapAdv_setVirtualAdvAddr(advHandleLegacy, &bdAddr);
Load Advertisement and Scan Response data. Advertising and scan response data is decoupled from the advertising set. That is, it is possible for multiple advertising sets to use the same memory for advertising/scan response data. An advertising set could also use the same memory for its advertising and scan response data. (Note that this requires diligence as there are some data types that are only allowed once in the advertisement and scan response data. See the Bluetooth Core Specification Supplement (CSSv7) for specifics.)
If your advertisement set is not scannable, you can of course skip the last step (load scan response data). Example advertising and scan response data is shown in Listing 75. and Listing 76.
1 // Load advertising data that is statically allocated by the app 2 status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV, 3 sizeof(advertData), advertData); 4 5 // Load scan response data that is statically allocated by the app 6 status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_SCAN_RSP, 7 sizeof(scanRspData), scanRspData);
// Advertisement data static uint8_t advertData[] = { 0x02, // length of this data GAP_ADTYPE_FLAGS, DEFAULT_DISCOVERABLE_MODE | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED, // service UUID, to notify central devices what services are included // in this peripheral 0x03, // length of this data GAP_ADTYPE_16BIT_MORE, // some of the UUID's, but not all LO_UINT16(SIMPLEPROFILE_SERV_UUID), HI_UINT16(SIMPLEPROFILE_SERV_UUID) };
// Scan Response Data static uint8_t scanRspData[] = { // complete name 17, // length of this data GAP_ADTYPE_LOCAL_NAME_COMPLETE, 'S', 'i', 'm', 'p', 'l', 'e', 'P', 'e', 'r', 'i', 'p', 'h', 'e', 'r', 'a', 'l', // connection interval range 5, // length of this data GAP_ADTYPE_SLAVE_CONN_INTERVAL_RANGE, LO_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL), // 100ms HI_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL), LO_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL), // 1s HI_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL), // Tx power level 2, // length of this data GAP_ADTYPE_POWER_LEVEL, 5 // 5dBm };
Set which events to send to application. The events will be sent to the callback function given in GapAdv_create() (in this case
SimplePeripheral_advCallback()
).1 // Set event mask 2 status = GapAdv_setEventMask(advHandleLegacy, 3 GAP_ADV_EVT_MASK_START_AFTER_ENABLE | 4 GAP_ADV_EVT_MASK_END_AFTER_DISABLE | 5 GAP_ADV_EVT_MASK_SET_TERMINATED);
Enable advertising. Calling GapAdv_enable() will start advertising.
1 // Enable advertising 2 status = GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
The above steps can be repeated to create multiple advertising sets. There is an upper limit of six advertising sets (defined in the controller). The heap may also restrict the number of advertising sets you can create in one application.
Changing advertising parameters¶
In order to change an individual parameter after advertising has been enabled, advertising must first be disabled. Re-enable advertising after the parameter is modified.
1 // Stop advertising
2 GapAdv_disable(advHandleLegacy);
3
4 // Set a parameter
5 uint32_t newAdvInt = 200;
6 GapAdv_setParam(advHandleLegacy, GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, &newAdvInt);
7
8 // Re-enable advertising
9 GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
Ending Advertisement¶
An advertising set can be disabled with GapAdv_disable() and deleted (such that all memory related to the set is freed) with GapAdv_destroy().
1 // Stop advertising
2 GapAdv_disable(advHandleLegacy);
3
4 // Free all data related to advertising set (besides advertising / scan response data).
5 // Note that this can be called while advertising is still enabled
6 GapAdv_destroy(advHandleLegacy, GAP_ADV_FREE_OPTION_DONT_FREE);
The advertising and scan response data is statically allocated and is thus not freed as part of GapAdv_destroy().
Updating Advertisement/Scan Response Data¶
Again, since the advertising and scan response data is decoupled from the advertising set, it is possible for multiple advertising sets to use the same memory for advertising/scan response data. An advertising set could also use the same memory for its advertising and scan response data. The memory used for advertising/scan response data is referred to as a “buffer” throughout this section.
The preferred and safest method to update a buffer is to use the prepare/load latching mechanism. This will ensure the following:
No buffer is freed if it is used by another advertising set.
Advertising is always disabled before the buffer is modified, thus ensuring that no corrupted advertisement packets are transmitted.
Prevent double-copying.
The following offers several ways to update the advertising and scan response data.
Update the Advertising/Scan response Data of a Single Handle¶
If the application wants to modify a few bytes of advertising/scan response data that is used by a single advertisement set, use GapAdv_prepareLoadByHandle() and GapAdv_loadByHandle().
1 // Don't free anything since we're going to use the same buffer to re-load
2 GapAdv_prepareLoadByHandle(advHandleLegacy, GAP_ADV_FREE_OPTION_DONT_FREE);
3
4 // Sample buffer modification
5 advertData[3] = 0xAA;
6
7 // Reload buffer to handle
8 GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV, ADV_DATA_LEN, advertData);
The GapAdv_prepareLoadByHandle() will perform the following here:
Check that this buffer isn’t used by other handles. If GapAdv_prepareLoadByHandle() returns success, the application will know that it can now safely modify this buffer.
Automatically disable advertising and mark it for re-enabling
GapAdv_loadByHandle() will automatically re-enable advertising with the updated buffer. This method can also be used to use a subset of the original advertising data. In this case, simply update the data length parameter of GapAdv_loadByHandle().
Load a New Buffer to a Single Advertising Handle¶
If the application wants to load a new buffer to a single advertising handle without double-copying, use GapAdv_prepareLoadByHandle() and GapAdv_loadByHandle(). This way, the advertising data exists in only one place in memory that is used by the GAP Advertiser. In this case we will free the buffer and allocate a new one.
1 // Free the buffer (to avoid double copying) since we're loading a new buffer
2 GapAdv_prepareLoadByHandle(advHandleLegacy, GAP_ADV_FREE_OPTION_ADV_DATA);
3
4 // Allocate new buffer (and then fill it as desired)
5 uint8_t *advertData2= ICall_malloc(ADV_DATA2_LEN);
6
7 // Load the new buffer to the advertisement set handle
8 GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV, ADV_DATA2_LEN, advertData2);
GapAdv_prepareLoadByHandle() will perform the following here:
Check that the buffer isn’t used by any other advertisement handles. If GapAdv_prepareLoadByHandle() returns success, the application will know that it can now safely modify this buffer.
Automatically disable advertising and mark it for re-enabling
Free the original buffer
The GapAdv_loadByHandle() will automatically re-enable advertising on the handle with the new buffer.
Update Advertising/Scan Response Data that is Used for Multiple Advertising Handles¶
This is the case where the application wants to modify a few bytes of advertising or scan response data that is shared among advertisement sets.
1 // Don't free anything since we're going to use the same buffer to reload
2 GapAdv_prepareLoadByBuffer(advertData, FALSE);
3
4 // Sample buffer modification
5 advertData[3] = 0xAA;
6
7 // Reload the buffer to be used by the advertisement set handles
8 GapAdv_loadByBuffer(ADV_DATA_LEN, advertData);
GapAdv_prepareLoadByBuffer() will automatically disable advertising for all advertising handles that use this buffer. GapAdv_loadByBuffer() will automatically re-enable advertising for all handles that use this buffer.
Load a New Buffer To Multiple Advertising Handles¶
This is the case where the applications wants to load a new buffer to all advertisement set handles that are using this buffer.
1 // Free buffer (to avoid double copying) since we're loading a new buffer
2 GapAdv_prepareLoadByBuffer(advertData, TRUE);
3
4 // Allocate new buffer (and then fill as desired)
5 uint8_t *advertData2= ICall_malloc(ADV_DATA2_LEN);
6
7 // Reload the buffer to be used by all the handles
8 GapAdv_loadByBuffer(ADV_DATA2_LEN, advertData2);
GapAdv_loadByBuffer() will perform the following here:
Automatically disable advertising and mark it for re-enabling on all handles that use this buffer
Free the original buffer
GapAdv_loadByBuffer() will automatically re-enable advertising on all handles that used the original buffer.
Directly Manipulating a Buffer While Advertising is Enabled¶
Since the application owns the advertising and scan response buffers and thus has access to the memory where the buffers are stored, there is nothing preventing it from directly modifying this memory. While discouraged, there are scenarios where this can be useful, such as updating the data after each advertisement in the most power-efficient manner. The main drawback to this is that there is no way to guarantee that this update won’t occur while an advertising packet is being transmitted that is using this buffer, potentially resulting in a corrupted advertising packet. This is especially true if multiple advertising sets are using the same buffer. If the application accepts the risk of potentially corrupting an advertising packet, there is a recommended way to do this with minimized risk.
The buffer should be updated directly in the advertising callback (in the stack context)
when the GAP_EVT_ADV_END
is received. Generally, it is recommended to
minimize processing in these callbacks and, instead, to post an event to process
in the application context. It should be noted that any processing in the stack
context has the potential to break the timing of the controller. This should not
be a problem if the only processing is to update the buffer. Also, for both this
reason and because it will lead to a semaphore that never gets posted due to
calling an ICall API from the stack context, it should be noted that no stack
API calls can be made from the stack context. To reiterate for clarity, no BLE-Stack APIs
can be called from the callback (stack) context.
1 // Callback passed into GapAdv_create(). This code is running in the stack context.
2 static void SimplePeripheral_advCallback(uint32_t event, void *pBuf, uintptr_t arg)
3 {
4 // Advertisement just ended so it should be safe to update buffer here
5 // without corrupting an advertisement.
6 if (event == GAP_EVT_ADV_END)
7 {
8 advertData[3] = 0xAA;
9 }
10 }
Note that this can not be guaranteed to work all the time without corrupting an
advertisement. Also, if the buffer is used by multiple advertisement handles, the
application would need to track the GAP_EVT_ADV_ENDs
across all of these handles to
find an ideal time to update the buffer. If this processing is added to the callback
in the stack context, this increases the risk of breaking the timing of the
controller. Also, remember to include GAP_EVT_ADV_END
in the event mask
passed in GapAdv_setEventMask().
Sending Up To 1650 Bytes Scan Response Data¶
The Advertising Extension enables user to send huge amount of data without forming connections and prevent jamming legacy advertising channels. There are currently three methods for sending 1650 bytes data without establishing connections which listed under GAP Constraints.
Here we are focusing on transmitting 1650 bytes through scan response data. Even though broadcasting and periodic advertising can achieve the same outcome, it can sometimes consume more energy than necessary due to it is always transmitting 1650 bytes of data whether or not there are scanners listening. To avoid wasting energy, we can store 1650 bytes data in scan response. Then only when the advertiser receives scan request, it will respond with 1650 scan response data.
To send 1650 bytes scan response data, you will need to enable
the extended advertisement which contains PDU type ADV_EXT_IND
and AUX_ADV_IND
packets.
The ADV_EXT_IND
contains the following information which makes it possible for
scanner to send AUX_SCAN_REQ
packets under correct timing.
The data channel for the Auxiliary Packet Pointer which is
AUX_ADV_IND
packet.The clock accuracy for advertiser.
The time of when the
AUX_ADV_IND
packet will be transmitted.The PHY which is used by
AUX_ADV_IND
packet.
With the information provided by ADV_EXT_IND
packet, the scanner can jump
to data channel to listen for AUX_ADV_IND
ahead of time and then send
out AUX_SCAN_REQ
packet to request more data.
Once the advertiser receives AUX_SCAN_REQ
packet, it will respond with
AUX_SCAN_RSP
packet which can hold up to 242 bytes application data.
If the scan response data is more than 242 bytes, then the BLE5-Stack will
automatically create AUX_CHAIN_IND
packet(s), which can also
hold up to 242 bytes application data, and fragment the rest of the
scan response data until all the 1650 bytes are sent.
Important
This is currently not supported through Sysconfig, therefore to implement this feature, you will need to Disable SysConfig.
To acheive this using BLE5-Stack, follow the steps below:
Set the advertising event property to
GAP_ADV_PROP_SCANNABLE
.1 // Advertisement Params 2 GapAdv_params_t advParams = { 3 .eventProps = GAP_ADV_PROP_SCANNABLE, 4 .primIntMin = 160, 5 .primIntMax = 160, 6 .primChanMap = GAP_ADV_CHAN_ALL, 7 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, 8 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, 9 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, 10 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, 11 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, 12 .secPhy = GAP_ADV_SEC_PHY_2_MBPS, 13 .sid = 0 14 };
Create advertising handle with above parameters.
1 static uint8 advHandle; 2 GapAdv_create(&Application_advCallback, &advParams, &advHandle);
Warning
Here we do NOT load the advertising data as we are creating AE scannable packet which is not allowed to have data on legacy advertising channels.
Change the size of scanResData.
1 extern uint8_t scanResData[1650];
Fill out the scanResData to what you want to send over the air under application_init function.
1 uint16_t i; 2 3 // Use the sysconfig-generated scan response 4 // data for the first 27 bytes and fill out 5 // the rest with 0x55 6 for ( i = 27; i < sizeof(scanResData); i++) 7 { 8 scanResData[i] = 0x55; 9 }
Load scan response data and enable advertising.
1 // Load scan response data 2 GapAdv_loadByHandle(advHandle, GAP_ADV_DATA_TYPE_SCAN_RSP, 3 sizeof(scanResData), scanResData); 4 // Enable advertising 5 GapAdv_enable(advHandle, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
Note
To change scan response data on the fly, you can refer to Update the Advertising/Scan response Data of a Single Handle.
Limited Advertising¶
The above code sets the advertising interval for limited and general
advertising modes. By default, the peripheral advertises in general
discoverable mode. To use limited discoverable mode, the
corresponding fields inside the advertising data packet should be
changed by defining DEFAULT_DISCOVERABLE_MODE
to
GAP_ADTYPE_FLAGS_LIMITED
. The application is responsible for setting the advertising
data and advertising duration.
Periodic Advertising¶
Important
The symbol USE_PERIODIC_ADV
must be pre-defined if you
wish to send periodic advertisements (for more details, please see
Bluetooth Low Energy Stack Configuration Parameters).
Periodic adverting is part of the Advertising Extension and it allows device to send data synchronously at a fixed interval. Periodic advertising is not scannable, not connectable and the advertiser’s address should not be hidden.
In order for scanner to receive periodic advertisement, the extended advertisement
needs to be enabled and contain at least one PDU type AUX_ADV_IND
packet. The reason for that
is the SyncInfo
to the periodic advertisement packets can only be found
under AUX_ADV_IND
packet.
The detailed process for enabling periodic advertisement is as follows:
Advertiser sends out
ADV_EXT_IND
PDU type. Scanner will find the channel index, timing and PHY that a coming auxiliary packet(AUX_ADV_IND
) will be sent at under AuxPtr field.Advertiser then sends out
AUX_ADV_IND
PDU type package. If there is periodic advertisement coming up, scanner will findSyncInfo
field under extended header. The SyncInfo field contains the needed information for a scanner to follow periodic advertisement packets. For more detail, please refer to the picture below and Vol 6, Part B, Section 2.3 of Bluetooth Core Specifications Version 5.2.
The picture below depicts the overall flow of how periodic advertisement works.
The following list describes how to configure the GAP layer for periodic advertising.
Warning
The periodic advertisement set creation is not supported in SysConfig.
Enable Non-Connectable Non-Scannable Extended Advertisement¶
Setup parameters for non-connectable and non-scannable extended advertisement. To achieve this, you can set eventProps = 0 and sid != 0
1 /// Non-Connectable & Non-Scannable advertising set 2 #define GAPADV_PARAMS_AE_NC_NS { \ 3 .eventProps = 0, \ 4 .primIntMin = 160, \ 5 .primIntMax = 160, \ 6 .primChanMap = GAP_ADV_CHAN_ALL, \ 7 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 8 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 9 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 10 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 11 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 12 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 13 .sid = 1 \ 14 } 15 16 // Create non connectable & non scannable advertising 17 GapAdv_params_t advParamNonConn = GAPADV_PARAMS_AE_NC_NS;
Creating non-connectable and non-scannable extended advertisement.
1 static uint8 advHandleNCNS; // Non-Connactable & Non-Scannable 2 3 // Create Advertisement set #3 and assign handle 4 status = GapAdv_create(&advCallback, &advParamNonConn, 5 &advHandleNCNS); 6 7 // Load advertising data for set #3 that is statically allocated by the app 8 status = GapAdv_loadByHandle(advHandleNCNS, GAP_ADV_DATA_TYPE_ADV, 9 sizeof(advertData), advertData); 10 11 // Set event mask for set #3 12 status = GapAdv_setEventMask(advHandleNCNS, 13 GAP_ADV_EVT_MASK_START_AFTER_ENABLE | 14 GAP_ADV_EVT_MASK_END_AFTER_DISABLE | 15 GAP_ADV_EVT_MASK_SET_TERMINATED); 16 17 // Enable non connectable & non scannable advertising for set #3 18 // This is a must in order to enable periodic advertisement 19 status = GapAdv_enable(advHandleNCNS, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
Setup parameters for periodic advertisement. The BLE5-Stack will then return
GAP_ADV_SET_PERIODIC_ADV_PARAMS_EVENT
to the application layer whether or not the parameters are set successfully.1 /// Non-Connectable & Non-Scannable advertising set 2 #define GAPADV_PARAMS_PERIODIC_ADV { \ 3 .periodicAdvIntervalMin = 160, \ 4 .periodicAdvIntervalMax = 160, \ 5 .periodicAdvProp = GAPADV_PERIODIC_ADV_ENABLE_TX_POWER \ 6 } 7 8 // Set Periodic Advertising parameters 9 GapAdv_periodicAdvParams_t advParamsPerAdv = GAPADV_PARAMS_PERIODIC_ADV; 10 11 status = GapAdv_SetPeriodicAdvParams(advHandleNCNS, &advParamsPerAdv);
Warning
Only bit 6 in periodicAdvProp field can be set, otherwise the BLE5-Stack will return bleInvalidRange.
Configure Advertising Data For Periodic Advertisement¶
Advertising data for periodic advertisement is optional. It’s not needed to have periodic advertisment running.
Setup advertising data for periodic advertisement. The BLE5-Stack will then return
GAP_ADV_SET_PERIODIC_ADV_DATA_EVENT
to the application layer whether or not the adverting data are set successfully.1 // Periodic Advertising Data 2 static uint8_t periodicData[] = 3 { 4 'P', 5 'e', 6 'r', 7 'i', 8 'o', 9 'd', 10 'i', 11 'c', 12 'A', 13 'd', 14 'v' 15 }; 16 17 #define GAPADV_DATA_PERIODIC_ADV { \ 18 .operation = GAPADV_PERIODIC_ADV_DATA_COMPLETE, \ 19 .dataLength = sizeof(periodicData), \ 20 .pData = periodicData \ 21 } 22 23 GapAdv_periodicAdvData_t periodicDataParams = GAPADV_DATA_PERIODIC_ADV; 24 status = GapAdv_SetPeriodicAdvData(advHandleNCNS, &periodicDataParams);
Note
You can find a list of define made for periodic advertisement under gap_advertiser.h.
Warning
The maximum data length that is supported here is 252 bytes. Therefore, if you have a advertising data for more than 252 bytes, you will have to fragment the payload in the application layer before calling GapAdv_SetPeriodicAdvData().
For example, if you have 1000 bytes advertising data you want to send using periodic advertisement, you will have to call GapAdv_SetPeriodicAdvData() four times. The operation field for first 252 bytes needs to be set to
GAPADV_PERIODIC_ADV_DATA_FIRST_FRAG(0x01)
. The operation field for 253 ~ 504 and 505 ~ 756 bytes needs to be set toGAPADV_PERIODIC_ADV_DATA_INTERMIDIATE_FRAG (0x00)
, and the operation field for the last part of the data needs to be set toGAPADV_PERIODIC_ADV_DATA_LAST_FRAG (0x02)
.The BLE5-Stack will chain the data based on the order of GapAdv_SetPeriodicAdvData() calls.
Enable Periodic Advertisement¶
Enable periodic advertisement. The BLE5-Stack will then return
GAP_ADV_SET_PERIODIC_ADV_ENABLE_EVENT
to the application layer whether or not the periodic advertising starts successfully.1 status = GapAdv_SetPeriodicAdvEnable(1, advHandleNCNS);
Attention
Even when GapAdv_SetPeriodicAdvEnable() was called, if the non-connectable non-scannable extended advertisement is not enabled, the periodic advertisement will not start.
Disable Periodic Advertisement¶
Disable periodic advertisement. The BLE5-Stack will then return
GAP_ADV_SET_PERIODIC_ADV_ENABLE_EVENT
to the application layer whether or not the periodic advertising stops successfully.1 status = GapAdv_SetPeriodicAdvEnable(0, advHandleNCNS);
Change Advertising Data For Periodic Advertisement¶
There are two methods to change the advertising data for periodic advertisement.
If the new data is less than or equal to 252 bytes, which means operation mode =
GAPADV_PERIODIC_ADV_DATA_COMPLETE (0x3)
. Then you can just follow Configure Advertising Data For Periodic Advertisement to populate the new data.If the new data is more than 252 bytes, then you will have to disable the periodic advertisement first, please refer to Disable Periodic Advertisement and then follow Configure Advertising Data For Periodic Advertisement to populate the new data.
GAP Peripheral¶
The peripheral role is demonstrated in simple_peripheral.c and simple_peripheral.h. The Peripheral role demonstrates the use of the advertising and connection states. The steps to use this role are as follows:
Initialize the GAP parameters. This initialization should occur in the application initialization function, for example in
SimplePeripheral_init
as shown below.1 // Configure GAP 2 { 3 uint16_t paramUpdateDecision = DEFAULT_PARAM_UPDATE_REQ_DECISION; 4 5 // Pass all parameter update requests to the app for it to decide 6 GAP_SetParamValue(GAP_PARAM_LINK_UPDATE_DECISION, ¶mUpdateDecision); 7 }
Initialize the application task for the Peripheral Role and register to receive GAP events.
1 //Initialize GAP layer for Peripheral role and register to receive GAP events 2 GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, NULL);
Now you can send commands from the application. The following is an example of the application initiating PHY change using HCI_LE_SetPhyCmd().
1 // Send PHY Update 2 HCI_LE_SetPhyCmd(connHandle, allPhys, txPhy, rxPhy, phyOpts);
The following shows the software flow when the user chooses to set the PHY preference from the terminal in simple_peripheral example:
As shown in the diagram above, the actual PHY change is returned asynchronously and is passed to the application with event code HCI_BLE_PHY_UPDATE_COMPLETE_EVENT.
The application task processes most of the GAP-related events passed to it from the Bluetooth Low Energy protocol stack. For example, when a link is terminated, the application automatically restarts advertising. The following code snippet can be found in
simple_peripheral.c
:1 static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg) 2 { 3 //....... 4 case GAP_LINK_TERMINATED_EVENT: 5 { 6 //....... 7 8 // Restart advertising since there is now an active connection 9 GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0); 10 11 //....... 12 break;
GAP Scanner¶
The GAP Scanner performs Extended Scanning, Legacy Scanning and Synchronization with periodic advertisements operations as defined by the Bluetooth Core Specifications Version 5.2. It controls the Scanner GAP state (see GAP State Diagram.). The Central and Observer role uses the scanning state implemented by the GAP Scanner. The GAP Scanner is demonstrated in the simple central and simple observer example projects. The periodic advertisement synchronization capability of the GAP Scanner is demonstrated in the rtls_master example project. See the BLE Stack API Reference for the full GAP Scanner API including commands, configurable parameters, events, and callbacks. The steps to use this module are listed in the following, along with example code from simple central.
Start a Central or Observer GAP role. In this case we will use the GAP Central role.
// Initialize GAP layer for Central role and register to receive GAP events GAP_DeviceInit(GAP_PROFILE_CENTRAL, selfEntity, addrMode, NULL);
Set up a callback function for scanner events and register to gap_advertiser.h. Since the callback (in this case
SimpleCentral_scanCb()
) is called from the stack, as little processing as possible should happen in it.// Register callback to process Scanner events GapScan_registerCb(SimpleCentral_scanCb, NULL);
Set which events to pass to application.
// Set Scanner Event Mask GapScan_setEventMask(GAP_EVT_SCAN_ENABLED | GAP_EVT_SCAN_DISABLED | GAP_EVT_ADV_REPORT);
Set scan parameters. It’s worth noting that the parameters are split into PHY-related parameters (set with GapScan_setPhyParams()) and non-PHY-related parameters (set with GapScan_setParam()). Remember to set both.
Note
Make sure the scanning window is at least twice the length of the expected advertising interval to ensure at least 1 advertising event is captured in each scanning window. Otherwise, the scanning device may not find the advertising device.
// Set Scan PHY parameters
GapScan_setPhyParams(DEFAULT_SCAN_PHY, SCAN_TYPE_ACTIVE,
SCAN_PARAM_DFLT_INTERVAL, SCAN_PARAM_DFLT_INTERVAL);
Set which advertising report fields to send to the application (to the callback function, in this case SimpleCentral_scanCb()
).
// Set Advertising report fields to keep
temp16 = SC_ADV_RPT_FIELDS;
GapScan_setParam(SCAN_PARAM_RPT_FIELDS, &temp16);
Enable filter to remove duplicate advertising reports.
// Set LL Duplicate Filter
temp8 = SCAN_FLT_DUP_ENABLE;
GapScan_setParam(SCAN_PARAM_FLT_DUP, &temp8);
Set which PHY to scan on.
// Set Scanning Primary PHY
temp8 = DEFAULT_SCAN_PHY;
GapScan_setParam(SCAN_PARAM_PRIM_PHYS, &temp8);
Set scan filter to filter by PDU type.
// Set PDU type filter -
// Only 'Connectable' and 'Complete' packets are desired.
// It doesn't matter if received packets are
// Scannable or Non-Scannable, Directed or Undirected,
// Scan_Rsp's or Advertisements, and whether they are Legacy or Extended.
temp16 = SCAN_FLT_PDU_CONNECTABLE_ONLY | SCAN_FLT_PDU_COMPLETE_ONLY;
GapScan_setParam(SCAN_PARAM_FLT_PDU_TYPE, &temp16);
Start scanning. Remember to reset the number of scan results every time you start scanning.
// Scanning for DEFAULT_SCAN_DURATION x 10 ms. // The stack does not need to record advertising reports // since the application will filter them by Service UUID and save. // Reset number of scan results to 0 before starting scan numScanRes = 0; GapScan_enable(0, DEFAULT_SCAN_DURATION, 0);
The return status from the protocol stack call of GapScan_enable() indicates only whether or not the attempt to perform device discovery was successful. The actual device discovered is returned asynchronously as a
SC_EVT_ADV_REPORT
forwarded through the GAP Scanner callbacks registered by the application (here:SimpleCentral_scanCb()
). This is described below.The GAP Scanner performs some processing on the GAP events it receives from the protocol stack. The task also forwards some events to the application. Figure 70. shows this and how the
SC_EVT_ADV_REPORT
is processed from the protocol stack to the application.
Note that during scanning, individual advertisements and scan responses are
returned as SC_EVT_ADV_REPORT
.This is defined by the Bluetooth Core Specifications Version 5.2. By
default, duplicate reports are filtered such that only one event is returned to
the application per peer device BDA. This can be configured via the
SCAN_PARAM_FLT_DUP GAP Scanner parameter.
SC_EVT_SCAN_ENABLED
indicates the start of scanning. After the scan
has completed, a summary of discovered reports will be returned to the
application with SC_EVT_SCAN_DISABLED
. You can see the implementation
of this in SimpleCentral_processAppMsg()
.
The maximum amount of scan responses that can be discovered during one scan can
be set with the DEFAULT_MAX_SCAN_RES
parameter that is passed into the maxNumReport
parameter of GapScan_enable().
In an environment saturated with advertisements and scan responses, this can have a drastic impact on heap usage to the point of potentially breaking the stack. Therefore, it is essential to profile your application for the worst-case scenario where the maximum amount of scan responses are discovered during a scan.
You can change scanning parameters with GapScan_setParam(). Note that some scanning parameters will not be updated before scanning has been disabled and re-enabled. This is true for the following parameters:
SCAN_PARAM_FLT_PDU_TYPE - Filter by PDU Type
SCAN_PARAM_FLT_MIN_RSSI - Filter by Minimum RSSI
SCAN_PARAM_FLT_DISC_MODE - Filter by Discoverable Mode
SCAN_PARAM_RPT_FIELDS - Advertising Report Fields
Advertising Report Recording¶
In addition to the advertising report, the advertising report recording feature can be used to record only a certain part of the Advertising Report information without the data payload. The application can specify which fields of the Advertising Report information by using GapScan_setParam() with the parameter ID SCAN_PARAM_RPT_FIELDS and the associate bitmap. This is useful in the use case where the application is not interested in the payload of Advertising Reports thus doesn’t want to get GAP_EVT_ADV_REPORT event from GAP Scanner but needs some specific information such as address type, address, RSSI, etc.. To prepare recording, GAP Scanner allocates necessary amount of memory in GapScan_enable(). Then whenever GAP Scanner gets a new packet, it puts only the specified fields of the information in the Advertising Report List in packed form. The list is kept in RAM even after the scanning ends until the application calls GapScan_discardAdvReportList() or a new scanning starts. While the list is available, the application can retrieve the information by using GapScan_getAdvReport(). When the list gets full, GAP Scanner issues SCAN_EVT_ADV_REPORT_FULL to the application to notify that no more Advertising Report information will be recorded. How many Advertising Reports’ information have been recorded can be found in the numReport field of the data buffer of type GapScan_Evt_End_t, coming with GAP_EVT_SCAN_END event. Alternatively, if the application didn’t mask GAP_EVT_SCAN_END and doesn’t get it, GapScan_getParam() with parameter ID SCAN_PARAM_NUM_ADV_RPT can be used.
Filtering¶
The GAP Scanner module provides 5 different types of filter to reduce the amount of advertising report notifications to the application and eventually save memory and power consumption. The result of the filtering affects both advertising reports and advertising report recording. The packets filtered out by the filter configurations are discarded and will neither be reported nor recorded. The filters are set by using the API GapScan_setParam() with the following parameter IDs:
All parameter IDs are described in the following sections. The GAP Scanner allows the application to apply any combination of the individual filters at the same time to narrow the scope of packets to receive.
Filter by LL Filter Policy¶
This filter is a link layer-level filter. The associated parameter ID used in GapScan_setParam() is SCAN_PARAM_FLT_POLICY. The parameter accompanying SCAN_PARAM_FLT_POLICY is passed to the link layer when GapScan_enable() is called before actually enabling scanning. Since the filtering is done by the link layer, the application only receives advertising report events that have passed the filter. The parameter value can be one of the following:
Name |
Value |
Description |
---|---|---|
SCAN_FLT_POLICY_ALL |
0 |
Accept all Advs except directed Adv not addressed to this device. |
SCAN_FLT_POLICY_WL |
1 |
Accept only Advs from devices where the advertiser’s address is in the FIlter Accept List. |
SCAN_FLT_POLICY_ALL_RPA |
2 |
Accept all Advs except directed Adv not addressed to this device and any packet addressed to this device or addressed to a private resolvable address. |
SCAN_FLT_POLICY_WL_RPA |
3 |
Accept only Advs from devices where the advertiser’s address is in the FIlter Accept List and any packet addressed to this device or addressed to a private resolvable address. |
Filter by PDU Type¶
This filter is based on the Event_Type
parameter coming with the LE Extended
Advertising Report Event. The associated parameter ID is
SCAN_PARAM_FLT_PDY_TYPE
. The parameter value specifies packets
classified in six categories:
Connectable/Non-Connectable
Scannable/Non-Scannable
Directed/Undirected
ScanRsp/Adv
Legacy/Extended
Complete/Incomplete.
Every incoming packet has exactly one attribute in each category. For example,
SCAN_FLT_PDU_NONSCANNABLE_ONLY and
SCAN_FLT_PDU_SCANNABLE_ONLY cannot be chosen together since they
represent scannable and non-scannable packets. Only either one can be used. If
neither type is selected in a set, the filter will not care about that category.
For example, if neither SCAN_FLT_PDU_NONCONNECTABLE_ONLY nor
SCAN_FLT_PDU_CONNECTABLE_ONLY is set in the parameter value, the GAP
Scanner will notify the application of both connectable packets and
non-connectable packets. It will also record both connectable packets and
non-connectable packets. The SCAN_PARAM_FLT_PDY_TYPE
parameter value
can be any combination of the following individual values (except individual
values that are mutually exclusive):
Name |
Value |
Description |
---|---|---|
SCAN_FLT_PDU_NONCONNECTABLE_ONLY |
0x0001 |
Non-connectable packets only. Mutually exclusive with SCAN_FLT_PDU_CONNECTABLE_ONLY |
SCAN_FLT_PDU_CONNECTABLE_ONLY |
0x0002 |
Connectable packets only. Mutually exclusive with SCAN_FLT_PDU_NONCONNECTABLE_ONLY |
SCAN_FLT_PDU_NONSCANNABLE_ONLY |
0x0004 |
Non-scannable packets only. Mutually exclusive with SCAN_FLT_PDU_SCANNABLE_ONLY |
SCAN_FLT_PDU_SCANNABLE_ONLY |
0x0008 |
Scannable packets only. Mutually exclusive with SCAN_FLT_PDU_NONSCANNABLE_ONLY |
SCAN_FLT_PDU_UNDIRECTED_ONLY |
0x0010 |
Undirected packets only. Mutually exclusive with SCAN_FLT_PDU_DIRECTIED_ONLY |
SCAN_FLT_PDU_DIRECTED_ONLY |
0x0020 |
Directed packets only. Mutually exclusive with SCAN_FLT_PDU_UNDIRECTED_ONLY |
SCAN_FLT_PDU_ADV_ONLY |
0x0040 |
Advertisement packets only. Mutually exclusive with SCAN_FLT_PDU_SCANRSP_ONLY |
SCAN_FLT_PDU_SCANRSP_ONLY |
0x0080 |
Scan Response packets only. Mutually exclusive with SCAN_FLT_PDU_ADV_ONLY |
SCAN_FLT_PDU_EXTENDED_ONLY |
0x0100 |
Extended packets only. Mutually exclusive with SCAN_FLT_PDU_LEGACY_ONLY |
SCAN_FLT_PDU_LEGACY_ONLY |
0x0200 |
Legacy packets only. Mutually exclusive with SCAN_FLT_PDU_EXTENDED_ONLY |
SCAN_FLT_PDU_TRUNCATED_ONLY |
0x0400 |
Truncated packets only. Mutually exclusive with SCAN_FLT_PDU_COMPLETE_ONLY |
SCAN_FLT_PDU_COMPLETE_ONLY |
0x0800 |
Complete packets only. Mutually exclusive with SCAN_FLT_PDU_TRUNCATED_ONLY |
Filter by Minimum RSSI¶
This filter is based on the RSSI parameter coming with the LE Extended Advertising Report Event. The associated parameter ID used in GapScan_setParam() is SCAN_PARAM_FLT_MIN_RSSI. The GAP Scanner will discard LE Extended Advertising Report Event whose RSSI parameter value is smaller than the minimum RSSI value given by the application. The available range is -128 dBm to 127 dBm.
Filter by Discoverable Mode¶
This filter is based on the Flags AD
type value in the payload (in
the Data
parameter) of the LE Extended Advertising Report Event. The
associated parameter ID used in GapScan_setParam() is
SCAN_PARAM_FLT_DISC_MODE. This filter is applied after the GAP
Scanner reassembles all the fragmented payloads delivered by multiple LE
Extended Advertising Report Events. The GAP Scanner will discard the
defragmented packet if the found Flags AD type value doesn’t match the parameter
value given by the application. The parameter value can be one of the following:
Name |
Value |
Description |
---|---|---|
SCAN_FLT_DISC_NONE |
0 |
Accept only Non-Discoverable mode |
SCAN_FLT_DISC_GENERAL |
1 |
Accept only General Discoverable mode |
SCAN_FLT_DISC_LIMITED |
2 |
Accept only Limited Discoverable mode |
SCAN_FLT_DISC_ALL |
3 |
Accept both General and Limited Discoverable mode |
SCAN_FLT_DISC_DISABLE |
4 |
Discoverable Mode Filter Off (Don’t care about the Flags AD type value) |
Filter by Duplicates¶
Like the Link Layer Scanner Filter Policy, this filter is a link layer-level filter.
The associated parameter ID used in GapScan_setParam() is
SCAN_PARAM_FLT_DUP. The parameter accompanying the
SCAN_PARAM_FLT_DUP parameter ID is passed to the link layer when
GapScan_enable() internally calls LE_SetExtScanEnable
to
enable scanning. Since the filtering is done by the link layer, GAP Scanner
receives only the LE Extended Advertising Report Events that have passed the
filter. The parameter value can be one of the following:
Name |
Value |
Description |
---|---|---|
SCAN_FLT_DUP_DISABLE |
0 |
Disable duplicate filtering. |
SCAN_FLT_DUP_ENABLE |
1 |
Enable duplicate filtering. |
SCAN_FLT_DUP_RESET |
2 |
Enable duplicate filtering. Reset for each scan period. |
Warning
When the duplicate filtering is enabled, the maximum amount of devices that can be found is 16. If more than 16 devices need to be discovered, the duplicate filtering needs to be disabled.
Synchronize with a Periodic Advertising Train¶
Important
The symbol USE_PERIODIC_SCAN
must be pre-defined if you
wish to use the functions related to scanning and synchronization with
periodic advertising (for more details, please see
Bluetooth Low Energy Stack Configuration Parameters).
Additional information about periodic advertisements is provided within the section Periodic Advertising.
From a high level point of view, in order to synchronize with a periodic advertiser, the scanner has to:
Start a Central or Observer GAP role
Set up a callback function for scanner events and register to
Set which events to pass to application.
Set scan parameters
Start scanning
Identify periodic advertisers
Synchronize with a periodic advertising train
Enable the reception of the periodic advertisements
Handle the periodic advertisements reports
Disable the reception of the periodic advertisements and terminate the synchronization
The first steps are detailed at the beginning of the GAP Scanner section.
Identify periodic advertisers¶
The advertising reports for
periodic advertisements have the exact same structure and the exact same way
of reception like other advertisement types.
The actual device discovered is returned asynchronously as a
SC_EVT_ADV_REPORT
forwarded through the GAP Scanner callbacks
registered by the application (here: SimpleCentral_scanCb()
).
Periodic advertisements are non-connectable, non-scannable. By default, the
simple_central
project example filters out non-connectable
advertisements. Make sure to change this PDU filtering policy.
uint16_t temp16; // ... //temp16 = SCAN_FLT_PDU_CONNECTABLE_ONLY | SCAN_FLT_PDU_COMPLETE_ONLY; temp16 = SCAN_FLT_PDU_NONCONNECTABLE_ONLY; GapScan_setParam(SCAN_PARAM_FLT_PDU_TYPE, &temp16);
The parameter periodicAdvInt
from the structure GapScan_Evt_AdvRpt_t
will help to assess it is possible to synchronize with the advertiser.
It means this field of the advertise report has to be activated.
The same apply to the field advSid
(Advertise Set Id).
GapScan_Evt_AdvRpt_t* pAdvRpt = (GapScan_Evt_AdvRpt_t*) (pMsg->pData); if(0 != pAdvRpt->periodicAdvInt) { // this is a periodic advertisement } else { // this is NOT a periodic advertisement }
Synchronize with a periodic advertising train¶
When a periodic advertisement is identified, the synchronization can be started.
Note
The Bluetooth Core Specifications Version 5.2 (Vol 6, Part B, §4.3.5) define two ways for the scanner’s Link Layer to process advertising PDUs when attempting to synchronize to a periodic advertising train. The first policy which requires specifying the device to synchronize with. The second policy allows to synchronize with all the devices in the Periodic Advertiser List with only one scan. This is then a way to save time and energy.
Policy 1: Ignore the Periodic Advertiser List and process advertising PDUs from a specific single device
GapScan_Evt_AdvRpt_t* pAdvRpt = (GapScan_Evt_AdvRpt_t*) (pMsg->pData); if(0 != pAdvRpt->periodicAdvInt) { // this is a periodic advertisement GapScan_PeriodicAdvCreateSyncParams_t pSyncParams; pSyncParams.options = SCAN_PERIODIC_DO_NOT_USE_PERIODIC_ADV_LIST | SCAN_PERIODIC_REPORTING_INITIALLY_DISABLED; pSyncParams.advAddrType = (uint8)pAdvRpt->addrType; // only ADDRTYPE_PUBLIC and ADDRTYPE_RANDOM are allowed osal_memcpy(pSyncParams.advAddress, pAdvRpt->addr, B_ADDR_LEN); pSyncParams.skip = 0; // should be between 0 and SCAN_PERIODIC_SKIP_MAX pSyncParams.syncTimeout = 1000; // synchronization timeout for the periodic advertising train is 1000*10ms = 10s // should be between SCAN_PERIODIC_TIMEOUT_MIN and SCAN_PERIODIC_TIMEOUT_MAX pSyncParams.syncCteType = SCAN_PERIODIC_CTE_TYPE_ALL; uint8_t status = GapScan_PeriodicAdvCreateSync(pAdvRpt->advSid, &pSyncParams); if(SUCCESS != status){ // handle error } GapScan_disable(""); break; } else { // this is NOT a periodic advertisement }
Policy 2: process advertising PDUs from all devices in the Periodic Advertiser List.
This policy first requires to add one or several device(s) to the Periodic Advertiser List. This can be done using the function GapScan_AddDeviceToPeriodicAdvList()
GapScan_Evt_AdvRpt_t* pAdvRpt = (GapScan_Evt_AdvRpt_t*) (pMsg->pData); if(0 != pAdvRpt->periodicAdvInt) { // this is a periodic advertisement // add the device to the Periodic Advertiser List GapScan_AddDeviceToPeriodicAdvList((uint8)pAdvRpt->addrType, pAdvRpt->addr, pAdvRpt->advSid); // connect the devices on the Periodic Advertiser List. GapScan_PeriodicAdvCreateSyncParams_t pSyncParams; pSyncParams.options = SCAN_PERIODIC_USE_PERIODIC_ADV_LIST | SCAN_PERIODIC_REPORTING_INITIALLY_DISABLED; pSyncParams.skip = 0; // should be between 0 and SCAN_PERIODIC_SKIP_MAX pSyncParams.syncTimeout = 1000; // synchronization timeout for the periodic advertising train is 1000*10ms = 10s // should be between SCAN_PERIODIC_TIMEOUT_MIN and SCAN_PERIODIC_TIMEOUT_MAX pSyncParams.syncCteType = SCAN_PERIODIC_CTE_TYPE_ALL; uint8_t status = GapScan_PeriodicAdvCreateSync(0, &pSyncParams); if(SUCCESS != status){ // handle error } GapScan_disable(""); break; }
The functions GapScan_RemoveDeviceFromPeriodicAdvList() and GapScan_ClearPeriodicAdvList() can be used to remove device(s) from the Periodic Advertiser List.
Once the synchronization is created, a GAP_SCAN_CREATE_SYNC_EVENT
event with status SUCCESS
is issued. After this, scanning has to be
enabled in order to let the device find the periodic advertisement train
that has been specified before.
{ GapScan_PeriodicAdvEvt_t *pPkt = (GapScan_PeriodicAdvEvt_t *)pMsg; uint8_t status; if(pPkt->status == SUCCESS) { status = GapScan_enable(0, DEFAULT_SCAN_DURATION, 0); if(SUCCESS != status){ // handle error } } break; }
Enable the reception of the periodic advertisements¶
After the synchronization is established, the event
GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT
is issued. If not already done, the reception of the periodic advertisements reports has to be turned on.{ GapScan_Evt_PeriodicAdvSyncEst_t *pPkt = (GapScan_Evt_PeriodicAdvSyncEst_t *)pMsg; uint8_t status; if(pPkt->status == SUCCESS) { status = GapScan_SetPeriodicAdvReceiveEnable(pPkt->syncHandle, 0x01); if(SUCCESS != status){ // handle error } } break; }
Handle the periodic advertisements reports¶
After enabling the reception of the periodic advertisements,
the reception of a periodic advertisement leads to the generation of a
GAP_SCAN_PERIODIC_ADV_REPORT_EVENT
event.
{ GapScan_Evt_PeriodicAdvRpt_t *pPkt = (GapScan_Evt_PeriodicAdvRpt_t *)pMsg; // Handle periodic advertisement report // ... // Free report payload data if (pPkt->pData != NULL) { ICall_free(pPkt->pData); } break; }
Disable the reception of the periodic advertisements and terminate the synchronization¶
The periodic advertisement reports can be disabled using the function GapScan_SetPeriodicAdvReceiveEnable().
{ GapScan_Evt_PeriodicAdvRpt_t *pPkt = (GapScan_Evt_PeriodicAdvRpt_t *)pMsg; uint8_t status; status = GapScan_SetPeriodicAdvReceiveEnable(pPkt->syncHandle, 0x00); if(SUCCESS != status){ // handle error } break; }
Disabling the periodic advertisement reports does NOT interrupt the synchronization. In other words, the device will still wake-up and scan at each periodic advertisement. The function GapScan_PeriodicAdvTerminateSync() is used to terminate the synchronization.
{ GapScan_Evt_PeriodicAdvRpt_t *pPkt = (GapScan_Evt_PeriodicAdvRpt_t *)pMsg; uint8_t status; status = GapScan_PeriodicAdvTerminateSync(pPkt->syncHandle); if(SUCCESS != status){ // handle error } break; }
The event GAP_SCAN_TERMINATE_SYNC_EVENT will be received once the synchronization is terminated.
GAP Initiator¶
The initiator module is used to initiate the connection to a peripheral device. An initiator generally scans for advertisements then connects to a specific device. The initiator is a short lived state that transitions to the Central Role after a connection is established. Unlike the GAP Advertiser and GAP Scanner modules, GAP Initiator doesn’t have any callback function to call or to be called.
Only a device initiated with the GAP Central Role can become an initiator.
1void SimpleCentral_init(void)
2{
3 // Register with GAP for HCI/Host messages (for RSSI)
4 GAP_RegisterForMsgs(selfEntity);
5
6 // Initialize GAP layer for Central role and register to receive GAP events
7 GAP_DeviceInit(GAP_PROFILE_CENTRAL, selfEntity, addrMode, NULL);
8}
The following API is used to initiate connection to a peer device, see GapInit_connect()
1GapScan_Evt_AdvRpt_t advRpt;
2
3GapScan_getAdvReport(index, &advRpt);
4
5/*
6 * The initiating timeout is in milliseconds and will automatically cancel
7 * connection initiation if the peer is not connected. This can be set to
8 * 0 to wait indefinitely.
9 */
10uint16_t initTimeout = 500;
11
12GapInit_connect(advRpt.addrType & MASK_ADDRTYPE_ID,
13 advRpt.addr, DEFAULT_INIT_PHY, initTimeout);
If the on-going connection attempt is intended to be canceled by either timeout or a user request (the application calling GapInit_cancelConnect()), the stack notifies the application of the cancellation completion with a GAP_CONNECTING_CANCELLED_EVENT.
The initiator task will use the parameters saved for the PHY specified in the
call to GapInit_connect(). These may be set with
GapInit_setPhyParam(). Defaults are shown in gap_initiator.h
GAP Central¶
The GAP Central role is demonstrated in simple_central.c and simple_central.h. The Central role demonstrates the use of the scanning and initiating states and supports connections to peripheral devices. See the simple_central example project for an example of implementing the Central role. The steps to use this module are as follows.
Initialize the GAP and GATT parameters. This initialization should occur in the application initialization function (for example in
SimpleCentral_init
). GAP parameters can also be set in this initialization function.static void SimpleCentral_init(void) { // Initialize GATT Client VOID GATT_InitClient(); ... // Accept all parameter update requests GAP_SetParamValue(GAP_PARAM_LINK_UPDATE_DECISION, GAP_UPDATE_REQ_ACCEPT_ALL); }
Start the GAP Central role and register to receive events in the application task.
// Initialize GAP layer for Central role and register to receive GAP events GAP_DeviceInit(GAP_PROFILE_CENTRAL, selfEntity, addrMode, NULL);
GAP Connection State¶
A BLE device can be either in the Central or Peripheral role in the Connection State. After devices enter connection state, the devices exchange data under specific time within a specific time slot. This slot where the data is exchanged is called a Connection Event.
The beginning of the Connection Event is called an Anchor Point. During the connection event, the central and peripheral device will meet at the anchor point and the central will transmit the first packet, while the peripheral will have woken up to listen for the central devices transmitted packet.
Note
There is no limitation on the number of packet transactions per connection event other than MAX_NUM_PDU define in TI’s BLE5-Stack. It can either be one packet per direction or multiple packets per direction.
Connection Event Callback¶
Knowing what happened during the connection event can be beneficial for the system design. For example, by knowing which channels has higher CRC error, the application layer can decide to do a channelmap update to avoid those channels to ensure better communication. In addition to CRC error, the connection report also contains RSSI value per channel, which can be useful for Real Time Localization System (RTLS) to distinguish which channel has higher interference. For more information on RSSI based RTLS, please refer to RSSI Based Localization
TI’s BLE5-Stack provides the ability for application to obtain a detailed report of thes connection event. The report will be sent at the end of the connection event and it contains status and statistics of the most recent connection event.
The report contains the following parameters:
status - Status of the last connection event.
status
Description
GAP_CONN_EVT_STAT_SUCCESS
Both central and peripheral show up for the conenction event and exchange packets.
GAP_CONN_EVT_STAT_CRC_ERROR
Packets were exchanged but the failed at the CRC checkout.
GAP_CONN_EVT_STAT_MISSED
The peer device did not show up for the connection event.
handle - Connection event handle which is used to identify the most recent connection event when there are multilple connections per device.
channel - The RF channel which the most recent connection event used.
phy - The PHY which the most recent connection event used.
lastRssi - The RSSI value measured on the last packet of the most recent connection event.
packets - Number of packets received during the most recent connection event.
errors - Accumulated number of packets with CRC error for this connection handle.
nextTaskType - The next task the link layer is going to run.
nextTaskTime - The time to next task.
eventCounter - The event counter of the most recent connection event.
timeStamp - The anchor point of the most recent connection event.
eventType - There are 3 types of events returning from BLE5-Stack.
eventType
Description
GAP_CB_CONN_ESTABLISHED
This event is returned when connection is established. When this returns, the eventCount will be 0.
GAP_CB_PHY_UPDATE
This event is returned when last connection event received LL_PHY_UPDATE_IND packet.
GAP_CB_CONN_EVENT_ALL
This event covers the above and rest of the scenarios.
To enable the application layer to receive connection report, you can use Gap_RegisterConnEventCb().
The following code is an example of how to register connection event report for all types of event within certain connection.
1// Assuming connHandle was assigned when the connection established.
2uint16_t connHandle;
3
4Gap_RegisterConnEventCb(application_connEvtCB, GAP_CB_REGISTER, GAP_CB_CONN_EVENT_ALL, connHandle);
Connection Parameters¶
This section describes the connection parameters which are sent by the initiating device with the connection request and can be modified by either device when the connection is established. These parameters are as follows:
Connection Interval - In Bluetooth Low Energy connections, a frequency-hopping scheme is used. The two devices each send and receive data from one another only on a specific channel at a specific time. These devices meet a specific amount of time later at a new channel (the link layer of the Bluetooth Low Energy protocol stack handles the channel switching). This meeting where the two devices send and receive data is known as a
connection event
. If there is no application data to be sent or received, the two devices exchange link layer data with empty application payload to maintain the connection. The connection interval is the amount of time between two connection events in units of 1.25 ms. The connection interval can range from a minimum value of 6 (7.5 ms) to a maximum of 3200 (4.0 s). See Connection Event and Interval for more details.
Different applications may require different connection intervals. As described in Connection Parameter Considerations, these requirements affect the power consumption of the device. For more detailed information on power consumption, see the Measuring Bluetooth Smart Power Consumption Application Report (SWRA478).
Peripheral Latency - Formerly known as ‘Slave Latency’. This parameter gives the Peripheral device the option of skipping a number of connection events. This ability gives the peripheral device some flexibility. If the peripheral does not have any data to send, it can skip connection events, stay asleep, and save power. The peripheral device selects whether to wake or not on a per connection event basis. The peripheral can skip connection events but must not skip more than allowed by the Peripheral latency parameter or the connection fails. See picture below for more details.
Supervision Time-out - This time-out is the maximum amount of time between two successful connection events. If this time passes without a successful connection event, the device terminates the connection and returns to an unconnected state. This parameter value is represented in units of 10 ms. The supervision time-out value can range from a minimum of 10 (100 ms) to 3200 (32.0 s). The time-out must be larger than the effective connection interval (see Effective Connection Interval for more details).
Effective Connection Interval¶
The effective connection interval is equal to the amount of time between two connection events, assuming that the Peripheral skips the maximum number of possible events if Peripheral latency is allowed (the effective connection interval is equal to the actual connection interval if Peripheral latency is set to 0).
The Peripheral Latency value represents the maximum number of events that can be skipped. This number can range from a minimum value of 0 (meaning that no connection events can be skipped) to a maximum of 499. The maximum value must not make the effective connection interval (see the following formula) greater than 16 s. The interval can be calculated using the following formula:
Effective Connection Interval = (Connection Interval) * (1 + [Peripheral Latency])
Consider the following example:
Connection Interval: 80 (100 ms)
Peripheral Latency: 4
Effective Connection Interval: (100 ms) * (1 + 4) = 500 ms
When no data is being sent from the Peripheral to the Central, the Peripheral transmits during a connection event once every 500 ms.
Connection Parameter Considerations¶
In many applications, the Peripheral skips the maximum number of connection events. Consider the effective connection interval when selecting or requesting connection parameters. Selecting the correct group of connection parameters plays an important role in power optimization of the Bluetooth Low Energy device. The following list gives a general summary of the trade-offs in connection parameter settings.
Reducing the connection interval does as follows:
Increases the power consumption for both devices
Increases the throughput in both directions
Reduces the time for sending data in either direction
Increasing the connection interval does as follows:
Reduces the power consumption for both devices
Reduces the throughput in both directions
Increases the time for sending data in either direction
Reducing the Peripheral latency (or setting it to zero) does as follows:
Increases the power consumption for the peripheral device
Reduces the time for the peripheral device to receive the data sent from a central device
Increasing the Peripheral latency does as follows:
Reduces power consumption for the peripheral during periods when the peripheral has no data to send to the central device
Increases the time for the peripheral device to receive the data sent from the central device
Connection Parameter Update¶
In some cases, the central device requests a connection with a
peripheral device containing connection parameters that are
unfavorable to the peripheral device. In other cases, a peripheral
device might have the desire to change connection parameters in the middle of a
connection, based on the peripheral application. The peripheral
device can request the central device to change the connection
parameters by sending a Connection Parameter Update Request
.
For Bluetooth 4.1, 4.2, 5.0 and 5.1-capable devices, this request is handled directly by
the Link Layer. For Bluetooth 4.0 devices, the L2CAP layer of the
protocol stack handles the request. The Bluetooth Low Energy stack
automatically selects the update method.
The Connection Parameter Update Request
contains four parameters:
Minimum connection interval
Maximum connection interval
Peripheral latency
Supervision time-out
These values represent the parameters that the peripheral device wants for
the connection. The connection interval is given as a range. When
the central device receives the Connection Parameter Update Request
request,
it can accept or reject the new parameters.
Sending a Connection Parameter Update Request
is optional and it is not
required for the central device to accept or apply the requested
parameters. Some applications try to establish a connection at a
faster connection interval to allow for a faster service discovery
and initial setup. These applications later request a longer
(slower) connection interval for optimal power usage.
Regardless of the roles (peripheral or central), connection parameter updates can be sent asynchronously with the GAP_UpdateLinkParamReq() command. The simple_peripheral application can be configured to automatically send a parameter update a certain amount of time after establishing a connection. An example is provided in the simple_peripheral application, which sends a connection parameter update upon a connection by default.
Note
To change or modify the default connection parameter update settings, open the project’s SysConfig file. Navigate to BLE → Peripheral Configuration. Here you can modify the Connection Update Request Params to configure the symbols below. If desired, you can also turn off the default connection parameter update by unchecking `Send Parameter Update Request`.
By default, the following symbols are generated by the SysConfig tool:
// Pass parameter updates to the app for it to decide.
#define DEFAULT_SEND_PARAM_UPDATE_REQ
// Delay (in ms) after connection establishment before sending a parameter update requst
#define SEND_PARAM_UPDATE_DELAY 6000
// Minimum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 400
// Maximum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 800
// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_DESIRED_SLAVE_LATENCY 0
// Supervision timeout value (units of 10ms) if automatic parameter update
// request is enabled
#define DEFAULT_DESIRED_CONN_TIMEOUT 600
In simple_peripheral, six seconds after a connection is established the application automatically sends a GAP Update Link Parameter Request:
1 static void SimplePeripheral_processParamUpdate(uint16_t connHandle)
2 {
3 gapUpdateLinkParamReq_t req;
4 uint8_t connIndex;
5
6 req.connectionHandle = connHandle;
7 #ifdef DEFAULT_SEND_PARAM_UPDATE_REQ
8 req.connLatency = DEFAULT_DESIRED_SLAVE_LATENCY;
9 req.connTimeout = DEFAULT_DESIRED_CONN_TIMEOUT;
10 req.intervalMin = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
11 req.intervalMax = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
12 #endif
13
14 //...
15
16 // Send parameter update
17 bStatus_t status = GAP_UpdateLinkParamReq(&req);
When the peer device receives this update request, the GAP parameter GAP_PARAM_LINK_UPDATE_DECISION determines how it responds. See GAP Peripheral for an explanation of how this parameter is configured.
Connection Termination¶
Either the Central or the Peripheral can terminate a connection for any reason. One side initiates termination and the other side must respond before both devices exit the connected state. Use the GAP_TerminateLinkReq() command to terminate an existing connection.