CC26XX specific ITM implementation.
This file should only be included in the board file to fill out the object and hwAttrs structures
The CC26XX is capable of treating the pins used by the SWO interface as GPIOs. This means that the pins must be managed by the ITM driver when not in use by the TPIU.
Go to the source code of this file.
Data Structures | |
struct | ITMCC26XX_HWAttrs |