48 #if !defined ( GAP_BONDINGS_MAX ) 49 #define GAP_BONDINGS_MAX 10 53 #if !defined ( GAP_CHAR_CFG_MAX ) 54 #define GAP_CHAR_CFG_MAX 4 78 #define GAPBOND_PAIRING_MODE 0x400 89 #define GAPBOND_MITM_PROTECTION 0x402 100 #define GAPBOND_IO_CAPABILITIES 0x403 111 #define GAPBOND_OOB_ENABLED 0x404 123 #define GAPBOND_OOB_DATA 0x405 134 #define GAPBOND_BONDING_ENABLED 0x406 148 #define GAPBOND_KEY_DIST_LIST 0x407 155 #define GAPBOND_ERASE_ALLBONDS 0x409 158 #define GAPBOND_AUTO_FAIL_PAIRING 0x40A 159 #define GAPBOND_AUTO_FAIL_REASON 0x40B 171 #define GAPBOND_KEYSIZE 0x40C 186 #define GAPBOND_AUTO_SYNC_WL 0x40D 195 #define GAPBOND_BOND_COUNT 0x40E 207 #define GAPBOND_BOND_FAIL_ACTION 0x40F 221 #define GAPBOND_ERASE_SINGLEBOND 0x410 236 #define GAPBOND_SECURE_CONNECTION 0x411 256 #define GAPBOND_ECCKEY_REGEN_POLICY 0x412 279 #define GAPBOND_ECC_KEYS 0x413 290 #define GAPBOND_SC_HOST_DEBUG 0x414 308 #define GAPBOND_ERASE_BOND_IN_CONN 0x415 327 #define GAPBOND_ALLOW_DEBUG_KEYS 0x416 342 #define GAPBOND_LRU_BOND_REPLACEMENT 0x418 352 #define GAPBOND_ERASE_LOCAL_INFO 0x41A 363 #define GAPBOND_AUTHEN_PAIRING_ONLY 0x41B 375 #define GAPBOND_SAME_IRK_OPTION 0x41C 388 #define GAPBOND_PAIRING_MODE_NO_PAIRING 0x00 390 #define GAPBOND_PAIRING_MODE_WAIT_FOR_REQ 0x01 392 #define GAPBOND_PAIRING_MODE_INITIATE 0x02 400 #define GAPBOND_IO_CAP_DISPLAY_ONLY 0x00 402 #define GAPBOND_IO_CAP_DISPLAY_YES_NO 0x01 404 #define GAPBOND_IO_CAP_KEYBOARD_ONLY 0x02 406 #define GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT 0x03 408 #define GAPBOND_IO_CAP_KEYBOARD_DISPLAY 0x04 416 #define GAPBOND_KEYDIST_SENCKEY 0x01 418 #define GAPBOND_KEYDIST_SIDKEY 0x02 420 #define GAPBOND_KEYDIST_SSIGN 0x04 422 #define GAPBOND_KEYDIST_SLINK 0x08 424 #define GAPBOND_KEYDIST_MENCKEY 0x10 426 #define GAPBOND_KEYDIST_MIDKEY 0x20 428 #define GAPBOND_KEYDIST_MSIGN 0x40 430 #define GAPBOND_KEYDIST_MLINK 0x80 438 #define GAPBOND_SAME_IRK_UPDATE_BOND_REC 0x00 440 #define GAPBOND_SAME_IRK_TERMINATE_LINK 0x01 478 #define GAP_BOND_REC_ID_OFFSET 0 479 #define GAP_BOND_LOCAL_LTK_OFFSET 1 480 #define GAP_BOND_DEV_LTK_OFFSET 2 481 #define GAP_BOND_DEV_IRK_OFFSET 3 482 #define GAP_BOND_DEV_CSRK_OFFSET 4 483 #define GAP_BOND_DEV_SIGN_COUNTER_OFFSET 5 484 #define GAP_BOND_REC_IDS 6 487 #define GAP_BONDED_STATE_AUTHENTICATED 0x01 488 #define GAP_BONDED_STATE_SERVICE_CHANGED 0x02 489 #define GAP_BONDED_STATE_CAR 0x04 490 #define GAP_BONDED_STATE_SECURECONNECTION 0x08 491 #define GAP_BONDED_STATE_RPA_ONLY 0x10 510 #define GAPBOND_PAIRING_STATE_STARTED 0x00 531 #define GAPBOND_PAIRING_STATE_COMPLETE 0x01 550 #define GAPBOND_PAIRING_STATE_ENCRYPTED 0x02 551 #define GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 553 #define GAPBOND_PAIRING_STATE_CAR_READ 0x04 555 #define GAPBOND_PAIRING_STATE_RPAO_READ 0x05 557 #define GAPBOND_GENERATE_ECC_DONE 0x06 574 #define SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED 0x01 575 #define SMP_PAIRING_FAILED_OOB_NOT_AVAIL 0x02 581 #define SMP_PAIRING_FAILED_AUTH_REQ 0x03 582 #define SMP_PAIRING_FAILED_CONFIRM_VALUE 0x04 584 #define SMP_PAIRING_FAILED_NOT_SUPPORTED 0x05 590 #define SMP_PAIRING_FAILED_ENC_KEY_SIZE 0x06 591 #define SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED 0x07 593 #define SMP_PAIRING_FAILED_UNSPECIFIED 0x08 599 #define SMP_PAIRING_FAILED_REPEATED_ATTEMPTS 0x09 604 #define SMP_PAIRING_FAILED_INVALID_PARAMETERS 0x0A 609 #define SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED 0x0B 614 #define SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED 0x0C 621 #define GAPBOND_FAIL_NO_ACTION 0x00 623 #define GAPBOND_FAIL_INITIATE_PAIRING 0x01 625 #define GAPBOND_FAIL_TERMINATE_LINK 0x02 631 #define GAPBOND_FAIL_TERMINATE_ERASE_BONDS 0x03 638 #define GAPBOND_SECURE_CONNECTION_NONE 0x00 640 #define GAPBOND_SECURE_CONNECTION_ALLOW 0x01 642 #define GAPBOND_SECURE_CONNECTION_ONLY 0x02 654 #define GAPBOND_REGENERATE_ALWAYS 0x00 656 #define GAPBOND_REGENERATE_NEVER 0xFF 660 #define ECC_KEYLEN 32 695 uint16_t connectionHandle,
698 uint32_t numComparison
714 uint16_t connectionHandle,
747 typedef struct gapBondOOBData
890 uint8_t *pIdentityAddr);
922 uint8_t status, uint32_t passcode);
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:727
Public and Private ECC Keys.
Definition: gapbondmgr.h:739
bStatus_t GAPBondMgr_Pair(uint16_t connHandle)
#define B_RANDOM_NUM_SIZE
BLE Random Number Size.
Definition: bcomdef.h:133
Structure of NV data for the connected device's encryption information.
Definition: gapbondmgr.h:754
bStatus_t GAPBondMgr_GenerateEccKeys(void)
Generates ECC keys.
bStatus_t GAPBondMgr_GetParameter(uint16_t param, void *pValue)
bStatus_t GAPBondMgr_PasscodeRsp(uint16_t connectionHandle, uint8_t status, uint32_t passcode)
void(* pfnPairStateCB_t)(uint16_t connectionHandle, uint8_t state, uint8_t status)
Definition: gapbondmgr.h:713
bStatus_t GAPBondMgr_SCGetLocalOOBParameters(gapBondOOBData_t *localOobData)
Get local Random number and confirm value for secure connection.
Structure of NV data for the connected device's address information.
Definition: gapbondmgr.h:763
pfnPasscodeCB_t passcodeCB
Passcode callback.
Definition: gapbondmgr.h:727
bStatus_t GAPBondMgr_FindAddr(uint8_t *pDevAddr, GAP_Peer_Addr_Types_t addrType, uint8_t *pIdx, GAP_Peer_Addr_Types_t *pIdentityAddrType, uint8_t *pIdentityAddr)
Search for an address in the bonding table. If the address is a random private resolvable address...
void GAPBondMgr_Register(gapBondCBs_t *pCB)
Definition: gapbondmgr.h:725
void(* pfnPasscodeCB_t)(uint8_t *deviceAddr, uint16_t connectionHandle, uint8_t uiInputs, uint8_t uiOutputs, uint32_t numComparison)
Definition: gapbondmgr.h:693
uint8_t gapBondMgrImportBond(gapBondRec_t *pBondRec, gapBondLTK_t *pLocalLtk, gapBondLTK_t *pDevLtk, uint8_t *pIRK, uint8_t *pSRK, uint32_t signCount, gapBondCharCfg_t *charCfg)
Import bond record to NV.
uint8_t gapBondMgrReadBondRec(GAP_Peer_Addr_Types_t addrType, uint8_t *pDevAddr, gapBondRec_t *pBondRec, gapBondLTK_t *pLocalLtk, gapBondLTK_t *pDevLtk, uint8_t *pIRK, uint8_t *pSRK, uint32_t signCount, gapBondCharCfg_t *charCfg)
Read bond record from NV.
uint8_t stateFlags
Definition: gapbondmgr.h:781
bStatus_t GAPBondMgr_ServiceChangeInd(uint16_t connectionHandle, uint8_t setParam)
GAP_Peer_Addr_Types_t addrType
Definition: gapbondmgr.h:775
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
bStatus_t GAPBondMgr_SetParameter(uint16_t param, uint8_t len, void *pValue)
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:251
#define ECC_KEYLEN
ECC Key Length: 256 bit keys.
Definition: gapbondmgr.h:661
bStatus_t GAPBondMgr_SCSetRemoteOOBParameters(gapBondOOBData_t *remoteOobData, uint8 OOBDataFlag)
Set remote's OOB parameters for secure connection.
#define KEYLEN
Default key length.
Definition: bcomdef.h:111
pfnPairStateCB_t pairStateCB
Pairing state callback.
Definition: gapbondmgr.h:728
Structure of NV data for the connected device's characteristic configuration.
Definition: gapbondmgr.h:785