![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.02.06.00
|
Data Fields | |
| uint16_t | connectionHandle |
| Connection handle. | |
| uint8_t | deviceAddr [B_ADDR_LEN] |
| address of device to pair with, and could be either public or random. | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status | |
| uint32_t | numComparison |
| Numeric Comparison value to be displayed. | |
| uint8_t | opcode |
| GAP_PASSKEY_NEEDED_EVENT | |
| uint8_t | uiInputs |
| Pairing User Interface Inputs - Ask user to input passcode. | |
| uint8_t | uiOutputs |
| Pairing User Interface Outputs - Display passcode. | |
GAP_PASSKEY_NEEDED_EVENT message format.
This message is sent to the app when a Passkey is needed from the app's user interface.
This event will be consumed by the gapbondmgr if it exists.