103 #ifndef ti_drivers_UDMACC26XX__include 104 #define ti_drivers_UDMACC26XX__include 112 #include <ti/devices/DeviceFamily.h> 113 #include DeviceFamily_constructPath(inc/hw_types.h) 114 #include DeviceFamily_constructPath(driverlib/udma.h) 149 #if !defined(UDMACC26XX_CONFIG_BASE) && (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2) 154 #define UDMACC26XX_CONFIG_BASE 0x20001800 155 #elif !defined(UDMACC26XX_CONFIG_BASE) && (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X1_CC26X1 || \ 156 DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 161 #define UDMACC26XX_CONFIG_BASE 0x20000400 162 #elif !defined(UDMACC26XX_CONFIG_BASE) 163 #define UDMACC26XX_CONFIG_BASE 0x20000400 167 #if (UDMACC26XX_CONFIG_BASE & 0x3FF) 168 #error "Base address for DMA control table 'UDMACC26XX_CONFIG_BASE' must be 1024 bytes aligned." 172 #if defined(__IAR_SYSTEMS_ICC__) 173 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 174 __no_init static volatile tDMAControlTable ENTRY_NAME @UDMACC26XX_CONFIG_BASE + \ 175 CHANNEL_INDEX * sizeof(tDMAControlTable) 176 #elif defined(__TI_COMPILER_VERSION__) || defined(__clang__) 177 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 178 static volatile tDMAControlTable ENTRY_NAME \ 179 __attribute__((retain, location(UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable)))) 180 #elif defined(__GNUC__) 181 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 182 extern int UDMACC26XX_##ENTRY_NAME##_is_placed; \ 183 __attribute__((section("." #ENTRY_NAME))) static volatile tDMAControlTable ENTRY_NAME = { \ 184 &UDMACC26XX_##ENTRY_NAME##_is_placed} 186 #error "don't know how to define ALLOCATE_CONTROL_TABLE_ENTRY for this toolchain" 190 #define UDMACC26XX_SET_TRANSFER_SIZE(SIZE) (((SIZE - 1) << UDMA_XFER_SIZE_S) & UDMA_XFER_SIZE_M) 192 #define UDMACC26XX_GET_TRANSFER_SIZE(CONTROL) (((CONTROL & UDMA_XFER_SIZE_M) >> UDMA_XFER_SIZE_S) + 1) 314 HWREG(hwAttrs->
baseAddr + UDMA_O_SETCHANNELEN) = channelBitMask;
343 return (uDMAIntStatus(hwAttrs->
baseAddr) & channelBitMask) ?
true :
false;
371 uDMAIntClear(hwAttrs->
baseAddr, channelBitMask);
398 HWREG(hwAttrs->
baseAddr + UDMA_O_CLEARCHANNELEN) = channelBitMask;
428 uDMAChannelAttributeDisable(hwAttrs->
baseAddr, channelNum, attr);
bool isOpen
Definition: UDMACC26XX.h:199
HwiP_Struct hwi
Definition: UDMACC26XX.h:200
void UDMACC26XX_hwiIntFxn(uintptr_t callbacks)
PowerCC26XX_Resource powerMngrId
Definition: UDMACC26XX.h:209
void UDMACC26XX_close(UDMACC26XX_Handle handle)
Function to close the DMA driver.
UDMACC26XX_Handle UDMACC26XX_open(void)
Function to initialize the CC26XX DMA peripheral.
__STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:363
__STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:306
uint8_t intNum
Definition: UDMACC26XX.h:210
__STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
Function to initialize the CC26XX DMA driver.
Definition: UDMACC26XX.h:265
__STATIC_INLINE void UDMACC26XX_disableAttribute(UDMACC26XX_Handle handle, uint32_t channelNum, uint32_t attr)
Definition: UDMACC26XX.h:421
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:239
Power manager interface for CC26XX/CC13XX.
UDMACC26XX hardware attributes.
Definition: UDMACC26XX.h:206
void * object
Definition: UDMACC26XX.h:241
uint8_t intPriority
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority...
Definition: UDMACC26XX.h:233
__STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:391
__STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:335
uint32_t baseAddr
Definition: UDMACC26XX.h:208
UDMACC26XX object.
Definition: UDMACC26XX.h:197
UDMACC26XX_Config * UDMACC26XX_Handle
A handle that is returned from a UDMACC26XX_open() call.
Definition: UDMACC26XX.h:248
void const * hwAttrs
Definition: UDMACC26XX.h:242