TI BLE5-Stack API Documentation  2.02.07.00
Modules | Files
HCI Function Maps

Modules

 HCI Constants
 
 HCI Event API Parameters
 
 RF Setup PHY Parameters
 

Files

file  hci.h
 HCI layer interface.
 

Detailed Description

HCI Function Mapping

This section lists the mapping between stack APIs and function names, as described in the BT core spec for commands that the application can call and receive a \ corresponding event. no.

API Function Map
Stack API BT Function
HCI_HostNumCompletedPktCmd Host Number Of Completed Packets Command
HCI_LE_AddDeviceToResolvingListCmd LE Add Device to Resolving List Command
HCI_LE_AddWhiteListCmd LE Add Device To White List Command
HCI_LE_ClearWhiteListCmd LE Clear White List Command
HCI_LE_EncryptCmd LE Encrypt Command
HCI_LE_RandCmd LE Rand Command
HCI_LE_ReadBufSizeCmd LE Read Buffer Size Command
HCI_LE_ReadChannelMapCmd LE Read Channel Map Command
HCI_LE_ReadLocalResolvableAddressCmd LE Read Local Resolvable Address Command
HCI_LE_ReadLocalSupportedFeaturesCmd Read Local Supported Commands Command
HCI_LE_ReadMaxDataLenCmd LE Read Maximum Data Length Command
HCI_LE_ReadPeerResolvableAddressCmd LE Read Peer Resolvable Address Command
HCI_LE_ReadResolvingListSizeCmd LE Read Resolving List Size Command
HCI_LE_ReadSuggestedDefaultDataLenCmd LE Read Suggested Default Data Length Command
HCI_LE_ReadSupportedStatesCmd LE Read Supported States Command
HCI_LE_ReadWhiteListSizeCmd LE Read White List Size Command
HCI_LE_RemoveDeviceFromResolvingListCmd LE Remove Device From Resolving List Command
HCI_LE_RemoveWhiteListCmd LE Remove Device From White List Command
HCI_LE_SetDataLenCmd LE Set Data Length Command
HCI_LE_SetEventMaskCmd LE Set Event Mask Command
HCI_LE_SetHostChanClassificationCmd LE Set Host Channel Classification Command
HCI_LE_SetResolvablePrivateAddressTimeoutCmd LE Set Resolvable Private Address Timeout Command
HCI_LE_SetPrivacyModeCmd LE Set Privacy Mode Command
HCI_LE_TestEndCmd LE Test End Command
HCI_LE_TransmitterTestCmd LE Transmitter Test Command
HCI_LE_WriteSuggestedDefaultDataLenCmd LE Write Suggested Default Data Length Command
HCI_ReadAuthPayloadTimeoutCmd Read Authenticated Payload Timeout Command
HCI_ReadBDADDRCmd Read BD_ADDR Command
HCI_ReadLocalSupportedCommandsCmd Read Local Supported Commands Command
HCI_ReadLocalSupportedFeaturesCmd Read Local Supported Features Command
HCI_ReadLocalVersionInfoCmd Read Local Version Information Command
HCI_ReadRssiCmd Read RSSI Command
HCI_ReadTransmitPowerLevelCmd Read Transmit Power Level Command
HCI_ResetCmd Reset Command
HCI_SetEventMaskCmd Set Event Mask Command
HCI_SetEventMaskPage2Cmd Set Event Mask Page 2 Command
HCI_LE_ReadTxPowerCmd LE Read Tx Power Command
HCI_LE_ReadRfPathCompCmd LE Read Rf Path Compensation Command
HCI_LE_WriteRfPathCompCmd LE Write Rf Path Compensation Command

This section lists the mapping between stack APIs and function names, as described in the Vendor Specific API guide included with the installer.

Vendor Specific API Function Map
Stack API Vendor Specific Function
HCI_EXT_BuildRevisionCmd HCI Extension Build Revision
HCI_EXT_DecryptCmd HCI Extension Decrypt
HCI_EXT_DisconnectImmedCmd HCI Extension Disconnect Immediate
HCI_EXT_EnhancedModemHopTestTxCmd HCI Extension Enhanced Modem Hop Test Transmit
HCI_EXT_EnhancedModemTestRxCmd HCI Extension Enhanced Modem Test Receive
HCI_EXT_EnhancedModemTestTxCmd HCI Extension Enhanced Modem Test Transmit
HCI_EXT_EnablePTMCmd HCI Extension Enable PTM
HCI_EXT_EndModemTestCmd HCI Extension End Modem Test
HCI_EXT_ModemHopTestTxCmd HCI Extension Modem Hop Test Transmit
HCI_EXT_ModemTestRxCmd HCI Extension Modem Test Receive
HCI_EXT_ModemTestTxCmd HCI Extension Modem Test Transmit
HCI_EXT_NumComplPktsLimitCmd HCI Extension Number Completed Packets Limit
HCI_EXT_OnePktPerEvtCmd HCI Extension One Packet Per Event
HCI_EXT_PacketErrorRateCmd HCI Extension Packet Error Rate
HCI_EXT_PERbyChanCmd HCI Extension Packet Error Rate By Channel
HCI_EXT_SaveFreqTuneCmd HCI Extension Save Frequency Tuning
HCI_EXT_SetFastTxResponseTimeCmd HCI Extension Set Fast Transmit Response Time
HCI_EXT_SetFreqTuneCmd HCI Extension Set Frequency Tuning
HCI_EXT_SetLocalSupportedFeaturesCmd HCI Extension Set Local Supported Features
HCI_EXT_SetMaxDataLenCmd HCI Extension Set Max Data Length
HCI_EXT_SetMaxDtmTxPowerCmd HCI Extension Set Max DTM Transmitter Power
HCI_EXT_SetRxGainCmd HCI Extension Set Receiver Gain
HCI_EXT_SetSCACmd HCI Extension Set SCA
HCI_EXT_SetTxPowerCmd HCI Extension Set Transmitter Power
HCI_EXT_SetDtmTxPktCntCmd HCI Extension Set DTM Transmitter Packet Count
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale