DMM 15.4 Collector + BLE Remote Display

Table of Contents

Introduction

The dmm_154collector_remote_display project showcases a dynamic multi-protocol example which enables concurrent proprietary 802.15.4g frequency hopping (WiSUN FAN) and BLE5. This example implements an IEEE 802.15.4g Wireless Network with a BLE Remote Display, using TI's DMM (Dynamic Multi-protocol Manager) to enable the multi-protocol and dual band features of the CC13x2/CC26x2 devices.

The BLE remote display allows a smartphone application to commission the IEEE 802.15.4g network with the collector and to see connected sensor data on the IEEE 802.15.4g Wireless Network.

This project has the following app configuration available:

App Build Configuration Description
FlashROM_Release (default) All TI-RTOS debug features disabled but application-logging to UART remains enabled.
The application uses the config file ble_release.cfg and the defines are in <app name>_FlashROM_Release.opt.

All application configurations use the stack library configuration, FlashROM_Library. This build configuration will yield additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Stack Library Configuration section of the BLE5-Stack User's Guide provided in the SDK.

This document discusses the procedure for using the DMM 15.4 Collector Remote Display application when the FlashROM_Release configuration is used.

Hardware Prerequisites

The default Simple Peripheral configuration uses the LAUNCHXL-CC1352R1. This hardware configuration is shown in the below image:

For custom hardware, see the Running the SDK on Custom Hardware section of the BLE5-Stack User's Guide.

Software Prerequisites

For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the dependencies section of the Release Notes located in the root folder of the SDK.

For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack Quick Start Guide.

Note: If you are running an OAD example, be sure to first build and flash a BIM project located in /examples/nortos/<BOARD>/bim. For more instructions on how to do this, please refer to the BLE5-Stack Quick Start Guide.

Dynamic Multi-protocol Manager

The DMM uses 2 main components to dynamically arbitrate the RF resource.

TI CC1352 devices are capable of dual band operation, the CC1352 Launchpad (TI development platform) has a dual band antenna which performs well in the 868/916MHz band as well as the 2.4GHz band. Using the DMM on a CC1352 device enables not only multi protocol, but also dual band. The below diagram shows how the DMM allows 2 stacks to run on the same device, which was previously only possible on 2 devices. In the diagram the Stack 1 is shown functioning along side Stack 2, this could be a BLE stack and a proprietary Sub1G stack (called Wireless Sensor Network) or a 15.4 Stack. The Stacks used are defined by the developer.

Single mode setup:

DMM Setup:

The DMM makes scheduling decisions based on Application Level information, Stack Level information, and the Global Priority Table (GPT).

The Stack Level information is embedded in each RF command and it includes: Start Type, Start Time, AllowDelay, Priority, Activity, etc.

The Global Priority Table (GPT) defines relative priorities of the two stacks based on the activity and priority of RF commands. For details of the GPT, refer to <SDK_DIR>\source\ti\common\dmm\dmm_priority_ble_154collector.c/h.

The Application Level information is the user defined information via the policy table and inludes: Application State Name, Weight, AppliedActivity, Pause, etc; the policy table can have multiple policies. A policy defines a specific state of the DMM application where the user wants to apply different priority based on an action. A simplified policy table is shown below, it defines the behavior when Stack 1 is performing an OAD and does not take into account the specific state of the stack 2 (i.e. any state). It specifies that when Stack 1 is in an OAD state, the priority of the BLE_CONNECTION, in this case, is increased by 25. If any RF scheduling conflicts happen during the OAD, they will be resolved by taking into account the modified priority defined in the policy.

Stack 1 State Name Stack 2 State Name Weight Applied Activity Description
OAD Any 25 CONNECTION Increase the priority of CONNECTION activity of Stack 1 by 25 during OAD operation

The policy used in this example is more complex than the illustration above. For details of the actual policy used refer to <SDK_DIR>\source\ti\common\dmm\policy.h and ti_dmm_application_policy.c/h as generated by the SysConfig tool.

The DMM also supports pausing/resuming stacks based on a policy change. This is achieved by an application callback, which is called from the DMM policy manager when a policy change requiring a stack to pause operation is entire. An example of pausing the Zigbee stack during a BLE_OAD is provided in the DMM Zigbee Coordinator Switch + BLE OAD example.

Note: The DMM Collector + BLE OAD example does not currently pause the 15.4 stack during an OAD.

See the DMM chapter in your protocol stack user's guide for more information about DMM.

Usage

Note: This example should be used in conjunction with one or more 15.4 Stack Sensor(s). The 15.4 Sensor(s) must be built with the same 15.4 mode setting, as configured with the SysConfig tool.

This application uses the UART peripheral to provide an interface for the application.

This document will use PuTTY to serve as the display for the output of the CC1352 LaunchPad. The LightBlue smartphone application will act as the BLE Central device that will connect to the Remote Display service in this example. The LightBlue smartphone application is available on the App Store and Google Play. Note that any other serial terminal and smartphone BLE scanner application may be used. The following default parameters are used for the UART peripheral for display:

UART Parameter Default Values
Baud Rate 115200
Data length 8 bits
Parity None
Stop bits 1 bit
Flow Control None

Note: If you are using a smartphone as the BLE central device and the same CC1352 LaunchPad was used previously with a different DMM or BLE example then you may need to forget the device in the smartphone BLE settings, then disable and enable BLE. Not doing this could result in the smartphone application displaying incorrect services and characteristics.

Once the 15.4 Collector Remote Display application starts, the output to the terminal will report its BLE address and the fact that it is advertising which is enabled by default upon startup, as shown below:

The Sensor should be showing:

BLE Services Overview

This project contains 3 services:

The characteristic UUID is a 128b value, with 16b that are used to specify the characteristic. The below shows the format of the 128b UUID:

0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xB0, 0x00, 0x40, 0x51, 0x04, LOW BYTE OF UUID, HIGH  BYTE OF UUID, 0x00, 0xF0

Provisioning Service/Profile Table

The provisioning profile is defined in software_stacks/ble_stack/profiles/provisioning_gatt_profile.c

The Characteristics and properties are shown below.

Characteristic UUID Format Properties
Network PAN ID 1191 2 Byte Integer Auth Read/Write
Extended Network PAN ID 1192 8 Byte Integer Auth Read/Write
Collector Operating Frequency 1193 1 Byte Integer Auth Read/Write
Collector Operating Channels 1194 17 Byte Integer Auth Read/Write
IEEE FFD address 1195 8 Byte Integer Auth Read/Write
Network Security Key 1196 16 Byte Integer Auth Read/Write
Provision Collector 1197 1 Byte Integer Auth Read/Write
Collector Provisioning State 1198 1 Byte Integer Auth Read

Collector Service/Profile Table

The collector service profile is defined in software_stacks/ble_stack/profiles/remote_display_gatt_profile.c

The Characteristics and properties are shown below.

Characteristic UUID Format Properties
Sensor Address 1181 2 Byte Integer Read/Notify
Sensor Report Interval 1182 4 Byte Integer Write
Toggle LED 1183 1 Byte Integer Read/Write
Disassociate Sensor 1184 2 Byte Integer Read/Write

Network Device Service/Profile Table

The network device service profile is defined in software_stacks/ble_stack/profiles/network_device_gatt_profile.c

The Characteristics and properties are shown below.

Characteristic UUID Format Properties
Network Device 11B1 7 Byte Integer Write/Notify

Using the Common User Interface

The Common User Interface (CUI) controls the access to User Interface resources. On a LaunchPad device, these resources are made up of Buttons, LEDs and UART I/O.

Using a UART terminal with the configuration described above, use the arrow keys to navigate the menu. Upon startup, pressing the ENTER key will display the HELP menu, as shown below:

To demonstrate the use of the CUI, let us change the BLE PHY. First, use the arrow keys to select the TI Remote Display menu. Pressing the ENTER key will take us to the TI Remote Display menu. Next, we see the option to CONFIGURE or go BACK to the previous menu. Make sure CONFIGURE is selected and hit the ENTER key to enter the CONFIGURE menu. Here, we have the option to SET PHY. After pressing ENTER once more, we can select a PHY. Chose the 2M PHY. You should see confirmation of this on the UART display, as shown below.

Note: When using the CUI, the buttons on the LaunchPad should not be used to navigate the CUI menu. These buttons perform other actions as described in the following section.

Provisioning the 15.4 Network

Before the user can connect any sensors to the 15.4 network, the network must be provisioned, followed by opening the network to allow new sensors to join the network.

The user has 3 choices regarding the provisioning of the 15.4 Network:

Note: The UART terminal output will be similar regardless of which method is used to provision the network and control the connected sensors.

Provisioning the 15.4 Network via BLE

To provision the device using BLE use LightBlue to scan for the device, you should see a device with the name of "DMM 15.4 COLLEC RD" (note that the navigation might be slightly different depending on your mobile application):

If there is more than 1 device called Node Remote Display, the RSSI value under the strength bars on the left can be used to find which device you are trying to connect to. Select "DMM 15.4 Collector RD" to connect to the device. When prompted enter the pairing code "123456".

Once connected, the terminal window will show the address of the connected device (smartphone):

In LightBlue, you should be able to see various information about the Node Remote Display device:

You should see the provisioning service, which is labeled as "UUID: F0001190-0451-B000-000000000000" (this may be slightly different for other smartphone applications). Under this service there should be the following characteristics shown:

The following sections detail the functions and operations of each of the characteristics.

Network PAN ID Characteristic (UUID: 1191)

This characteristic sets PAN ID of the 15.4 network. This is the same as setting CONFIG_PAN_ID as configured with the SysConfig Tool.

Setting CONFIG_PAN_ID or Node Data Characteristic to 0xFFFF (the default) on the Collector allows it to join any network, setting it to a specific valeue forces it to only join a network with that PAN ID. Setting CONFIG_PAN_ID to 0xFFFF on the Collector allows it to form a network with a random PAN ID, setting it to a specific value forces it to form a network with that specific PAN ID.

Collector Operating Channels Characteristic (UUID: 1194)

This characteristic sets the Channel mask that the 15.4 Collector will use to find a network. This is the same as setting CONFIG_CHANNEL_MASK, CONFIG_FH_CHANNEL_MASK and FH_ASYNC_CHANNEL_MASK as configured with the SysConfig Tool.

To successfully discover and join a network the same setting must be used on the Sensor and Collector.

Network Security Key Characteristic (UUID: 1196)

This characteristic sets security key that the 15.4 sensor will use encrypt and decrypt 15.4 packet data payload. This is the same as setting KEY_TABLE_DEFAULT_KEY in the Collector as configured with the SysConfig Tool.

To successfully communicate with connected sensors, the Network Security Key Characteristic must be set the same as the Collector KEY_TABLE_DEFAULT_KEY as configured with the SysConfig Tool.

Provision Collector Characteristic (UUID: 1197)

This characteristic is used to start the IEEE 802.15.4g network and open/close the network to allow sensors to join. These commands are defined in provisioning_gatt_profile.h.

Writing the value 0xAA to this characteristic will start the IEEE 802.15.4g network using the provisioning settings.

Writing the value 0x55 to this characteristic will open the IEEE 802.15.4g network and allow sensors to join the network.

Writing the value 0xCC to this characteristic will close the IEEE 802.15.4g network and block new sensors from joining the network.

Note: All the above provisioning characteristics default to those configured with the SysConfig Tool. The characteristics only need to be written to if the user requires to change them from the defaults.

Note: In FH mode, the BLE connection may drop while new sensors associate to the IEEE 802.15.4g network. The BLE connection can be resumed once the 15.4 Sensor is associated to a 15.4 network, and full concurrent IEEE 802.15.4g Frequency Hopping and BLE advertisements or connection can be demonstrated.

Collector Provisioning State (UUID: 1198)

This characteristic is used to read the Collector's IEEE 802.15.4g network state. The following states will be observed:

Provisioning the 15.4 Network via CUI

To provision the device using the CUI, navigate to the TI COLLECTOR menu and press the ENTER key to enter this menu.

Then, navigate to the NETWORK ACTIONS tab and press the ENTER key to enter this submenu.

Next, navigate to FORM NWK and press the ENTER key.

Once the network it started, navigate to OPEN NWK and press the ENTER key to allow new sensors to join the formed IEEE 802.15.4g network. This will turn 'PermitJoin=On'. After the above actions have been performed, the UART terminal should look like the following:

Note 1: The above screenshot was taken after a BLE connection was established between the LaunchPad and a smartphone.

Note 2: The screenshots shown in this example do not reflect default network settings.

Finally, use the CUI on the sensor project to start the association process from the sensor.

Once connected, the following UART output should be displayed:

Note: "Joined - 0x0001" will be displayed followed by a Config Rsp on the same line. After that, you should see sensor message updates printed as displayed above.

For more details regarding the use of CUI for 15.4 network configuration, refer to the collector project's README.html file, located here: <SDK DIR>\examples\rtos\CC1352R1_LAUNCHXL\ti154stack\collector\README.html

Provisioned 15.4 Network on the Collector

The DMM 15.4 Collector example enables the user to control its connected sensors in the following ways:

You should see the remote display service, which is labeled as "UUID: F0001180-0451-4000-B000-000000000000" (this may be slightly different for other smartphone applications). Under this service there should be the following characteristics shown:

Sensor Address Characteristic (UUID: 1181)

This characteristic supports read and write properties, and it contains a 2-byte-long value indicating the address of the sensor to control. The user must enter the address of the sensor it wishes to control before writing to the other characteristics in this service.

Sensor Report Interval Characteristic (UUID: 1182)

This characteristic supports write properties, it contains a 4-byte-long value indicating the sensor report interval in ms. By default this is set to 3s. In the LightBlue application select the Sensor Report Interval characteristic. From here the reporting interval can only be written to. When a value is written, the rate at which node data is updated changes to reflect the new value.

Note: In LightBlue you must write to the characteristic in hex, using the correct number of digits, or the length will be incorrect and the Remote Display profile will reject the write. To set the report interval to 1s write a value of 000003E8.

Toggle LED (UUID: 1183)

This characteristic supports read and write properties, it contains a 1-byte-long value used to make the Sub1GHz 802.15.4 Collector blink a connected sensor's LED. The application is not dependent on this value. A write to this characteristic of any value will toggle the selected sensor's LED.

Disassociate Sensor (UUID: 1184)

This characteristic supports read and write properties, and it contains a 2-byte-long value indicating the address of the sensor to disassociate from the 15.4 network.

15.4 Network Device Discovery via BLE

The DMM 15.4 Collector example enables the user to discover the devices connected to its IEEE 802.15.4g network with the Network Device Service which is labeled as "UUID: F00011B0-0451-4000-B000-000000000000" (this may be slightly different for other smartphone applications).

Network Device Characteristic (UUID: 11B1)

This characteristic supports write and notify properties, and it contains a 7-byte-long value indicating the address of the sensor to retrieve the latest data from.

Writing the value 0xFFFF0000000000 to this characteristic will start the IEEE 802.15.4g network discovery process. The network device discovery process will send a BLE notification for each sensor in the network. If a sensor was previously in the network but is not responding, these sensors will also be reported; their device status will be 0 in this case.

The Network Device information in the BLE notification will be sent as follows:

2 Bytes 2 Bytes 1 Byte 1 Byte 1 Byte
Device Address Parent Address Sensor Data RSSI Device Status

The user also has the option to check the status of a single device by writing the address of the sensor it would like to receive a notification from. For example, to receive a BLE notification from sensor with short address 0x0001, simply write the value 0x00010000000000 to this characteristic.

The figure above shows notifications being received for 3 sensors connected to the 15.4 network.

In LightBlue, make sure to select the "Listen for notifications" button.

DMM 15.4 Security Manager (SM) Commissioning

If using either a dmm_154sensor_sm_remote_display_app or dmm_154collector_sm_remote_display_app project, these will support secure commissioning of a SM Sensor to a SM Collector. This DMM project will enable remote control and monitoring of the secure commissioning service via a BLE phone application connected to a DMM device. Once the phone is connected to the DMM device, the user will be able to select the Authentication Mode via the BLE phone application. If the user selects the "Passkey" mode, then the user will be able to enter the passkey via the app. This passkey will be passed to the BLE Remote Display application and then passed to the SM Sensor application. This passkey will then be used to begin commissioning of the Sensor to the Collector network. Throughout the commissioning process status updates will be sent to the BLE phone application.

DMM SM Commissioning

Using DMM SM Commissioning Example

The SimpleLink Starter mobile application is the easiest way to get started using the DMM SM feature. The steps below outline the how to use the app:

  1. Open the SimpleLink Starter mobile application, scan and connect to the DMM 15.4 SM Collec. Once the services load, select the DMM Provisioning Service.

  2. Click Form Network to form a new 15.4 network.

  3. Once the network has formed, click Open Network to allow devices to connect to the network.

  4. Once the DMM SM Collector network has been setup, disconnect the mobile app from the device.

  5. Scan and connect the DMM 15.4 SM Sensor device. Wait for all the services to load and select the DMM Provisioning Service.

    SimpleLink Starter DMM Provisioning Service Selection

  6. Once connected, the app will read and display the current SM State in the TI15.4 Security Manager section. Tap the Auth Mode Selection drop down menu to select one of the three desired authentication modes (Passkey, Default Code, Just Allow). If nothing is selected, the "Default Code" mode will be used during the commissioning process.

    SimpleLink Starter SM Auth Mode Selection

  7. In the TI DMM Provisioning Interface section, click the START PROVISIONING (CONNECT) button.

    SimpleLink Starter Start Commissioning

  8. Once the SM Sensor associates to the open SM Collector, the SM Commissioning process will start. If "Default Mode" or "Just Allow" was selected the commissioning process will be automatic and the commissioning state will eventually update to SM Success if the commissioning process was successful. If the commissioning process fails, it will be re-attempted two more times. If all attempts fail, the Sensor will decommission from the Collector's network.

    SimpleLink Starter Passkey Entry Success

  9. If "Passkey" was selected as the authentication mode, the app will eventually pop-up a module for the user to enter a custom 6-digit passkey.

    SimpleLink Starter SM Success

  10. After the passkey has been entered on the DMM SM Sensor device, disconnect the mobile app from the DMM SM Sensor and connect to the DMM 15.4 SM Collec device.

  11. Once the services load, select the DMM Provisioning Service.

    SimpleLink Starter DMM Provisioning Service Selection

  12. The app will eventually pop-up a module for the user to enter the same custom 6-digit passkey entered on the DMM SM Sensor.

    SimpleLink Starter SM Success

  13. After the passkey has been entered, the commissioning process will complete and the commissioning state will eventually update to SM Success if the commissioning process was successful. If the commissioning process fails, it will be re-attempted two more times. On each re-attempt, the user will have the ability to re-enter a custom passkey on each device. If all attempts fail, the Sensor will decommission from the Collector's network.

    SimpleLink Starter Passkey Entry Success

  14. If desired, after commissioning, the user may disconnect from the DMM SM Collector and connect to the DMM SM Sensor via the SimpleLink Starter app to view the current SM Commissioning State of the sensor.

By default, the DMM examples can support connecting up to 4 BLE centrals devices at a time. Due to the secure nature of the SM Commissioning Profile, it is important to only allow a single device being able to read/write to the SM Auth Mode and Passkey characteristics at a time. This will limit the ability for an attacker to interfere with the SM commissioning process. This will be accomplished by only allowing the first device that has an authenticated BLE bond and is trying to access an SM characteristic. Once this first device disconnects, the next device that aligns with the same criteria will be allowed to read/write the characteristics.

SM Commissioning BLE Service

A separate BLE profile sm_commisioning_gatt_profile is enabled to control and track all SM related activities. The sm_commisioning_gatt_profile has the following characeristics and permissions.

Service UUID: 0xf000baaa-0451-4000-b000-000000000000

Below summarizes the characteristics that comprise the SM Service:

SMCOMMISSIONING_PROFILE_STATECHAR_UUID

0x0000: SM Idle
0x0001: SM Starting
0x0002: SM Request Passkey
0x0003: SM Passkey Timeout
0x0004: SM Commissioning
0x0005: SM Success
0x0006: SM Error
Otherwise: Error

The software flowchart below describes the different scenarios for the SMCOMMISSIONING_PROFILE_STATECHAR_UUID to be updated. Updates to the SMCOMMISSIONING_PROFILE_STATECHAR_UUID characteristic are illustrated by the green circle objects.

DMM SM Commissioning

SMCOMMISSIONING_PROFILE_SETAUTHMODECHAR_UUID

0x0001: Passkey
0x0002: Default Code
0x0004: Just Allow

SMCOMMISSIONING_PROFILE_SETPASSKEYCHAR_UUID

Disabling Common User Interface

The common user interface (CUI) is a UART based interface that allows users to control and receive updates regarding the application. For various reasons, including reducing the memory footprint, the user is able to disable the common user interface (CUI). To disable the CUI, the following variable must be defined in the dmm_154collector_remote_display_app.opts:

-DCUI_DISABLE

Please Note: particular features that are dependednt on the CUI wil be unavailable when this feature is enabled.

DMM Collector Reboot and Reset

By default the DMM 15.4 Collector RD is configured to store network parameters in Non-Volatile memory and will be allow sensors to rejoin the network on power cycle or reset. To disable this feature you need to change:

-DNV_RESTORE

to

-DxNV_RESTORE

in the Tools/dmm_154collector_remote_display_cc13x2r1lp_app_FlashROM_Release.opt file.

Once this feature is disabled the collector will not store its connected sensor information in NV. Connected sensors will not rejoin the network when it is reset or power cycled.

By default, when the Collector is reset or power cycled the Provisioning State will be 2 (Restoring a network), and the UART should print "Restarted" once the collector network has been restarted. This will happen if there is old network information in the NV.

By default, the DMM Collector will not restart the 15.4 network on its own on reset. It must be done manually using the steps above with either the GPIO buttons, the CUI, or BLE.

To clear the NV, perform a device reset while holding the RIGHT button.

Note: Once booted the RIGHT button is used to turn Permit Join on in the network. Be careful not to hold the Right button down for to long.

DMM Limitations

The initial implementation of 15.4 + BLE DMM has only been tested with this policy.

The following limitations exist in the DMM implementation: