Zigbee End Device Door Lock Example App

Introduction

This document discusses how to use the Zigbee Door Lock Example App and the different parts that compose it. Zigbee Door Lock Application is an example which exercises different features of TI Z-Stack.

Some of the features exercised include:

Hardware Prerequisites

Software Prerequisites

Functional Description

Software Overview

This section describes the software components and the corresponding source files.

Application Files

Configuration With SysConfig

SysConfig is a GUI configuration tool that allows for TI driver and stack configurations.

To configure using SysConfig, import the SysConfig-enabled project into CCS. Double click the *.syscfg file from the CCS project explorer, where * is the name of the example project. The SysConfig GUI window will appear, where Zigbee stack and TI driver configurations can be adjusted. These settings will be reflected in the generated files.

The example project comes with working default settings for SysConfig. For the purposes of this README, it is not recommended to change the default driver settings, as any changes may impact the functionality of the example. The Zigbee stack settings may be changed as required for your use case.

Note that some Z-Stack settings are stored in non-volatile storage, and Z-Stack prioritizes stored settings over SysConfig settings. To guarantee SysConfig settings are applied, perform a factory reset of the device to clear non-volatile storage.

Example Usage

This section describes how to use this sample application.

Buttons

LEDs

Serial interface

The connection will have the following settings:

    Baud-rate:     115200
    Data bits:          8
    Stop bits:          1
    Parity:          None
    Flow Control:    None

Note: The serial output is known to be formatted incorrectly in Tera Term and in the CCS Terminal.

The serial interface allows you to control the commissioning configuration as well as application behavior. The commissioning interface is common for all applications and is implemented in the module zcl_sampleapps_ui.c/.h. Any application specific behavior of the serial interface is implemented in the example application files.

The serial interface implements a common set of menus described in 'Application Overview' within the Zigbee docs in this SDK. This common menu can be used to commission the device into a network.

Commissioning the Device Into the Network

Zigbee end devices can only join networks. This is done using the Steering Mode and executing the commissioning process in the Commissioning Screen. Zigbee end devices must also have a router parent device (this can be either Zigbee Coordinator or Zigbee Router), which is the device that allows it to join. End Devices cannot transmit/receive frames unless these goes through its parent. If an end device lost its parent, then it cannot be active in the network until it finds another suitable parent. This sample application uses stack notifications (zstackmsg_CmdIDs_BDB_NOTIFICATION) to automatically find a new suitable parent if it is lost (unresponsive due to any reason).

Interfacing with the Door Lock Controller Example App

Setup for automatic Attribute reports

Once the Door Lock and Door Lock Controller device are in the same network, enable the Finding and Binding Mode and execute it from the Commissioning Screen. When Finding and Binding is executed, the Door Lock Controller device will be set in Identify mode for 180 seconds. During this time the the Door Lock device must perform Finding and Binding as well to find the Door Lock Controller device in Identify mode and create a bind to it. The status of the Identify process is shown in the BDB status line.

FindingBinding

Finding and binding status in the BDB status line

IdXXX shows the remaining XXX seconds in Identify mode, SrchYYY/ZZ shows the remaining YYY seconds searching for devices in Identify mode and ZZ the number of binds created during this process. Once the Door Lock device has the bind, it will be able to send Report Attribute commands periodically according to the reporting configuration.

Door Lock Controller device will set IdXXX, while Door Lock device will set SrcYYY and count the binds in ZZ. Multiple devices can perform this procedure at the same time, by default up to 4 Door Lock Controllers can be binded to a single Door Lock (defined by NWK_MAX_BINDING_ENTRIES). There is no limit on the number of attribute reports that a single Door Lock Controller can receive, but is up to the application how to handle/ignore those.

Setup to control the Door Lock

As Finding and Binding does not create the binds needed in the Door Lock Controller to control the Door Lock, a custom commissioning method is available in the App Menu. To create the bind in the Door Lock Controller follow these steps:

  1. In Door Lock's App Menu, go to the Discover screen and execute it. This will enable Identify mode in the in Door Lock for 1 minute.
  2. In Door Lock Controller's App Menu, go to the Discover screen and execute it. This will discover the Door Lock and will create the bind to it.

AppMenu

Application menu entrance screen

DiscoverableScreen

Discover screen

Controlling the Door Lock

In the Change PIN screen, the PIN can be changed. Both devices, Door Lock and Door Lock Controller, must have the same PIN in order to lock or unlock the door.

Change PIN

Change PIN screen

The status of the door is displayed in the Door Lock status line. The Doorlock LOCK and UNLOCK App Menu screens can be used to change the local lock state.

Doorlock Lock

Doorlock Status

LOCK screen and Doorlock Status Line