Changelog

Table of Contents

 

New Features

BLE5-Stack

ID Summary
BLE_AGAMA-4523 [SysConfig] Add support for CC2674R10RGZ & CC2674P10RGZ and enable migration to it
BLE_AGAMA-4521 [syscfg] Add Migration Support for CC2642R1FRTCQ1 & CC2642R1FRGZQ1

Proprietary RF

ID Summary
PROPRF-1217 Implement SysConfig migration path for CC2674[RP]10 on rfDiagnostics

TI-OpenThread

ID Summary
None None

TI 15.4-Stack

ID Summary
TI154STACK-4296 Add migration support for CC2674

TI Wi-SUN FAN

ID Summary
None None

TI Z-Stack

ID Summary
ZIGBEE-2027 Add migration support for CC2674

DMM

ID Summary
DMM-1372 Add migration support for CC2674

TI-RTOS and Drivers

ID Summary
None None

Radio Software Bundle (RFLib)

ID Summary
RFDRIVER-470 CC13x4: Add support for increased Sub-1GHz PA table resolution
RFCORE-961 CC2652R-Q1: PA Table Update - Improved Performance
RFCORE-971 cc13x4_cc26x4: Settings Release - 5/20 dBm: BLE 1M, 2M, Coded and IEEE 802.15.4 (ZigBee) - Characterized
RFCORE-972 cc13x4_cc26x4: PA Table Update - Increased Sub-1GHz Granularity
RFCORE-967 cc13x4_cc26x4: Settings Release - 20 dBm: PROP 16.384 kbps OOK, Manchester encoding - Characterized
RFCORE-932 CC1312PSIP: Settings Release - 14 dBm: 50 kbps/ 200 kbps / 1 Mbps 2-GFSK - Characterized
RFCORE-924 cc13x4_cc26x4: Settings Release - 5 dBm: 50/25/12.5/6.25 kbps SUN O-QPSK - Release Candidate
RFCORE-966 CC1312PSIP: PA Table Update - 20 dBm: Characterized
RFCORE-965 CC1312PSIP: Settings Release - 20 dBm: 50 kbps 2-GFSK - Characterized
RFCORE-964 CC1312PSIP: Settings Release - 20 dBm: Zigbee R23 500 kbps 2-GFSK - Characterized
RFCORE-938 CC1312PSIP: Settings Release - 14 dBm: Zigbee R23 100/500 kbps 2-GFSK - Characterized
RFCORE-953 CC1312PSIP: Settings Release - 14 dBm: WB-DSSS 240/120/60/30 kbps with 1/2/4/8 x spreading - Characterized
RFCORE-952 CC1312PSIP: Settings Release - 14 dBm: 4.8 kbps OOK - Characterized
RFCORE-934 CC1312PSIP: Settings Release - 14 dBm: Wireless MBUS S1-/S2-/T-/C-Mode - Characterized
RFCORE-933 CC1312PSIP: PA Table Update - 14 dBm: Characterized
RFCORE-944 CC1312PSIP: Settings Release - 14 dBm: Wi-SUN Mode #1-5 - Characterized
RFCORE-940 CC1312PSIP: Settings Release - 14 dBm: SimpleLink Long Range 2.5/5 kbps - Characterized
RFCORE-931 CC1312PSIP: Settings Release - 14 dBm: 9.6 kbps Narrowband - Characterized
RFCORE-927 cc13x4_cc26x4: Settings Release - 5/14 dBm: PROP 16.384 kbps OOK, Manchester encoding - Characterized
RFCORE-892 cc13x1_cc26x1: Settings Update - Patch: Remove deprecated “rf_patch_cpe_multi_protocol”

 

Fixed Issues

BLE5-Stack

ID Summary
None None

Proprietary RF

ID Summary
None None

TI-OpenThread

ID Summary
None None

TI 15.4-Stack

ID Summary
TI154STACK-4305 DSR Reported that MAC_PURGE_CNF is being received with an invalid handle

TI Wi-SUN FAN

ID Summary
None None

TI Z-Stack

ID Summary
None None

DMM

ID Summary
None None

TI-RTOS and Drivers

ID Summary
None None

Radio Software Bundle (RFLib)

ID Summary
None None

 

Known Issues

BLE5-Stack

ID Summary
BLE_AGAMA-4560 [CC13x4 / CC26x4] Connection timeouts observed during during data streaming with PHY changes, and MTU modifications
BLE_AGAMA-4484 multi_role FreeRTOS support removed from CC13XX / CC26XX
BLE_AGAMA-4483 [MESH] eRPC support removed due to build failure
BLE_AGAMA-4480 [Basic Example] Basic Broadcaster Doesn't Advertise
BLE_AGAMA-4406 multi_sensor project has been removed from CC13XX / CC26XX
BLE_AGAMA-4354 Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager
BLE_AGAMA-4352 simple_mesh_node_and_peripheral_oad_onchip build failed error in TI Clang for CC26X2PSIP & CC13X2P2
BLE_AGAMA-4324 [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar
BLE_AGAMA-4029 Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set.
BLE_AGAMA-4009 [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands
BLE_AGAMA-3896 [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands
BLE_AGAMA-3774 Under certain conditions the CC2652R1 failed to synchronize to periodic advertising
BLE_AGAMA-3752 [CC2651] Host_test memory limitation using CCS+TI-CLANG
BLE_AGAMA-3747 [MESH][AE][eRPC] ~100% missing packets more than 3 hops while GATT Bearer is enabled
BLE_AGAMA-3606 [Mesh][Stability] Messages might stop after ~3 hours in a network with more than ~20 nodes
BLE_AGAMA-3597 [Mesh] LPN might fail to maintain friendship with ble.scanLatency < 10, when Display module is enabled
BLE_AGAMA-3556 [Mesh][IOP] LPN fails to configure after provisioning over PB-GATT with BlueZ
BLE_AGAMA-3543 [Build] Simple Mesh and Peripheral OAD onchip example fail to compile with GATT Bearer for CCS/TICLANG due to memory limitation
BLE_AGAMA-3540 [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC
BLE_AGAMA-3486 Device asserts upon connection when HeapMem and HeapTrack is used
BLE_AGAMA-3427 System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued
BLE_AGAMA-3391 [Mesh][eRPC] Limitation - Mesh node with eRPC unable to transmit messages > 221B
BLE_AGAMA-3388 [Mesh] Relay fails to transmit segmented message without re-transmission (relay re-transmit = 0)
BLE_AGAMA-3383 Mesh stack delay work API is limited to a maximum delay of uint32 maximum value (42,949,672 milliseconds)
BLE_AGAMA-3381 Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration
BLE_AGAMA-3169 Connecting twice to the same device causing wrong count of connections and a memory leakage
BLE_AGAMA-3107 [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms
BLE_AGAMA-3077 [RTLS] CTE reception on the 2M PHY do not meet spec requirements
BLE_AGAMA-3076 [RTLS] CTEs sent on the 2M PHY do not meet spec requirements
BLE_AGAMA-3024 [MESH] [IOP] Mesh DUT is not publishing its mesh supported roles (Unable to config Mesh node) with iPhone
BLE_AGAMA-2266 Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms
BLE_AGAMA-2033 [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release)
BLE_AGAMA-2010 [Multi-Sensor] Updating Report Interval Have no effect
BLE_AGAMA-1675 IOP: Device fails to pair with Meizu Pro 7
BLE_AGAMA-1435 [Multi-Sensor] Accelerometer Service Disappears After First Connection
BLE_AGAMA-139 When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection
BLE_AGAMA-80 The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases.

Proprietary RF

ID Summary
None None

TI-OpenThread

ID Summary
None None

TI 15.4-Stack

ID Summary
None None

TI Wi-SUN FAN

ID Summary
None None

TI Z-Stack

ID Summary
None None

DMM

ID Summary
None None

TI-RTOS and Drivers

ID Summary
TIRTOS-2164 Simultaneous TI-RTOS 6 and TI-RTOS 7 support causes CCS XDS include path warning for TI-RTOS 6
TIPOSIX-4 clock_nanosleep() with CLOCK_REALTIME broken on msp432
TIDRIVERS-4844 Implement restrictions in errata note IOC_01 in SysConfig
TIDRIVERS-4127 ADCBuf causes jitter when switching clock sources
TIDRIVERS-1642 NVSSPI25x driver does not work when using internal SPI CS
SYSBIOS-642 Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field
SYSBIOS-446 Reported CPU load is not 100% when a task is in “while 1 {}” loop
SYSBIOS-98 Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432
FREERTOS-8 Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex

Radio Software Bundle (RFLib)

ID Summary
None None