![]() |
![]() |
|
rflib
|
RF_ratCompare parameter structure. More...
#include <RFCC26X2.h>

Data Fields | |
| RF_RatCallback | callback |
| Callback function to be invoked upon a capture event (optional). More... | |
| RF_RatHandle | channel |
| RF_RatHandle identifies the channel to be allocated. More... | |
| uint32_t | timeout |
RF_ratCompare parameter structure.
RF_RatCompare parameters are used with the RF_ratCompare() call.
| RF_RatCallback RF_RatConfigCompare::callback |
Callback function to be invoked upon a capture event (optional).
| RF_RatHandle RF_RatConfigCompare::channel |
RF_RatHandle identifies the channel to be allocated.
| uint32_t RF_RatConfigCompare::timeout |
Timeout value in RAT ticks to be programmed in the timer as the trigger of compare event.