![]() |
![]() |
|
rflib
|
RF schedule map entry structure. More...
#include <RFCC26X2.h>

Data Fields | |
| RF_CmdHandle | ch |
| Command handle. More... | |
| RF_Handle | pClient |
| Pointer to client object. More... | |
| uint32_t | startTime |
| Start time (in RAT tick) of the command or access request. More... | |
| uint32_t | endTime |
| End time (in RAT tick) of the command or access request. More... | |
| RF_Priority | priority |
| Priority of the command or access request. More... | |
RF schedule map entry structure.
| RF_CmdHandle RF_ScheduleMapElement::ch |
Command handle.
| RF_Handle RF_ScheduleMapElement::pClient |
Pointer to client object.
| uint32_t RF_ScheduleMapElement::startTime |
Start time (in RAT tick) of the command or access request.
| uint32_t RF_ScheduleMapElement::endTime |
End time (in RAT tick) of the command or access request.
| RF_Priority RF_ScheduleMapElement::priority |
Priority of the command or access request.