![]() |
![]() |
|
rflib
|
Clear all RX Queue Entries. More...
#include <rf_common_cmd.h>

Data Fields | |
| uint16_t | commandNo |
| The command ID number 0x0008. More... | |
| uint16_t | __dummy0 |
| dataQueue_t * | pQueue |
| Pointer to the queue structure to be cleared. More... | |
Clear all RX Queue Entries.
| uint16_t rfc_CMD_CLEAR_RX_s::commandNo |
The command ID number 0x0008.
| uint16_t rfc_CMD_CLEAR_RX_s::__dummy0 |
| dataQueue_t * rfc_CMD_CLEAR_RX_s::pQueue |
Pointer to the queue structure to be cleared.