![]() |
![]() |
|
rflib
|
Set Radio Timer Channel in Compare Mode. More...
#include <rf_common_cmd.h>
Data Fields | |
| uint16_t | commandNo |
| The command ID number 0x000A. More... | |
| uint8_t | ratCh |
| The radio timer channel number. More... | |
| uint8_t | __dummy0 |
| ratmr_t | compareTime |
| The time at which the compare occurs. More... | |
Set Radio Timer Channel in Compare Mode.
| uint16_t rfc_CMD_SET_RAT_CMP_s::commandNo |
The command ID number 0x000A.
| uint8_t rfc_CMD_SET_RAT_CMP_s::ratCh |
The radio timer channel number.
| uint8_t rfc_CMD_SET_RAT_CMP_s::__dummy0 |
| ratmr_t rfc_CMD_SET_RAT_CMP_s::compareTime |
The time at which the compare occurs.