34 #ifndef ti_drivers_CryptoKeyKeyStore_PSA_init__include 35 #define ti_drivers_CryptoKeyKeyStore_PSA_init__include The CryptoKey type is an opaque representation of a cryptographic key.
CryptoKeyKeyStore_PSA driver header.
CryptoKey datastructure.
Definition: CryptoKey.h:192
int_fast16_t KeyStore_PSA_initKey(CryptoKey *keyHandle, KeyStore_PSA_KeyFileId keyID, size_t keyLength, void *keyAttributes)
Initializes a CryptoKey type.
psa_key_file_id_t KeyStore_PSA_KeyFileId
Definition: CryptoKeyKeyStore_PSA.h:762
int_fast16_t KeyStore_PSA_initBlankKey(CryptoKey *keyHandle, KeyStore_PSA_KeyFileId keyID, size_t keyLength, void *keyAttributes)
Initializes a Blank CryptoKey type.