rfOADServer
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
Example Summary
The rfOADServer project together with rfOADClientExtFlash, rfOADClientIntFlashPApp + rfOADClientIntFlashUApp, or rfOADClient, illustrates how over-the-air download works. This example works by sending a signed firmware image to the OAD Client one block at a time.
Peripherals Exercised
CONFIG_GPIO_GLED
- Toggled when data is transmitted over the RF interfaceCONFIG_GPIO_RLED
- Toggled when data is received over the RF interface
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433 and the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNCHXL and the CC26X2R1-LAUNCHXL
- 868.0 MHz for other launchpads In order to change frequency, modify the ti_radio_config.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default.
- On the CC1352P-2 and CC1352P-4 the high PA operation for Sub-1 GHz modes is not supported
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Required Firmware Images
- rfOADServer Image
- From this rfOADServer Project:
<CCS_WORKSPACE>\rfOADServer_<PLATFORM>_tirtos7_ticlang\Debug\rfOADServer_<PLATFORM>_tirtos7_ticlang.hex
- From this rfOADServer Project:
- A Signed Version 2 of the Client Image
- If using the Boot Image Manager (BIM) as bootloader, the client image v2 must be built from rfOADClientExtFlash or rfOADClientIntFlashUApp project. This will be the image that rfOADServer will transmit over the air to the client launchpad. Refer to rfOADClientIntFlashUApp's
README.md
for information on how to sign images. - If using MCUBoot as bootloader, the client image v2 must be built from the rfOADClient project. This will be the image that rfOADServer will transmit over the air to the client launchpad. Refer to rfOADClient's
README.md
for information on how to sign images.
- If using the Boot Image Manager (BIM) as bootloader, the client image v2 must be built from rfOADClientExtFlash or rfOADClientIntFlashUApp project. This will be the image that rfOADServer will transmit over the air to the client launchpad. Refer to rfOADClientIntFlashUApp's
Example Usage
- Open a serial session (e.g. PuTTY, TeraTerm) to appropriate COM port with the following settings:
Baud-rate: 115200 Data bits: 8 Stop bits: 1 Parity: None Flow Control: None
- Using BTN2 on the Launchpad, cycle through the options, and then select Update Available FW using BTN1
- IMPORTANT: Close the serial session. This is required to allow the next step to use the COM port.
- Open a terminal and run oad_write_bin.py to write the signed client image to flash in preparation for OAD.
cd <SDK_INSTALL_DIR>/tools/proprf/oad
python oad_write_bin.py COM96 path/to/signed_client_image_v2.bin
- At this point, the image is now saved in the rfOADServer's external flash. Open a serial session again and cycle through the options. This time, select Update Client FW to start over-the-air download to the client launchpad.
- Once the OAD is complete, the client will reboot to the new client application.
Application Design Details
Init
|
|
+----> Wait for OAD/Radio Events/Button Press
| |
| V
| Process OAD Client & Radio Events
| |
| V
| +-----------+----------+---------------------------+------------------------+-------------------+
| | | | | |
| V V V V V
| Get FW Version Start OAD RX Block Req Update Curr FW Send Reset Req
| | | | | |
| | V V V |
| | Send Img Identify Req Read then Send Block Write new blocks to flash |
| | | | |
| V | | |
| Send FW Version Req | | |
| | | |
| +---------------------------+--------------------------------------------+
| |
| V
+-----> Packet RX Packet TX