AESCTRCC26X4_s.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022-2023, Texas Instruments Incorporated - http://www.ti.com
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_drivers_aesctr_AESCTRCC26X4_s__include
34 #define ti_drivers_aesctr_AESCTRCC26X4_s__include
35 
36 #include <stdint.h>
37 
39 #include <ti/drivers/AESCTR.h>
40 
42 
43 #include <third_party/tfm/interface/include/psa/error.h>
44 #include <third_party/tfm/interface/include/psa/service.h>
45 
46 #if defined(TFM_BUILD)
47  #include "ti_drivers_config.h" /* Sysconfig generated header */
48 #endif
49 
50 #ifdef __cplusplus
51 extern "C" {
52 #endif
53 
54 /*
55  * AES CTR secure message types
56  */
57 #define AESCTR_S_MSG_TYPE_CONSTRUCT AESCTR_S_MSG_TYPE(0U)
58 #define AESCTR_S_MSG_TYPE_OPEN AESCTR_S_MSG_TYPE(1U)
59 #define AESCTR_S_MSG_TYPE_REGISTER_CALLBACK AESCTR_S_MSG_TYPE(2U)
60 #define AESCTR_S_MSG_TYPE_CLOSE AESCTR_S_MSG_TYPE(3U)
61 #define AESCTR_S_MSG_TYPE_ONE_STEP_ENCRYPT AESCTR_S_MSG_TYPE(4U)
62 #define AESCTR_S_MSG_TYPE_ONE_STEP_DECRYPT AESCTR_S_MSG_TYPE(5U)
63 #define AESCTR_S_MSG_TYPE_SETUP_ENCRYPT AESCTR_S_MSG_TYPE(6U)
64 #define AESCTR_S_MSG_TYPE_SETUP_DECRYPT AESCTR_S_MSG_TYPE(7U)
65 #define AESCTR_S_MSG_TYPE_ADD_DATA AESCTR_S_MSG_TYPE(8U)
66 #define AESCTR_S_MSG_TYPE_FINALIZE AESCTR_S_MSG_TYPE(9U)
67 #define AESCTR_S_MSG_TYPE_CANCEL_OPERATION AESCTR_S_MSG_TYPE(10U)
68 
69 /*
70  * Config pool size determines how many dynamic driver instances can be created
71  * by the non-secure client using AESCTR_construct().
72  */
73 #ifndef CONFIG_AESCTR_S_CONFIG_POOL_SIZE
74  #define CONFIG_AESCTR_S_CONFIG_POOL_SIZE 1
75 #endif
76 
77 #define AESCTR_SECURE_CALLBACK_COUNT (CONFIG_TI_DRIVERS_AESCTR_COUNT + CONFIG_AESCTR_S_CONFIG_POOL_SIZE)
78 
79 /*
80  * ========= AES CTR Secure Callback struct =========
81  * Non-secure clients must register their callback after opening or
82  * constructing a driver instance with blocking or callback return behavior.
83  */
84 typedef struct
85 {
87  /* AES CTR callback fxn parameters */
89  int_fast16_t returnValue;
93 
94 /*
95  * ========= AES CTR Secure Message Structs =========
96  * These secure message structs correspond to the secure message types defined
97  * above. Together, they are used by non-secure client to make PSA calls to the
98  * AES CTR secure service. There is a single input vector for the PSA call
99  * which is a pointer to secure message struct. If the underlying function
100  * has a return value, there is a single output vector which is a pointer to
101  * storage for the return value.
102  */
103 typedef struct
104 {
108 
109 typedef struct
110 {
111  uint_least8_t index;
114 
115 typedef struct
116 {
120 
121 typedef struct
122 {
125 
126 typedef struct
127 {
131 
132 typedef struct
133 {
135  const CryptoKey *key;
136  const uint8_t *initialCounter;
138 
139 typedef struct
140 {
144 
146 
147 typedef struct
148 {
151 
162 psa_status_t AESCTR_s_handlePsaMsg(psa_msg_t *msg);
163 
169 void AESCTR_s_init(void);
170 
171 #ifdef __cplusplus
172 }
173 #endif
174 
175 #endif /* ti_drivers_aesctr_AESCTRCC26X4_s__include */
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:141
Definition: AESCTRCC26X4_s.h:132
Definition: AESCTRCC26X4_s.h:147
Definition: AESCTRCC26X4_s.h:84
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:128
Definition: SecureCallback.h:51
Definition: AESCTRCC26X4_s.h:126
CTR Parameters.
Definition: AESCTR.h:679
const uint8_t * initialCounter
Definition: AESCTRCC26X4_s.h:136
Struct containing the parameters required for encrypting/decrypting a message using a one-step operat...
Definition: AESCTR.h:510
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:123
Definition: AESCTRCC26X4_s.h:121
AES Global configuration.
Definition: AESCommon.h:154
AESCTR_OperationType
Enum for the operation types supported by the driver.
Definition: AESCTR.h:623
CryptoKey datastructure.
Definition: CryptoKey.h:196
AESCTR_Config * config
Definition: AESCTRCC26X4_s.h:105
void AESCTR_s_init(void)
Initializes the AES CTR secure driver.
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:134
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:117
Definition: AESCTRCC26X4_s.h:109
Secure Crypto Service.
const CryptoKey * key
Definition: AESCTRCC26X4_s.h:135
AESCTR_OperationUnion * operation
Definition: AESCTRCC26X4_s.h:90
Struct containing the parameters required for encrypting/decrypting a message using a segmented opera...
Definition: AESCTR.h:549
Definition: AESCTRCC26X4_s.h:103
AESCTR_s_AddDataMsg AESCTR_s_FinalizeMsg
Definition: AESCTRCC26X4_s.h:145
AESCTR_OperationType operationType
Definition: AESCTRCC26X4_s.h:91
psa_status_t AESCTR_s_handlePsaMsg(psa_msg_t *msg)
Handles PSA messages for AES CTR secure driver.
Definition: AESCTRCC26X4_s.h:139
SecureCallback_Object object
Definition: AESCTRCC26X4_s.h:86
int_fast16_t returnValue
Definition: AESCTRCC26X4_s.h:89
AESCTR_s_SecureCallback * callback
Definition: AESCTRCC26X4_s.h:118
AESCTR_OneStepOperation * operation
Definition: AESCTRCC26X4_s.h:129
Definition: AESCTRCC26X4_s.h:115
uint_least8_t index
Definition: AESCTRCC26X4_s.h:111
const AESCTR_Params * params
Definition: AESCTRCC26X4_s.h:106
AESCTR_SegmentedOperation * operation
Definition: AESCTRCC26X4_s.h:142
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:149
Union containing a reference to a one-step and segmented operation structure.
Definition: AESCTR.h:585
const AESCTR_Params * params
Definition: AESCTRCC26X4_s.h:112
AESCTR_Handle handle
Definition: AESCTRCC26X4_s.h:88
AESCTR driver header.
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale