Go to the source code of this file.
§ ECCParams_s_getCurveParams()
Returns a pointer to curve params stored in secure memory.
- Parameters
-
| curveParams | Points to curve param struct provided by non-secure code which references a curve by its name. |
- Returns
- Pointer to the curve params stored in secure memory.
§ ECCParams_s_getUncompressedGeneratorPoint()
| int_fast16_t ECCParams_s_getUncompressedGeneratorPoint |
( |
const ECCParams_CurveParams * |
curveParams, |
|
|
uint8_t * |
buffer, |
|
|
size_t |
length |
|
) |
| |
Veneer to extract the curve generator point from an ecliptic curve description.
- Note
- See ECCParams_s_getUncompressedGeneratorPoint() in ECCParam.h for full description, parameters, and return values. PSA_ERROR_PROGRAMMER_ERROR is an additional return value.
- Return values
-
| PSA_ERROR_PROGRAMMER_ERROR | if any args point to secure addresses. |