![]() |
![]() |
ECDHCC26X2 Object. More...
#include <ECDHCC26X2.h>

Data Fields | |
| bool | isOpen |
| bool | operationInProgress |
| bool | operationCanceled |
| int_fast16_t | operationStatus |
| ECDH_CallbackFxn | callbackFxn |
| ECDH_ReturnBehavior | returnBehavior |
| ECDH_Operation | operation |
| ECDH_OperationType | operationType |
| ECDHCC26X2_FsmState | fsmState |
| uint32_t | semaphoreTimeout |
| uint32_t | resultAddress |
ECDHCC26X2 Object.
The application must not access any member variables of this structure!
| bool ECDHCC26X2_Object::isOpen |
| bool ECDHCC26X2_Object::operationInProgress |
| bool ECDHCC26X2_Object::operationCanceled |
| int_fast16_t ECDHCC26X2_Object::operationStatus |
| ECDH_CallbackFxn ECDHCC26X2_Object::callbackFxn |
| ECDH_ReturnBehavior ECDHCC26X2_Object::returnBehavior |
| ECDH_Operation ECDHCC26X2_Object::operation |
| ECDH_OperationType ECDHCC26X2_Object::operationType |
| ECDHCC26X2_FsmState ECDHCC26X2_Object::fsmState |
| uint32_t ECDHCC26X2_Object::semaphoreTimeout |
| uint32_t ECDHCC26X2_Object::resultAddress |