![]() |
![]() |
LCD Object. More...
#include <LCDDogm1286.h>

Data Fields | |
| bool | isOpen |
| SPI_Handle | spiHandle |
| unsigned int | lcdWriteTimeout |
| SemaphoreP_Struct | lcdMutex |
| LCD_Buffer * | lcdBuffers |
| uint8_t | nBuffers |
LCD Object.
The application must not access any member variables of this structure!
| bool LCD_Object::isOpen |
| SPI_Handle LCD_Object::spiHandle |
| unsigned int LCD_Object::lcdWriteTimeout |
| SemaphoreP_Struct LCD_Object::lcdMutex |
| LCD_Buffer* LCD_Object::lcdBuffers |
| uint8_t LCD_Object::nBuffers |