![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint8_t | endpoint |
| The endpoint that will receive messages sent to the group in the group field. | |
| uint16_t | groupID |
| This is the group ID that is set over the air. | |
| uint8_t | n_name |
| length of "name" | |
| uint8_t * | pName |
| pointer to the Human readable "name" of group | |
Structure to send an APS Add Group Request.