Z-Stack API Reference  7.40.00.20
_zstack_bdbRecoverNwkRsp_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t status
 

Detailed Description

Structure to send a BDB to Recover Network Request.

Field Documentation

§ status

uint8_t status

Indicate if the request was process or not. The request will fail if the device has not been commissioned yet


The documentation for this struct was generated from the following file: