Z-Stack API Reference  7.40.00.20
_zstack_bdbtouchlinktargetenablecommissioningreq_t Struct Reference

#include <zstack.h>

Data Fields

uint32_t timeoutTime
 

Detailed Description

Structure to send a BDB Touchlink Target Enable Commissioning Request.

Field Documentation

§ timeoutTime

uint32_t timeoutTime

Time that touchlink commissioning as target will be enabled. A value equal or bigger than TOUCHLINK_TARGET_PERPETUAL will enable this commissioning method until disabled by the application.


The documentation for this struct was generated from the following file: