Z-Stack API Reference  7.40.00.20
_zstack_bdbzclidentifycmdindreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t identifyTime
 
uint8_t endpoint
 

Detailed Description

Structure to send to the stack the identify command parameters.

Field Documentation

§ identifyTime

uint16_t identifyTime

Parameters of identify command


The documentation for this struct was generated from the following file: