Z-Stack API Reference  7.40.00.20
_zstack_bindrec_t Struct Reference

#include <zstack.h>

Data Fields

zstack_LongAddr_t srcAddr
 
uint8_t srcEndpoint
 
uint16_t clusterID
 
zstack_AFAddr_t dstAddr
 

Detailed Description

Structure for the Binding Information record.

Field Documentation

§ clusterID

uint16_t clusterID

Cluster ID

§ dstAddr

zstack_AFAddr_t dstAddr

Binding's destination address (IEEE address only)

§ srcAddr

Targeted device's ieee address

§ srcEndpoint

uint8_t srcEndpoint

Targeted device's endpoint


The documentation for this struct was generated from the following file: