Z-Stack API Reference  7.40.00.20
_zstack_capabilityinfo_t Struct Reference

#include <zstack.h>

Data Fields

bool panCoord
 
bool ffd
 
bool mainsPower
 
bool rxOnWhenIdle
 
bool security
 

Detailed Description

Structure defines the Capabilities Information bit field.

Field Documentation

§ ffd

bool ffd

True if the device is a full function device (FFD)

§ mainsPower

bool mainsPower

True if the device is mains powered

§ panCoord

bool panCoord

True if the device is a PAN Coordinator

§ rxOnWhenIdle

bool rxOnWhenIdle

True if the device's RX is on when the device is idle

§ security

bool security

True if the device is capable of sending and receiving secured frames


The documentation for this struct was generated from the following file: