Z-Stack API Reference  7.40.00.20
_zstack_gpSecReq_t Struct Reference

#include <zstack.h>

Data Fields

gpdID_t gpdID
 
uint8_t EndPoint
 
gp_SecData_t gp_SecData
 
uint8_t dGPStubHandle
 

Detailed Description

Structure to send a GP Security Request.

Field Documentation

§ EndPoint

uint8_t EndPoint

The identifier of the GPD endpoint used in combination with the GPD IEEE address if ApplicationID = 0b010. If ApplicationID = 0b000 this parameter is ignored

§ gp_SecData

gp_SecData_t gp_SecData

Security parameters

§ gpdID

gpdID_t gpdID

Green power device ID parameters


The documentation for this struct was generated from the following file: