Z-Stack API Reference  7.40.00.20
_zstack_nodedescriptor_t Struct Reference

#include <zstack.h>

Data Fields

zstack_LogicalTypes logicalType
 
bool complexDescAvail
 
bool userDescAvail
 
uint8_t apsFlags
 
uint8_t freqBand
 
zstack_CapabilityInfo_t capInfo
 
uint16_t manufacturerCode
 
uint8_t maxBufferSize
 
uint16_t maxInTransferSize
 
zstack_ServerCapabilities_t serverMask
 
uint16_t maxOutTransferSize
 
uint32_t descCap
 

Detailed Description

Structure for the ZDO Node Descriptor

Field Documentation

§ apsFlags

uint8_t apsFlags

(5 bits) Node Flags assigned for APS

§ capInfo

MAC Capabilities

§ complexDescAvail

bool complexDescAvail

Set if the Complex Descriptor is available

§ descCap

uint32_t descCap

Descriptor capabilities

§ freqBand

uint8_t freqBand

(3 bits) Identifies node frequency band capabilities

§ logicalType

zstack_LogicalTypes logicalType

Device type

§ manufacturerCode

uint16_t manufacturerCode

Manufacturer Code allocated by Zigbee Alliance

§ maxBufferSize

uint8_t maxBufferSize

Maximum size of NPDU

§ maxInTransferSize

uint16_t maxInTransferSize

Maximum size of transfer up to 0x7FFF, reserved and shall be set to 0

§ maxOutTransferSize

uint16_t maxOutTransferSize

(uint16_t) Maximum size of Transfer up to 0x7FFF

§ serverMask

Server Capabilities

§ userDescAvail

bool userDescAvail

Set if the User Descriptor is available


The documentation for this struct was generated from the following file: