Z-Stack API Reference  7.40.00.20
_zstack_secnwkkeygetrsp_t Struct Reference

#include <zstack.h>

Data Fields

bool activeKey
 
uint8_t seqNum
 
uint8_t key [16]
 

Detailed Description

Structure to send a Security Network Key Get Response.

Field Documentation

§ activeKey

bool activeKey

True for the active key information, False for the alternate key information

§ key

uint8_t key[16]

16 bytes of key data

§ seqNum

uint8_t seqNum

Key sequence number


The documentation for this struct was generated from the following file: