![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| bool | activeKey |
| uint8_t | seqNum |
| bool | has_key |
| uint8_t | key [16] |
Structure to send a Security Network Key Set Request.
| bool activeKey |
True to set the active key information, False to set the alternate key
| bool has_key |
True if key is included
| uint8_t key[16] |
(optional) 16 bytes of key data, if not included the key is randomly generated.
| uint8_t seqNum |
Key sequence number