Z-Stack API Reference  7.40.00.20
_zstack_zdosimpledescreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t dstAddr
 
uint16_t nwkAddrOfInterest
 
uint8_t endpoint
 

Detailed Description

Structure to send the ZDO Simple Descriptor Request.

Field Documentation

§ dstAddr

uint16_t dstAddr

Destination address

§ endpoint

uint8_t endpoint

Application endpoint being queried

§ nwkAddrOfInterest

uint16_t nwkAddrOfInterest

The network address of the destination device being queried.


The documentation for this struct was generated from the following file: