References¶
Terms and Acronyms¶
TI Wi-SUN FAN Stack Terms and Acronyms¶
- AES¶
- Advanced Encryption Standard. 
- BR¶
- Border router¶
- Each Wi-SUN network contains a Border Router providing WAN connectivity to the PAN. The Border Router maintains source routing tables for all nodes within its PAN, provides node authentication and key management services, and disseminates PAN wide information such as broadcast schedules. 
- GAK¶
- Group AES Key¶
- All devices within a Wi-SUN FAN or PAN network use a common key called GAK for encrypting packets at MAC layer. 
- GTK¶
- Group Transient Key¶
- The GAK is derived from the Group Transient Key (GTK) which is installed on the node during the joining process. More info in Join Process. 
- IEs¶
- Information elements¶
- IEs allow hopping neighbors to transmit unicast messages to each other. IEs can be exchanged either during the joining of the network or during the network operation time. 
- NCP¶
- Network co-processor¶
- The TI Wi-SUN FAN network processor mode uses one host and one network co-processor with a UART interface. 
- Root¶
- In a Wi-SUN network, the border router is the root of the RPL tree. 
- RPL¶
- Routing protocol for low-power and lossy networks. See Routing Layer (RPL). 
Sensor Controller Terms and Acronyms¶
- SC¶
- Sensor Controller¶
- A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states. 
- SCS¶
- Sensor Controller Studio¶
- A stand-alone IDE used to write, test and debug code for the Sensor Controller. 
TI-RTOS7 Terms and Acronyms¶
- HWI¶
- Hardware Interrupts¶
- A TI-RTOS7 hardware interrupt. 
- Idle Task¶
- A TI-RTOS7 default task that is executes when no other higher priority thread needs to run. 
- ROV¶
- Runtime Object View¶
- A TI-RTOS7 kernel plugin for CCS and IAR to view a target’s instrumentation data. 
- RTC¶
- Real-Time Clock¶
- An accurate computer clock which keeps track of the current time. 
- RTOS¶
- Real Time Operating System¶
- An operating system intended to serve applications with real-time requirements. 
- SWI¶
- Software Interrupts¶
- A TI-RTOS7 software interrupt. 
- TI-RTOS7¶
- Texas Instruments Real Time Operating System¶
- An RTOS developed by TI for TI microcontrollers. 
- Zero-Latency Interrupts¶
- An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS7 Kernel (SYS/BIOS) User’s Guide. 
Over-the-Air Download (OAD) Terms and Acronyms¶
- BIM¶
- Boot Image Manager¶
- A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry. 
- CRC¶
- Cyclic Redundancy Check¶
- An error-detecting code used to check the integrity of blocks of data. 
- ECDSA¶
- Elliptic Curve Digital Signature Algorithm¶
- A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography. 
- Factory Image¶
- The factory image is a “golden” image that resides in external flash as a fail-safe mechanism. 
- HIB¶
- Halt In Boot¶
- A mechanism in CC13xx or CC26xx to ensure that the external emulator can take control of the device before it executes any application code. 
- OAD¶
- Over-the-Air Download¶
- The process of performing a device firmware update over the air. 
- OAD Target¶
- The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx or CC13xx device running the TI protocol-specific transport for OAD. 
- OAD Distributor¶
- The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target. 
General Terms and Acronyms¶
- CCFG¶
- Customer Configuration¶
- Customer Configuration Area¶
- Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual. 
- CCS¶
- Code Composer Studio¶
- An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio 
- cJTAG¶
- compact JTAG¶
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG. 
- GCC¶
- GNU Compiler Collection¶
- A compiler system produced by the GNU Project, which support various programming languages such as C and C++. 
- GPRAM¶
- General purpose RAM¶
- This memory area is used for the cache per default, but can be configured to be used as RAM. 
- IAR¶
- Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications. 
- JTAG¶
- Joint Test Action Group¶
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG. 
- MCU¶
- Microcontroller Unit¶
- A small computer on a single integrated circuit. 
- NVS¶
- Non-Volatile Storage¶
- Storage of data in non-volatile memory (NVM). NVM retains saved data during power cycles. In the context of CC13xx and CC26xx devices, NVM either refers to the internal flash or some external flash. 
- ROM¶
- Read-only Memory¶
- Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read. 
- RTSC¶
- Real Time Software Components¶
- A toolset for creating reusable code, used by TI-RTOS. See RTSC and RTSC-Pedia. 
- SysConfig¶
- System Configuration Tool¶
- SysConfig is a graphical interface for configuring software projects. Configuration files, C source files and header files are generated based on the parameters configured in the SysConfig dashboard. See Get started with SysConfig. 
- TI-CLANG¶
- TI Arm Clang Compiler Toolchain¶
- The TI Arm Clang Compiler Toolchain (tiarmclang) is the next generation TI Arm compiler, replacing the previous TI Arm Compiler Tools (armcl). You can use the tiarmclang compiler toolchain to build applications from C, C++, and/or assembly source files to be loaded and run on one of the Cortex-M or Cortex-R Arm processors that are supported by the toolchain. You can find more information here. 
- VIMS¶
- Versatile Instruction Memory System¶
- A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual. 
- .bss¶
- Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.