Z-Stack API Reference  8.31.00.00
SS IAS WD Commands Received

This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification. More...

Macros

#define COMMAND_IASWD_START_WARNING   0x00
 
#define COMMAND_IASWD_SQUAWK   0x01
 

Detailed Description

This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification.

Macro Definition Documentation

§ COMMAND_IASWD_SQUAWK

#define COMMAND_IASWD_SQUAWK   0x01

This command uses the WD capabilities to emit a quick audible/visible pulse called a "squawk". The squawk command has no effect if the WD is currently active (warning in progress).

§ COMMAND_IASWD_START_WARNING

#define COMMAND_IASWD_START_WARNING   0x00

This command starts the WD operation. The WD alerts the surrounding area by audible (siren) and visual (strobe) signals.