Z-Stack API Reference  8.31.00.00
SS IAS Zone Status Command Received

This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification. More...

Macros

#define COMMAND_IAS_ZONE_ZONE_ENROLL_RESPONSE   0x00
 
#define COMMAND_IAS_ZONE_INITIATE_NORMAL_OPERATION_MODE   0x01
 Used to tell the IAS Zone server to commence normal operation mode.
 
#define COMMAND_IAS_ZONE_INITIATE_TEST_MODE   0x02
 

Detailed Description

This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification.

Macro Definition Documentation

§ COMMAND_IAS_ZONE_INITIATE_TEST_MODE

#define COMMAND_IAS_ZONE_INITIATE_TEST_MODE   0x02

This command enables IAS Zone servers to be remotely placed into a test mode so that the user or installer MAY configure their field of view, sensitivity, and other operational parameters.

§ COMMAND_IAS_ZONE_ZONE_ENROLL_RESPONSE

#define COMMAND_IAS_ZONE_ZONE_ENROLL_RESPONSE   0x00

On receipt, the device embodying the Zone server is notified that it is now enrolled as an active alarm device