![]() |
![]() |
|
Z-Stack API Reference
8.31.00.00
|
#include <zstack.h>
Data Fields | |
| bool | panCoord |
| bool | ffd |
| bool | mainsPower |
| bool | rxOnWhenIdle |
| bool | security |
Structure defines the Capabilities Information bit field.
| bool ffd |
True if the device is a full function device (FFD)
| bool mainsPower |
True if the device is mains powered
| bool panCoord |
True if the device is a PAN Coordinator
| bool rxOnWhenIdle |
True if the device's RX is on when the device is idle
| bool security |
True if the device is capable of sending and receiving secured frames